CC23x0r2DriverLibrary
cmsis_iccarm.h
Go to the documentation of this file.
1 /**************************************************************************/
8 //------------------------------------------------------------------------------
9 //
10 // Copyright (c) 2017-2020 IAR Systems
11 // Copyright (c) 2017-2019 Arm Limited. All rights reserved.
12 //
13 // SPDX-License-Identifier: Apache-2.0
14 //
15 // Licensed under the Apache License, Version 2.0 (the "License")
16 // you may not use this file except in compliance with the License.
17 // You may obtain a copy of the License at
18 // http://www.apache.org/licenses/LICENSE-2.0
19 //
20 // Unless required by applicable law or agreed to in writing, software
21 // distributed under the License is distributed on an "AS IS" BASIS,
22 // WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
23 // See the License for the specific language governing permissions and
24 // limitations under the License.
25 //
26 //------------------------------------------------------------------------------
27 
28 
29 #ifndef __CMSIS_ICCARM_H__
30 #define __CMSIS_ICCARM_H__
31 
32 #ifndef __ICCARM__
33  #error This file should only be compiled by ICCARM
34 #endif
35 
36 #pragma system_include
37 
38 #define __IAR_FT _Pragma("inline=forced") __intrinsic
39 
40 #if (__VER__ >= 8000000)
41  #define __ICCARM_V8 1
42 #else
43  #define __ICCARM_V8 0
44 #endif
45 
46 #ifndef __ALIGNED
47  #if __ICCARM_V8
48  #define __ALIGNED(x) __attribute__((aligned(x)))
49  #elif (__VER__ >= 7080000)
50  /* Needs IAR language extensions */
51  #define __ALIGNED(x) __attribute__((aligned(x)))
52  #else
53  #warning No compiler specific solution for __ALIGNED.__ALIGNED is ignored.
54  #define __ALIGNED(x)
55  #endif
56 #endif
57 
58 
59 /* Define compiler macros for CPU architecture, used in CMSIS 5.
60  */
61 #if __ARM_ARCH_6M__ || __ARM_ARCH_7M__ || __ARM_ARCH_7EM__ || __ARM_ARCH_8M_BASE__ || __ARM_ARCH_8M_MAIN__
62 /* Macros already defined */
63 #else
64  #if defined(__ARM8M_MAINLINE__) || defined(__ARM8EM_MAINLINE__)
65  #define __ARM_ARCH_8M_MAIN__ 1
66  #elif defined(__ARM8M_BASELINE__)
67  #define __ARM_ARCH_8M_BASE__ 1
68  #elif defined(__ARM_ARCH_PROFILE) && __ARM_ARCH_PROFILE == 'M'
69  #if __ARM_ARCH == 6
70  #define __ARM_ARCH_6M__ 1
71  #elif __ARM_ARCH == 7
72  #if __ARM_FEATURE_DSP
73  #define __ARM_ARCH_7EM__ 1
74  #else
75  #define __ARM_ARCH_7M__ 1
76  #endif
77  #endif /* __ARM_ARCH */
78  #endif /* __ARM_ARCH_PROFILE == 'M' */
79 #endif
80 
81 /* Alternativ core deduction for older ICCARM's */
82 #if !defined(__ARM_ARCH_6M__) && !defined(__ARM_ARCH_7M__) && !defined(__ARM_ARCH_7EM__) && \
83  !defined(__ARM_ARCH_8M_BASE__) && !defined(__ARM_ARCH_8M_MAIN__)
84  #if defined(__ARM6M__) && (__CORE__ == __ARM6M__)
85  #define __ARM_ARCH_6M__ 1
86  #elif defined(__ARM7M__) && (__CORE__ == __ARM7M__)
87  #define __ARM_ARCH_7M__ 1
88  #elif defined(__ARM7EM__) && (__CORE__ == __ARM7EM__)
89  #define __ARM_ARCH_7EM__ 1
90  #elif defined(__ARM8M_BASELINE__) && (__CORE == __ARM8M_BASELINE__)
91  #define __ARM_ARCH_8M_BASE__ 1
92  #elif defined(__ARM8M_MAINLINE__) && (__CORE == __ARM8M_MAINLINE__)
93  #define __ARM_ARCH_8M_MAIN__ 1
94  #elif defined(__ARM8EM_MAINLINE__) && (__CORE == __ARM8EM_MAINLINE__)
95  #define __ARM_ARCH_8M_MAIN__ 1
96  #else
97  #error "Unknown target."
98  #endif
99 #endif
100 
101 
102 
103 #if defined(__ARM_ARCH_6M__) && __ARM_ARCH_6M__==1
104  #define __IAR_M0_FAMILY 1
105 #elif defined(__ARM_ARCH_8M_BASE__) && __ARM_ARCH_8M_BASE__==1
106  #define __IAR_M0_FAMILY 1
107 #else
108  #define __IAR_M0_FAMILY 0
109 #endif
110 
111 
112 #ifndef __ASM
113  #define __ASM __asm
114 #endif
115 
116 #ifndef __COMPILER_BARRIER
117  #define __COMPILER_BARRIER() __ASM volatile("":::"memory")
118 #endif
119 
120 #ifndef __INLINE
121  #define __INLINE inline
122 #endif
123 
124 #ifndef __NO_RETURN
125  #if __ICCARM_V8
126  #define __NO_RETURN __attribute__((__noreturn__))
127  #else
128  #define __NO_RETURN _Pragma("object_attribute=__noreturn")
129  #endif
130 #endif
131 
132 #ifndef __PACKED
133  #if __ICCARM_V8
134  #define __PACKED __attribute__((packed, aligned(1)))
135  #else
136  /* Needs IAR language extensions */
137  #define __PACKED __packed
138  #endif
139 #endif
140 
141 #ifndef __PACKED_STRUCT
142  #if __ICCARM_V8
143  #define __PACKED_STRUCT struct __attribute__((packed, aligned(1)))
144  #else
145  /* Needs IAR language extensions */
146  #define __PACKED_STRUCT __packed struct
147  #endif
148 #endif
149 
150 #ifndef __PACKED_UNION
151  #if __ICCARM_V8
152  #define __PACKED_UNION union __attribute__((packed, aligned(1)))
153  #else
154  /* Needs IAR language extensions */
155  #define __PACKED_UNION __packed union
156  #endif
157 #endif
158 
159 #ifndef __RESTRICT
160  #if __ICCARM_V8
161  #define __RESTRICT __restrict
162  #else
163  /* Needs IAR language extensions */
164  #define __RESTRICT restrict
165  #endif
166 #endif
167 
168 #ifndef __STATIC_INLINE
169  #define __STATIC_INLINE static inline
170 #endif
171 
172 #ifndef __FORCEINLINE
173  #define __FORCEINLINE _Pragma("inline=forced")
174 #endif
175 
176 #ifndef __STATIC_FORCEINLINE
177  #define __STATIC_FORCEINLINE __FORCEINLINE __STATIC_INLINE
178 #endif
179 
180 #ifndef __UNALIGNED_UINT16_READ
181 #pragma language=save
182 #pragma language=extended
183 __IAR_FT uint16_t __iar_uint16_read(void const *ptr)
184 {
185  return *(__packed uint16_t*)(ptr);
186 }
187 #pragma language=restore
188 #define __UNALIGNED_UINT16_READ(PTR) __iar_uint16_read(PTR)
189 #endif
190 
191 
192 #ifndef __UNALIGNED_UINT16_WRITE
193 #pragma language=save
194 #pragma language=extended
195 __IAR_FT void __iar_uint16_write(void const *ptr, uint16_t val)
196 {
197  *(__packed uint16_t*)(ptr) = val;;
198 }
199 #pragma language=restore
200 #define __UNALIGNED_UINT16_WRITE(PTR,VAL) __iar_uint16_write(PTR,VAL)
201 #endif
202 
203 #ifndef __UNALIGNED_UINT32_READ
204 #pragma language=save
205 #pragma language=extended
206 __IAR_FT uint32_t __iar_uint32_read(void const *ptr)
207 {
208  return *(__packed uint32_t*)(ptr);
209 }
210 #pragma language=restore
211 #define __UNALIGNED_UINT32_READ(PTR) __iar_uint32_read(PTR)
212 #endif
213 
214 #ifndef __UNALIGNED_UINT32_WRITE
215 #pragma language=save
216 #pragma language=extended
217 __IAR_FT void __iar_uint32_write(void const *ptr, uint32_t val)
218 {
219  *(__packed uint32_t*)(ptr) = val;;
220 }
221 #pragma language=restore
222 #define __UNALIGNED_UINT32_WRITE(PTR,VAL) __iar_uint32_write(PTR,VAL)
223 #endif
224 
225 #ifndef __UNALIGNED_UINT32 /* deprecated */
226 #pragma language=save
227 #pragma language=extended
228 __packed struct __iar_u32 { uint32_t v; };
229 #pragma language=restore
230 #define __UNALIGNED_UINT32(PTR) (((struct __iar_u32 *)(PTR))->v)
231 #endif
232 
233 #ifndef __USED
234  #if __ICCARM_V8
235  #define __USED __attribute__((used))
236  #else
237  #define __USED _Pragma("__root")
238  #endif
239 #endif
240 
241 #undef __WEAK /* undo the definition from DLib_Defaults.h */
242 #ifndef __WEAK
243  #if __ICCARM_V8
244  #define __WEAK __attribute__((weak))
245  #else
246  #define __WEAK _Pragma("__weak")
247  #endif
248 #endif
249 
250 #ifndef __PROGRAM_START
251 #define __PROGRAM_START __iar_program_start
252 #endif
253 
254 #ifndef __INITIAL_SP
255 #define __INITIAL_SP CSTACK$$Limit
256 #endif
257 
258 #ifndef __STACK_LIMIT
259 #define __STACK_LIMIT CSTACK$$Base
260 #endif
261 
262 #ifndef __VECTOR_TABLE
263 #define __VECTOR_TABLE __vector_table
264 #endif
265 
266 #ifndef __VECTOR_TABLE_ATTRIBUTE
267 #define __VECTOR_TABLE_ATTRIBUTE @".intvec"
268 #endif
269 
270 #ifndef __ICCARM_INTRINSICS_VERSION__
271  #define __ICCARM_INTRINSICS_VERSION__ 0
272 #endif
273 
274 #if __ICCARM_INTRINSICS_VERSION__ == 2
275 
276  #if defined(__CLZ)
277  #undef __CLZ
278  #endif
279  #if defined(__REVSH)
280  #undef __REVSH
281  #endif
282  #if defined(__RBIT)
283  #undef __RBIT
284  #endif
285  #if defined(__SSAT)
286  #undef __SSAT
287  #endif
288  #if defined(__USAT)
289  #undef __USAT
290  #endif
291 
292  #include "iccarm_builtin.h"
293 
294  #define __disable_fault_irq __iar_builtin_disable_fiq
295  #define __disable_irq __iar_builtin_disable_interrupt
296  #define __enable_fault_irq __iar_builtin_enable_fiq
297  #define __enable_irq __iar_builtin_enable_interrupt
298  #define __arm_rsr __iar_builtin_rsr
299  #define __arm_wsr __iar_builtin_wsr
300 
301 
302  #define __get_APSR() (__arm_rsr("APSR"))
303  #define __get_BASEPRI() (__arm_rsr("BASEPRI"))
304  #define __get_CONTROL() (__arm_rsr("CONTROL"))
305  #define __get_FAULTMASK() (__arm_rsr("FAULTMASK"))
306 
307  #if ((defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U)) && \
308  (defined (__FPU_USED ) && (__FPU_USED == 1U)) )
309  #define __get_FPSCR() (__arm_rsr("FPSCR"))
310  #define __set_FPSCR(VALUE) (__arm_wsr("FPSCR", (VALUE)))
311  #else
312  #define __get_FPSCR() ( 0 )
313  #define __set_FPSCR(VALUE) ((void)VALUE)
314  #endif
315 
316  #define __get_IPSR() (__arm_rsr("IPSR"))
317  #define __get_MSP() (__arm_rsr("MSP"))
318  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
319  (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3)))
320  // without main extensions, the non-secure MSPLIM is RAZ/WI
321  #define __get_MSPLIM() (0U)
322  #else
323  #define __get_MSPLIM() (__arm_rsr("MSPLIM"))
324  #endif
325  #define __get_PRIMASK() (__arm_rsr("PRIMASK"))
326  #define __get_PSP() (__arm_rsr("PSP"))
327 
328  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
329  (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3)))
330  // without main extensions, the non-secure PSPLIM is RAZ/WI
331  #define __get_PSPLIM() (0U)
332  #else
333  #define __get_PSPLIM() (__arm_rsr("PSPLIM"))
334  #endif
335 
336  #define __get_xPSR() (__arm_rsr("xPSR"))
337 
338  #define __set_BASEPRI(VALUE) (__arm_wsr("BASEPRI", (VALUE)))
339  #define __set_BASEPRI_MAX(VALUE) (__arm_wsr("BASEPRI_MAX", (VALUE)))
340  #define __set_CONTROL(VALUE) (__arm_wsr("CONTROL", (VALUE)))
341  #define __set_FAULTMASK(VALUE) (__arm_wsr("FAULTMASK", (VALUE)))
342  #define __set_MSP(VALUE) (__arm_wsr("MSP", (VALUE)))
343 
344  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
345  (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3)))
346  // without main extensions, the non-secure MSPLIM is RAZ/WI
347  #define __set_MSPLIM(VALUE) ((void)(VALUE))
348  #else
349  #define __set_MSPLIM(VALUE) (__arm_wsr("MSPLIM", (VALUE)))
350  #endif
351  #define __set_PRIMASK(VALUE) (__arm_wsr("PRIMASK", (VALUE)))
352  #define __set_PSP(VALUE) (__arm_wsr("PSP", (VALUE)))
353  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
354  (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3)))
355  // without main extensions, the non-secure PSPLIM is RAZ/WI
356  #define __set_PSPLIM(VALUE) ((void)(VALUE))
357  #else
358  #define __set_PSPLIM(VALUE) (__arm_wsr("PSPLIM", (VALUE)))
359  #endif
360 
361  #define __TZ_get_CONTROL_NS() (__arm_rsr("CONTROL_NS"))
362  #define __TZ_set_CONTROL_NS(VALUE) (__arm_wsr("CONTROL_NS", (VALUE)))
363  #define __TZ_get_PSP_NS() (__arm_rsr("PSP_NS"))
364  #define __TZ_set_PSP_NS(VALUE) (__arm_wsr("PSP_NS", (VALUE)))
365  #define __TZ_get_MSP_NS() (__arm_rsr("MSP_NS"))
366  #define __TZ_set_MSP_NS(VALUE) (__arm_wsr("MSP_NS", (VALUE)))
367  #define __TZ_get_SP_NS() (__arm_rsr("SP_NS"))
368  #define __TZ_set_SP_NS(VALUE) (__arm_wsr("SP_NS", (VALUE)))
369  #define __TZ_get_PRIMASK_NS() (__arm_rsr("PRIMASK_NS"))
370  #define __TZ_set_PRIMASK_NS(VALUE) (__arm_wsr("PRIMASK_NS", (VALUE)))
371  #define __TZ_get_BASEPRI_NS() (__arm_rsr("BASEPRI_NS"))
372  #define __TZ_set_BASEPRI_NS(VALUE) (__arm_wsr("BASEPRI_NS", (VALUE)))
373  #define __TZ_get_FAULTMASK_NS() (__arm_rsr("FAULTMASK_NS"))
374  #define __TZ_set_FAULTMASK_NS(VALUE)(__arm_wsr("FAULTMASK_NS", (VALUE)))
375 
376  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
377  (!defined (__ARM_FEATURE_CMSE) || (__ARM_FEATURE_CMSE < 3)))
378  // without main extensions, the non-secure PSPLIM is RAZ/WI
379  #define __TZ_get_PSPLIM_NS() (0U)
380  #define __TZ_set_PSPLIM_NS(VALUE) ((void)(VALUE))
381  #else
382  #define __TZ_get_PSPLIM_NS() (__arm_rsr("PSPLIM_NS"))
383  #define __TZ_set_PSPLIM_NS(VALUE) (__arm_wsr("PSPLIM_NS", (VALUE)))
384  #endif
385 
386  #define __TZ_get_MSPLIM_NS() (__arm_rsr("MSPLIM_NS"))
387  #define __TZ_set_MSPLIM_NS(VALUE) (__arm_wsr("MSPLIM_NS", (VALUE)))
388 
389  #define __NOP __iar_builtin_no_operation
390 
391  #define __CLZ __iar_builtin_CLZ
392  #define __CLREX __iar_builtin_CLREX
393 
394  #define __DMB __iar_builtin_DMB
395  #define __DSB __iar_builtin_DSB
396  #define __ISB __iar_builtin_ISB
397 
398  #define __LDREXB __iar_builtin_LDREXB
399  #define __LDREXH __iar_builtin_LDREXH
400  #define __LDREXW __iar_builtin_LDREX
401 
402  #define __RBIT __iar_builtin_RBIT
403  #define __REV __iar_builtin_REV
404  #define __REV16 __iar_builtin_REV16
405 
406  __IAR_FT int16_t __REVSH(int16_t val)
407  {
408  return (int16_t) __iar_builtin_REVSH(val);
409  }
410 
411  #define __ROR __iar_builtin_ROR
412  #define __RRX __iar_builtin_RRX
413 
414  #define __SEV __iar_builtin_SEV
415 
416  #if !__IAR_M0_FAMILY
417  #define __SSAT __iar_builtin_SSAT
418  #endif
419 
420  #define __STREXB __iar_builtin_STREXB
421  #define __STREXH __iar_builtin_STREXH
422  #define __STREXW __iar_builtin_STREX
423 
424  #if !__IAR_M0_FAMILY
425  #define __USAT __iar_builtin_USAT
426  #endif
427 
428  #define __WFE __iar_builtin_WFE
429  #define __WFI __iar_builtin_WFI
430 
431  #if __ARM_MEDIA__
432  #define __SADD8 __iar_builtin_SADD8
433  #define __QADD8 __iar_builtin_QADD8
434  #define __SHADD8 __iar_builtin_SHADD8
435  #define __UADD8 __iar_builtin_UADD8
436  #define __UQADD8 __iar_builtin_UQADD8
437  #define __UHADD8 __iar_builtin_UHADD8
438  #define __SSUB8 __iar_builtin_SSUB8
439  #define __QSUB8 __iar_builtin_QSUB8
440  #define __SHSUB8 __iar_builtin_SHSUB8
441  #define __USUB8 __iar_builtin_USUB8
442  #define __UQSUB8 __iar_builtin_UQSUB8
443  #define __UHSUB8 __iar_builtin_UHSUB8
444  #define __SADD16 __iar_builtin_SADD16
445  #define __QADD16 __iar_builtin_QADD16
446  #define __SHADD16 __iar_builtin_SHADD16
447  #define __UADD16 __iar_builtin_UADD16
448  #define __UQADD16 __iar_builtin_UQADD16
449  #define __UHADD16 __iar_builtin_UHADD16
450  #define __SSUB16 __iar_builtin_SSUB16
451  #define __QSUB16 __iar_builtin_QSUB16
452  #define __SHSUB16 __iar_builtin_SHSUB16
453  #define __USUB16 __iar_builtin_USUB16
454  #define __UQSUB16 __iar_builtin_UQSUB16
455  #define __UHSUB16 __iar_builtin_UHSUB16
456  #define __SASX __iar_builtin_SASX
457  #define __QASX __iar_builtin_QASX
458  #define __SHASX __iar_builtin_SHASX
459  #define __UASX __iar_builtin_UASX
460  #define __UQASX __iar_builtin_UQASX
461  #define __UHASX __iar_builtin_UHASX
462  #define __SSAX __iar_builtin_SSAX
463  #define __QSAX __iar_builtin_QSAX
464  #define __SHSAX __iar_builtin_SHSAX
465  #define __USAX __iar_builtin_USAX
466  #define __UQSAX __iar_builtin_UQSAX
467  #define __UHSAX __iar_builtin_UHSAX
468  #define __USAD8 __iar_builtin_USAD8
469  #define __USADA8 __iar_builtin_USADA8
470  #define __SSAT16 __iar_builtin_SSAT16
471  #define __USAT16 __iar_builtin_USAT16
472  #define __UXTB16 __iar_builtin_UXTB16
473  #define __UXTAB16 __iar_builtin_UXTAB16
474  #define __SXTB16 __iar_builtin_SXTB16
475  #define __SXTAB16 __iar_builtin_SXTAB16
476  #define __SMUAD __iar_builtin_SMUAD
477  #define __SMUADX __iar_builtin_SMUADX
478  #define __SMMLA __iar_builtin_SMMLA
479  #define __SMLAD __iar_builtin_SMLAD
480  #define __SMLADX __iar_builtin_SMLADX
481  #define __SMLALD __iar_builtin_SMLALD
482  #define __SMLALDX __iar_builtin_SMLALDX
483  #define __SMUSD __iar_builtin_SMUSD
484  #define __SMUSDX __iar_builtin_SMUSDX
485  #define __SMLSD __iar_builtin_SMLSD
486  #define __SMLSDX __iar_builtin_SMLSDX
487  #define __SMLSLD __iar_builtin_SMLSLD
488  #define __SMLSLDX __iar_builtin_SMLSLDX
489  #define __SEL __iar_builtin_SEL
490  #define __QADD __iar_builtin_QADD
491  #define __QSUB __iar_builtin_QSUB
492  #define __PKHBT __iar_builtin_PKHBT
493  #define __PKHTB __iar_builtin_PKHTB
494  #endif
495 
496 #else /* __ICCARM_INTRINSICS_VERSION__ == 2 */
497 
498  #if __IAR_M0_FAMILY
499  /* Avoid clash between intrinsics.h and arm_math.h when compiling for Cortex-M0. */
500  #define __CLZ __cmsis_iar_clz_not_active
501  #define __SSAT __cmsis_iar_ssat_not_active
502  #define __USAT __cmsis_iar_usat_not_active
503  #define __RBIT __cmsis_iar_rbit_not_active
504  #define __get_APSR __cmsis_iar_get_APSR_not_active
505  #endif
506 
507 
508  #if (!((defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U)) && \
509  (defined (__FPU_USED ) && (__FPU_USED == 1U)) ))
510  #define __get_FPSCR __cmsis_iar_get_FPSR_not_active
511  #define __set_FPSCR __cmsis_iar_set_FPSR_not_active
512  #endif
513 
514  #ifdef __INTRINSICS_INCLUDED
515  #error intrinsics.h is already included previously!
516  #endif
517 
518  #include <intrinsics.h>
519 
520  #if __IAR_M0_FAMILY
521  /* Avoid clash between intrinsics.h and arm_math.h when compiling for Cortex-M0. */
522  #undef __CLZ
523  #undef __SSAT
524  #undef __USAT
525  #undef __RBIT
526  #undef __get_APSR
527 
528  __STATIC_INLINE uint8_t __CLZ(uint32_t data)
529  {
530  if (data == 0U) { return 32U; }
531 
532  uint32_t count = 0U;
533  uint32_t mask = 0x80000000U;
534 
535  while ((data & mask) == 0U)
536  {
537  count += 1U;
538  mask = mask >> 1U;
539  }
540  return count;
541  }
542 
543  __STATIC_INLINE uint32_t __RBIT(uint32_t v)
544  {
545  uint8_t sc = 31U;
546  uint32_t r = v;
547  for (v >>= 1U; v; v >>= 1U)
548  {
549  r <<= 1U;
550  r |= v & 1U;
551  sc--;
552  }
553  return (r << sc);
554  }
555 
556  __STATIC_INLINE uint32_t __get_APSR(void)
557  {
558  uint32_t res;
559  __asm("MRS %0,APSR" : "=r" (res));
560  return res;
561  }
562 
563  #endif
564 
565  #if (!((defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U)) && \
566  (defined (__FPU_USED ) && (__FPU_USED == 1U)) ))
567  #undef __get_FPSCR
568  #undef __set_FPSCR
569  #define __get_FPSCR() (0)
570  #define __set_FPSCR(VALUE) ((void)VALUE)
571  #endif
572 
573  #pragma diag_suppress=Pe940
574  #pragma diag_suppress=Pe177
575 
576  #define __enable_irq __enable_interrupt
577  #define __disable_irq __disable_interrupt
578  #define __NOP __no_operation
579 
580  #define __get_xPSR __get_PSR
581 
582  #if (!defined(__ARM_ARCH_6M__) || __ARM_ARCH_6M__==0)
583 
584  __IAR_FT uint32_t __LDREXW(uint32_t volatile *ptr)
585  {
586  return __LDREX((unsigned long *)ptr);
587  }
588 
589  __IAR_FT uint32_t __STREXW(uint32_t value, uint32_t volatile *ptr)
590  {
591  return __STREX(value, (unsigned long *)ptr);
592  }
593  #endif
594 
595 
596  /* __CORTEX_M is defined in core_cm0.h, core_cm3.h and core_cm4.h. */
597  #if (__CORTEX_M >= 0x03)
598 
599  __IAR_FT uint32_t __RRX(uint32_t value)
600  {
601  uint32_t result;
602  __ASM volatile("RRX %0, %1" : "=r"(result) : "r" (value));
603  return(result);
604  }
605 
606  __IAR_FT void __set_BASEPRI_MAX(uint32_t value)
607  {
608  __asm volatile("MSR BASEPRI_MAX,%0"::"r" (value));
609  }
610 
611 
612  #define __enable_fault_irq __enable_fiq
613  #define __disable_fault_irq __disable_fiq
614 
615 
616  #endif /* (__CORTEX_M >= 0x03) */
617 
618  __IAR_FT uint32_t __ROR(uint32_t op1, uint32_t op2)
619  {
620  return (op1 >> op2) | (op1 << ((sizeof(op1)*8)-op2));
621  }
622 
623  #if ((defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) || \
624  (defined (__ARM_ARCH_8M_BASE__ ) && (__ARM_ARCH_8M_BASE__ == 1)) )
625 
626  __IAR_FT uint32_t __get_MSPLIM(void)
627  {
628  uint32_t res;
629  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
630  (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3)))
631  // without main extensions, the non-secure MSPLIM is RAZ/WI
632  res = 0U;
633  #else
634  __asm volatile("MRS %0,MSPLIM" : "=r" (res));
635  #endif
636  return res;
637  }
638 
639  __IAR_FT void __set_MSPLIM(uint32_t value)
640  {
641  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
642  (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3)))
643  // without main extensions, the non-secure MSPLIM is RAZ/WI
644  (void)value;
645  #else
646  __asm volatile("MSR MSPLIM,%0" :: "r" (value));
647  #endif
648  }
649 
650  __IAR_FT uint32_t __get_PSPLIM(void)
651  {
652  uint32_t res;
653  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
654  (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3)))
655  // without main extensions, the non-secure PSPLIM is RAZ/WI
656  res = 0U;
657  #else
658  __asm volatile("MRS %0,PSPLIM" : "=r" (res));
659  #endif
660  return res;
661  }
662 
663  __IAR_FT void __set_PSPLIM(uint32_t value)
664  {
665  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
666  (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3)))
667  // without main extensions, the non-secure PSPLIM is RAZ/WI
668  (void)value;
669  #else
670  __asm volatile("MSR PSPLIM,%0" :: "r" (value));
671  #endif
672  }
673 
674  __IAR_FT uint32_t __TZ_get_CONTROL_NS(void)
675  {
676  uint32_t res;
677  __asm volatile("MRS %0,CONTROL_NS" : "=r" (res));
678  return res;
679  }
680 
681  __IAR_FT void __TZ_set_CONTROL_NS(uint32_t value)
682  {
683  __asm volatile("MSR CONTROL_NS,%0" :: "r" (value));
684  }
685 
686  __IAR_FT uint32_t __TZ_get_PSP_NS(void)
687  {
688  uint32_t res;
689  __asm volatile("MRS %0,PSP_NS" : "=r" (res));
690  return res;
691  }
692 
693  __IAR_FT void __TZ_set_PSP_NS(uint32_t value)
694  {
695  __asm volatile("MSR PSP_NS,%0" :: "r" (value));
696  }
697 
698  __IAR_FT uint32_t __TZ_get_MSP_NS(void)
699  {
700  uint32_t res;
701  __asm volatile("MRS %0,MSP_NS" : "=r" (res));
702  return res;
703  }
704 
705  __IAR_FT void __TZ_set_MSP_NS(uint32_t value)
706  {
707  __asm volatile("MSR MSP_NS,%0" :: "r" (value));
708  }
709 
710  __IAR_FT uint32_t __TZ_get_SP_NS(void)
711  {
712  uint32_t res;
713  __asm volatile("MRS %0,SP_NS" : "=r" (res));
714  return res;
715  }
716  __IAR_FT void __TZ_set_SP_NS(uint32_t value)
717  {
718  __asm volatile("MSR SP_NS,%0" :: "r" (value));
719  }
720 
721  __IAR_FT uint32_t __TZ_get_PRIMASK_NS(void)
722  {
723  uint32_t res;
724  __asm volatile("MRS %0,PRIMASK_NS" : "=r" (res));
725  return res;
726  }
727 
728  __IAR_FT void __TZ_set_PRIMASK_NS(uint32_t value)
729  {
730  __asm volatile("MSR PRIMASK_NS,%0" :: "r" (value));
731  }
732 
733  __IAR_FT uint32_t __TZ_get_BASEPRI_NS(void)
734  {
735  uint32_t res;
736  __asm volatile("MRS %0,BASEPRI_NS" : "=r" (res));
737  return res;
738  }
739 
740  __IAR_FT void __TZ_set_BASEPRI_NS(uint32_t value)
741  {
742  __asm volatile("MSR BASEPRI_NS,%0" :: "r" (value));
743  }
744 
745  __IAR_FT uint32_t __TZ_get_FAULTMASK_NS(void)
746  {
747  uint32_t res;
748  __asm volatile("MRS %0,FAULTMASK_NS" : "=r" (res));
749  return res;
750  }
751 
752  __IAR_FT void __TZ_set_FAULTMASK_NS(uint32_t value)
753  {
754  __asm volatile("MSR FAULTMASK_NS,%0" :: "r" (value));
755  }
756 
757  __IAR_FT uint32_t __TZ_get_PSPLIM_NS(void)
758  {
759  uint32_t res;
760  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
761  (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3)))
762  // without main extensions, the non-secure PSPLIM is RAZ/WI
763  res = 0U;
764  #else
765  __asm volatile("MRS %0,PSPLIM_NS" : "=r" (res));
766  #endif
767  return res;
768  }
769 
770  __IAR_FT void __TZ_set_PSPLIM_NS(uint32_t value)
771  {
772  #if (!(defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) && \
773  (!defined (__ARM_FEATURE_CMSE ) || (__ARM_FEATURE_CMSE < 3)))
774  // without main extensions, the non-secure PSPLIM is RAZ/WI
775  (void)value;
776  #else
777  __asm volatile("MSR PSPLIM_NS,%0" :: "r" (value));
778  #endif
779  }
780 
781  __IAR_FT uint32_t __TZ_get_MSPLIM_NS(void)
782  {
783  uint32_t res;
784  __asm volatile("MRS %0,MSPLIM_NS" : "=r" (res));
785  return res;
786  }
787 
788  __IAR_FT void __TZ_set_MSPLIM_NS(uint32_t value)
789  {
790  __asm volatile("MSR MSPLIM_NS,%0" :: "r" (value));
791  }
792 
793  #endif /* __ARM_ARCH_8M_MAIN__ or __ARM_ARCH_8M_BASE__ */
794 
795 #endif /* __ICCARM_INTRINSICS_VERSION__ == 2 */
796 
797 #define __BKPT(value) __asm volatile ("BKPT %0" : : "i"(value))
798 
799 #if __IAR_M0_FAMILY
800  __STATIC_INLINE int32_t __SSAT(int32_t val, uint32_t sat)
801  {
802  if ((sat >= 1U) && (sat <= 32U))
803  {
804  const int32_t max = (int32_t)((1U << (sat - 1U)) - 1U);
805  const int32_t min = -1 - max ;
806  if (val > max)
807  {
808  return max;
809  }
810  else if (val < min)
811  {
812  return min;
813  }
814  }
815  return val;
816  }
817 
818  __STATIC_INLINE uint32_t __USAT(int32_t val, uint32_t sat)
819  {
820  if (sat <= 31U)
821  {
822  const uint32_t max = ((1U << sat) - 1U);
823  if (val > (int32_t)max)
824  {
825  return max;
826  }
827  else if (val < 0)
828  {
829  return 0U;
830  }
831  }
832  return (uint32_t)val;
833  }
834 #endif
835 
836 #if (__CORTEX_M >= 0x03) /* __CORTEX_M is defined in core_cm0.h, core_cm3.h and core_cm4.h. */
837 
838  __IAR_FT uint8_t __LDRBT(volatile uint8_t *addr)
839  {
840  uint32_t res;
841  __ASM volatile ("LDRBT %0, [%1]" : "=r" (res) : "r" (addr) : "memory");
842  return ((uint8_t)res);
843  }
844 
845  __IAR_FT uint16_t __LDRHT(volatile uint16_t *addr)
846  {
847  uint32_t res;
848  __ASM volatile ("LDRHT %0, [%1]" : "=r" (res) : "r" (addr) : "memory");
849  return ((uint16_t)res);
850  }
851 
852  __IAR_FT uint32_t __LDRT(volatile uint32_t *addr)
853  {
854  uint32_t res;
855  __ASM volatile ("LDRT %0, [%1]" : "=r" (res) : "r" (addr) : "memory");
856  return res;
857  }
858 
859  __IAR_FT void __STRBT(uint8_t value, volatile uint8_t *addr)
860  {
861  __ASM volatile ("STRBT %1, [%0]" : : "r" (addr), "r" ((uint32_t)value) : "memory");
862  }
863 
864  __IAR_FT void __STRHT(uint16_t value, volatile uint16_t *addr)
865  {
866  __ASM volatile ("STRHT %1, [%0]" : : "r" (addr), "r" ((uint32_t)value) : "memory");
867  }
868 
869  __IAR_FT void __STRT(uint32_t value, volatile uint32_t *addr)
870  {
871  __ASM volatile ("STRT %1, [%0]" : : "r" (addr), "r" (value) : "memory");
872  }
873 
874 #endif /* (__CORTEX_M >= 0x03) */
875 
876 #if ((defined (__ARM_ARCH_8M_MAIN__ ) && (__ARM_ARCH_8M_MAIN__ == 1)) || \
877  (defined (__ARM_ARCH_8M_BASE__ ) && (__ARM_ARCH_8M_BASE__ == 1)) )
878 
879 
880  __IAR_FT uint8_t __LDAB(volatile uint8_t *ptr)
881  {
882  uint32_t res;
883  __ASM volatile ("LDAB %0, [%1]" : "=r" (res) : "r" (ptr) : "memory");
884  return ((uint8_t)res);
885  }
886 
887  __IAR_FT uint16_t __LDAH(volatile uint16_t *ptr)
888  {
889  uint32_t res;
890  __ASM volatile ("LDAH %0, [%1]" : "=r" (res) : "r" (ptr) : "memory");
891  return ((uint16_t)res);
892  }
893 
894  __IAR_FT uint32_t __LDA(volatile uint32_t *ptr)
895  {
896  uint32_t res;
897  __ASM volatile ("LDA %0, [%1]" : "=r" (res) : "r" (ptr) : "memory");
898  return res;
899  }
900 
901  __IAR_FT void __STLB(uint8_t value, volatile uint8_t *ptr)
902  {
903  __ASM volatile ("STLB %1, [%0]" :: "r" (ptr), "r" (value) : "memory");
904  }
905 
906  __IAR_FT void __STLH(uint16_t value, volatile uint16_t *ptr)
907  {
908  __ASM volatile ("STLH %1, [%0]" :: "r" (ptr), "r" (value) : "memory");
909  }
910 
911  __IAR_FT void __STL(uint32_t value, volatile uint32_t *ptr)
912  {
913  __ASM volatile ("STL %1, [%0]" :: "r" (ptr), "r" (value) : "memory");
914  }
915 
916  __IAR_FT uint8_t __LDAEXB(volatile uint8_t *ptr)
917  {
918  uint32_t res;
919  __ASM volatile ("LDAEXB %0, [%1]" : "=r" (res) : "r" (ptr) : "memory");
920  return ((uint8_t)res);
921  }
922 
923  __IAR_FT uint16_t __LDAEXH(volatile uint16_t *ptr)
924  {
925  uint32_t res;
926  __ASM volatile ("LDAEXH %0, [%1]" : "=r" (res) : "r" (ptr) : "memory");
927  return ((uint16_t)res);
928  }
929 
930  __IAR_FT uint32_t __LDAEX(volatile uint32_t *ptr)
931  {
932  uint32_t res;
933  __ASM volatile ("LDAEX %0, [%1]" : "=r" (res) : "r" (ptr) : "memory");
934  return res;
935  }
936 
937  __IAR_FT uint32_t __STLEXB(uint8_t value, volatile uint8_t *ptr)
938  {
939  uint32_t res;
940  __ASM volatile ("STLEXB %0, %2, [%1]" : "=r" (res) : "r" (ptr), "r" (value) : "memory");
941  return res;
942  }
943 
944  __IAR_FT uint32_t __STLEXH(uint16_t value, volatile uint16_t *ptr)
945  {
946  uint32_t res;
947  __ASM volatile ("STLEXH %0, %2, [%1]" : "=r" (res) : "r" (ptr), "r" (value) : "memory");
948  return res;
949  }
950 
951  __IAR_FT uint32_t __STLEX(uint32_t value, volatile uint32_t *ptr)
952  {
953  uint32_t res;
954  __ASM volatile ("STLEX %0, %2, [%1]" : "=r" (res) : "r" (ptr), "r" (value) : "memory");
955  return res;
956  }
957 
958 #endif /* __ARM_ARCH_8M_MAIN__ or __ARM_ARCH_8M_BASE__ */
959 
960 #undef __IAR_FT
961 #undef __IAR_M0_FAMILY
962 #undef __ICCARM_V8
963 
964 #pragma diag_default=Pe940
965 #pragma diag_default=Pe177
966 
967 #define __SXTB16_RORn(ARG1, ARG2) __SXTB16(__ROR(ARG1, ARG2))
968 
969 #endif /* __CMSIS_ICCARM_H__ */
__STATIC_FORCEINLINE uint32_t __USAT(int32_t val, uint32_t sat)
Unsigned Saturate.
Definition: cmsis_gcc.h:1407
uint32_t v
Definition: cmsis_iccarm.h:228
#define __STATIC_INLINE
Definition: cmsis_iccarm.h:169
#define __IAR_FT
Definition: cmsis_iccarm.h:38
__STATIC_FORCEINLINE int16_t __REVSH(int16_t value)
Reverse byte order (16 bit)
Definition: cmsis_gcc.h:1001
__IAR_FT uint32_t __ROR(uint32_t op1, uint32_t op2)
Definition: cmsis_iccarm.h:618
#define __ASM
Definition: cmsis_iccarm.h:113
__STATIC_FORCEINLINE uint32_t __RBIT(uint32_t value)
Reverse bit order of value.
Definition: cmsis_gcc.h:1048
__STATIC_FORCEINLINE uint32_t __get_APSR(void)
Get APSR Register.
Definition: cmsis_gcc.h:286
__IAR_FT void __iar_uint32_write(void const *ptr, uint32_t val)
Definition: cmsis_iccarm.h:217
__STATIC_FORCEINLINE uint8_t __CLZ(uint32_t value)
Count leading zeros.
Definition: cmsis_gcc.h:1078
__IAR_FT uint32_t __LDREXW(uint32_t volatile *ptr)
Definition: cmsis_iccarm.h:584
__STATIC_FORCEINLINE int32_t __SSAT(int32_t val, uint32_t sat)
Signed Saturate.
Definition: cmsis_gcc.h:1382
__IAR_FT uint32_t __iar_uint32_read(void const *ptr)
Definition: cmsis_iccarm.h:206
__IAR_FT uint16_t __iar_uint16_read(void const *ptr)
Definition: cmsis_iccarm.h:183
Definition: cmsis_iccarm.h:228
__IAR_FT void __iar_uint16_write(void const *ptr, uint16_t val)
Definition: cmsis_iccarm.h:195
__IAR_FT uint32_t __STREXW(uint32_t value, uint32_t volatile *ptr)
Definition: cmsis_iccarm.h:589