UTIL_NV_Read
------------
:Opcode: 0xFE81
:Command Description: Send this command to read an NV parameter.

**Command Parameters**

:nvID: 

 :Size: 2 byte(s)
 :Default: 0
 :Range: Any 2-byte value

:nvLen: 

 :Size: 1 byte(s)
 :Default: 0
 :Range: Any 1-byte value

**Events Generated**

When this command is received, the host will send the CommandStatus Event.

UTIL_NV_Write
-------------
:Opcode: 0xFE82
:Command Description: Send this command to write an NV parameter.

**Command Parameters**

:nvID: 

 :Size: 2 byte(s)
 :Default: 0
 :Range: Any 2-byte value

:nvDataLen: Size of NV data

 :Size: 1 byte(s)
 :Value: size(nvData)

:nvData: NV Data Field. Structure can be different for each NV item

 :Size: input byte(s)
 :Default: "00"
 :Range: Any 1-byte value

**Events Generated**

When this command is received, the host will send the CommandStatus Event.

UTIL_ForceBoot
--------------
:Opcode: 0xFE83
:Command Description: Force the boot loader to run.

**Events Generated**

When this command is received, the device resets if the boot loader is present. Otherwise, the host will send the CommandStatus Event.

UTIL_BuildRevision
------------------
:Opcode: 0xFE84
:Command Description: This command is used to read the build revision information of the BLE stack software.

**Events Generated**

When this command is received, the host will send the CommandStatus Event.

**Additional Command Status Return Parameters**

:dataLen: 

 :Size: 1 byte(s)
 :Range: 

:stk ver (mj/mn/ph): 

 :Condition: ( StatStatus==0x00)
 :Size: 3 byte(s)
 :Range: 

:bld ver: 

 :Condition: ( StatStatus==0x00)
 :Size: 2 byte(s)
 :Range: 

:stk info: 

 :Condition: ( StatStatus==0x00)
 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  IARProject 
         0x02                  CCSProject 
         0x10                  IARLibrary 
         0x80                  ROMBuild   
         ===================== ========================================================

:ctrl info: 

 :Condition: ( StatStatus==0x00)
 :Size: 2 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  ADV_NCONN      
         0x02                  ADV_CONN       
         0x04                  SCAN           
         0x08                  INIT           
         0x10                  PING           
         0x20                  SLV_FEAT_EXCHG 
         0x40                  CONN_PARAM_REQ 
         ===================== ========================================================

:host info: 

 :Condition: ( StatStatus==0x00)
 :Size: 2 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  BROADCASTER 
         0x02                  OBSERVER    
         0x04                  PERIPHERAL  
         0x08                  CENTRAL     
         ===================== ========================================================


UTIL_GetMemStats
----------------
:Opcode: 0xFE87
:Command Description: Get memory statistics

**Command Parameters**

:command ID: 

 :Size: 1 byte(s)
 :Default: 2
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  Light Heap Statistic 
         0x02                  Full Heap Statistic (requieres HEAPMGR_METRICS) 
         0x04                  Thread usage Statistic (requieres HEAPMGR_METRICS)
         ===================== ========================================================

**Events Generated**

When this command is received, the host will send the CommandStatus Event.

**Additional Command Status Return Parameters**

:dataLen: 

 :Size: 1 byte(s)
 :Range: 

:all cmdID receive : 

 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  Light Heap Statistic 
         0x02                  Full Heap Statistic (requieres HEAPMGR_METRICS) 
         0x04                  Thread usage Statistic (requieres HEAPMGR_METRICS)
         ===================== ========================================================

:cmdID: 

 :Condition: ( (cmdID & 0x01) == 0x01)
 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  Light Heap Statistic 
         0x02                  Full Heap Statistic (requieres HEAPMGR_METRICS) 
         0x04                  Thread usage Statistic (requieres HEAPMGR_METRICS)
         ===================== ========================================================

:Heap Size: 

 :Condition: ( (cmdID & 0x01) == 0x01)
 :Size: 4 byte(s)
 :Range: 

:Heap Size Free: 

 :Condition: ( (cmdID & 0x01) == 0x01)
 :Size: 4 byte(s)
 :Range: 

:Biggest free buffer Available: 

 :Condition: ( (cmdID & 0x01) == 0x01)
 :Size: 4 byte(s)
 :Range: 

:cmdID: 

 :Condition: ( (cmdID & 0x02) == 0x02)
 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  Light Heap Statistic 
         0x02                  Full Heap Statistic (requieres HEAPMGR_METRICS) 
         0x04                  Thread usage Statistic (requieres HEAPMGR_METRICS)
         ===================== ========================================================

:Heap Fail number: 

 :Condition: ( (cmdID & 0x02) == 0x02)
 :Size: 2 byte(s)
 :Range: 

:Heap Allocated: 

 :Condition: ( (cmdID & 0x02) == 0x02)
 :Size: 4 byte(s)
 :Range: 

:Heap Max Allocated: 

 :Condition: ( (cmdID & 0x02) == 0x02)
 :Size: 4 byte(s)
 :Range: 

:cmdID: 

 :Condition: ( (cmdID & 0x04) ==0x04)
 :Size: 1 byte(s)
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  Light Heap Statistic 
         0x02                  Full Heap Statistic (requieres HEAPMGR_METRICS) 
         0x04                  Thread usage Statistic (requieres HEAPMGR_METRICS)
         ===================== ========================================================

:Number of Thread: 

 :Condition: ( (cmdID & 0x04) ==0x04)
 :Size: 1 byte(s)
 :Range: 


An array of size "Count" will be returned containing the parameters starting here:

:Priority: 

 :Condition: ( (cmdID & 0x04) ==0x04)
 :Size: 1 byte(s)
 :Range: 

:Handle: 

 :Condition: ( (cmdID & 0x04) ==0x04)
 :Size: 2 byte(s)
 :Range: 

:max Stack used: 

 :Condition: ( (cmdID & 0x04) ==0x04)
 :Size: 2 byte(s)
 :Range: 

:stack size: 

 :Condition: ( (cmdID & 0x04) ==0x04)
 :Size: 2 byte(s)
 :Range: 


The array of parameters ends here.