***********************************
L2CAP Extension Vendor Specific API
***********************************

L2CAP Extension Commands
========================

All L2CAP commands have the following format (this is also displayed for each command description):

============================= ============ ==============================================================
Name                          Size (bytes) Description
----------------------------- ------------ --------------------------------------------------------------
Opcode                        2
connectionHandle, CID, or PSM 2            Connection Handle, Channel ID, or Protocol/Service Multiplexer
Command PDU                   Variable     Command Parameters
============================= ============ ==============================================================

For the command parameters, please see the corresponding command description below.

Note: The connection handle of 0xFFFE is considered as the loopback connection. All message sent to this connection will be looped back to the local host.

LE Protocol/Service Multiplexer (PSM) values are separated into two ranges:
- Fixed (0x0001 – 0x007F): Values in the first range are assigned by the Bluetooth
SIG and indicate protocols.
- Dynamic (0x0080 – 0x00FF): Values in the second rage are dynamically allocated
and used in conjunction with services defined in the GATT server.

.. include:: /BLE_Vendor_Specific_HCI_Guide/l2cap_cmd_extracted.rst

L2CAP Extension Events
======================

All L2CAP event have the following format (this is also displayed for each event description):

================= ============ =============================
Name              Size (bytes) Description
----------------- ------------ -----------------------------
Opcode            2            PDU operation code
Status            1            Event Status
Connection Handle 2            Connection handle of the link
Event PDU         Variable     Event parameters
================= ============ =============================

For the event parameters, please see the corresponding section below.

.. include:: /BLE_Vendor_Specific_HCI_Guide/l2cap_event_extracted.rst