Introduction
************

The purpose of this document is to describe the Texas Instruments Inc. (TI)
vendor specific Host Controller Interface (HCI) for Bluetooth® low energy (BLE).
This document is intended for customer product software engineers and field
application engineers working with the TI BLE stack software.

Functional Overview
===================

In BLE, there is a logical distinction between the Host software (often referred
to as the higher layer stack) and the Controller software as shown in
:numref:`stack-layers`.

.. _stack-layers:
.. figure:: vsg_resources/stack-layers.png
    :align: center

    BLE Protocol Stack Layers

These components can either exist on the same device (single-device
configuration), or be placed on separate devices (dual-device configuration)
utilizing a Host Controller Interface (HCI) for communication (see section 7 for
more detail). In the single-device configuration, there is obviously only one
device, and the application software would execute on top of the BLE profiles
and stack (see :numref:`single-device`).

.. _single-device:
.. figure:: vsg_resources/single-device.png
    :align: center

    Single Device Configuration

In the dual-device configuration, the application software would also execute
on top of the BLE profiles and stack, and only the controller would be located
on a separate device (see :num_ref:'dual-device'). This configuration is not
supported by the TI BLE-Stack since both the Host and Controller components of
the BLE protocol stack reside on the wireless MCU.

.. _dual-device:
.. figure:: vsg_resources/dual-device.png
    :align: center

    Dual Device Configuration

However, allowing an application to be developed on one device, while
communicating with the BLE stack executing on another, enables access to the
BLE stack that would not normally be available (see
:num_ref:'network-processor').

.. _network-processor:
.. figure:: vsg_resources/network-processor.png
    :align: center

    Network Processor Configuration with HCI

This configuration provides is a very convenient configuration for creating a
test development environment where the “application” is actually a test tool
that can execute scripts, generate logs, etc. Note however that the HCI as
defined by Bluetooth only allows Controller commands and events. As such, a set
of Vendor Specific commands and events will be used instead, and that is what
this document intends to convey.

Numerical Notation Conventions
==============================

Multiple-octets may be specified in hexadecimal notation in one of two ways:

Standard Hexadecimal Notation
-----------------------------

In this notation, a single hexadecimal radix indicator “0x” precedes the entire
value. The octet order as read from left to right is from most significant octet
to least significant octet. For example, for the value 0x123456ABCDEF, ’12’ is
the most significant octet and ‘EF’ is the least significant octet.

Colon Separated Hexadecimal Notation
------------------------------------

In this notation, the hexadecimal radix indicator “0x” is not used and octets
are colon separated. The octet order as read from left to right is from least
significant octet to most significant octet. For example, for the value
12:34:56:AB:CD:EF, ’12’ is the least significant octet and ‘EF’ is the most
significant octet.

Definitions, Abbreviations, Acronyms
====================================

glossary needs to be added for enxt release.

References
==========

1. `Specification of the Bluetooth System, Core Version 4.0, June 30, 2010
<http://www.bluetooth.com/Specification%20Documents/Core_V40.zip>`_.

Revision History
================

2017-10-10: v 4.0: BLE5 V1.1   Added Command for Advertising extension.