HCI_EXT_SetRxGainCmd
--------------------
:Opcode: 0xFC00
:Command Description: Set the receiver gain.

**Command Parameters**

:RX Gain: Set RX gain to standard or high.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     RX Gain Standard
         1                     RX Gain High
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_SetRxGainDone event shall be generated.

HCI_EXT_OnePktPerEvtCmd
-----------------------
:Opcode: 0xFC02
:Command Description: This command is used to configure the Link Layer to only allow one packet per connection event. This command can be used to trade-off throughput and power consumption during a connection. When enabled, power can be conserved during a connection by limiting the number of packets per connection event to one, at the expense of more limited throughput. When disabled, the number of packets transferred during a connection event is not limited, at the expense of higher power consumption. Note that when set, all connections will be restricted to one packet per event.

**Command Parameters**

:Control: Enable or disable allowing only one packet per event.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Disable
         1                     Enable
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_OnePacketPerEventDone event shall be generated.

HCI_EXT_DecryptCmd
------------------
:Opcode: 0xFC05
:Command Description: This command is used to decrypt encrypted text using AES128.

**Command Parameters**

:Key: 128 bit key for the decryption of the data given in the command. The most significant octet of the data corresponds to key[0] using the notation specified in FIPS 197.

 :Size: 16 byte(s)
 :Default: "BF:01:FB:9D:4E:F3:BC:36:D8:74:F5:39:41:38:68:4C"
 :Range: Any 16 byte value

:Data: 128 bit encrypted data to be decrypted. The most significant octet of the key corresponds to key[0] using the notation specified in FIPS 197.

 :Size: 16 byte(s)
 :Default: "66:C6:C2:27:8E:3B:8E:05:3E:7E:A3:26:52:1B:AD:99"
 :Range: Any 16 byte value

**Events Generated**

When this command has completed, an HCI_EXT_DecryptCommandDone event shall be generated.

HCI_EXT_SetLocalSupportedFeaturesCmd
------------------------------------
:Opcode: 0xFC06
:Command Description: This command is used to set the Controllers Local Supported Features. For a complete list of supported LE features, please see [1], Part B, Section 4.6. Note: This command can be issued either before or after one or more connections are formed. However, the local features set in this manner are only effective if performed before a Feature Exchange Procedure has been initiated by the Central. Once this control procedure has been completed for a particular connection, only the exchanged feature set for that connection will be used. Since the Link Layer may initiate the feature exchange procedure autonomously, it is best to use this command before the connection is formed.

**Command Parameters**

:FeatureSet: Write LL local supported features.

 :Size: 8 byte(s)
 :Default: 0x0000000000000001
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x0000000000000000    No Events Specified
         0x0000000000000001    Encryption
         0x0000000000000002    Connection Parameters Request
         0x0000000000000004    Reject Extended Indication
         0x0000000000000008    Peripheral Features Exchange
         0x0000000000000010    Ping
         0x0000000000000020    Data Packet Length Extension
         0x0000000000000040    Privacy
         0x0000000000000080    Extended Scanner Filter Policies
         0x0000000000000100    2M PHY
         0x0000000000000200    Stable Modulation Index Tx
         0x0000000000000400    Stable Modulation Index Rx
         0x0000000000000800    Coded PHY
         0x0000000000001000    Extended Advertising
         0x0000000000002000    Periodic Advertising
         0x0000000000004000    Channel Selection Algorithm #2
         0x0000000000008000    LE Power Class 1
         0x0000000000010000    Minimum Number of Used Channels
         0x0000000000020000    Connection CTE Request
         0x0000000000040000    Connection CTE Response
         0x0000000000080000    Connectionless CTE Transmitter
         0x0000000000100000    Connectionless CTE Receiver
         0x0000000000200000    Antenna Switching During CTE Tx
         0x0000000000400000    Antenna Switching During CTE Rx
         0x0000000000800000    Receiving CTE
         0x0000002000000000    LE Power Control Request 1
         0x0000004000000000    LE Power Control Request 2
         0x0400000000000000    Channel Sounding
         0x0800000000000000    Channel Sounding Host Support
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_WriteLocalFeatureSupportDone event shall be generated.

HCI_EXT_ModemTestTxCmd
----------------------
:Opcode: 0xFC08
:Command Description: This API is used to start a continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel. Use the HCI_EXT_EndModemTest command to end the test. Note: The RF channel, not the BLE frequency, is specified! You can obtain the RF channel from the BLE frequency as follows: RF Channel = (BLE Frequency - 2402) / 2. Note: When the HCI_EXT_EndModemTest is issued to stop this test, a Controller reset will take place. Note: The device will transmit at the default output power (0 dBm) unless changed by HCI_EXT_SetTxPowerCmd. Note: This modem test can be used to satisfy in part radio regulation requirements as specific in standards such as ARIB STD-T66.

**Command Parameters**

:CW Mode: Set Modem Test CW modulation.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Modulated Transmit Carrier
         1                     Unmodulated Transmit Carrier
         ===================== ========================================================

:TX RF Channel: RF channel of transmit frequency.

 :Size: 1 byte(s)
 :Default: 0
 :Range: 0-39

**Events Generated**

When this command has completed, an HCI_EXT_ModemTestTxDone event shall be generated.

HCI_EXT_ModemHopTestTxCmd
-------------------------
:Opcode: 0xFC09
:Command Description: This API is used to start a continuous transmitter direct test mode test using a modulated carrier wave and transmitting a 37 byte packet of pseudo-random 9 bit data. A packet is transmitted on a different frequency (linearly stepping through all RF channels 0..39) every 625us. Use the HCI_EXT_EndModemTest command to end the test. Note: When the HCI_EXT_EndModemTest is issued to stop this test, a Controller reset will take place. Note: The device will transmit at the default output power (0 dBm) unless changed by HCI_EXT_SetTxPowerDbmCmd. Note: This modem test can be used to satisfy in part radio regulation requirements as specific in standards such as ARIB STD-T66.

**Events Generated**

When this command has completed, an HCI_EXT_ModemHopTestTxDone event shall be generated.

HCI_EXT_ModemTestRxCmd
----------------------
:Opcode: 0xFC0A
:Command Description: This API is used to start a continuous receiver modem test using a modulated carrier wave tone, at the frequency that corresponds to the specific RF channel. Any received data is discarded. Receiver gain may be adjusted using the HCI_EXT_SetRxGain command. RSSI may be read during this test by using the HCI_ReadRssi command. Use HCI_EXT_EndModemTest command to end the test. Note: The RF channel, not the BLE frequency, is specified! You can obtain the RF channel from the BLE frequency as follows: RF Channel = (BLE Frequency - 2402) / 2. Note: When the HCI_EXT_EndModemTest is issued to stop this test, a Controller reset will take place. Note: This modem test can be used to satisfy in part radio regulation requirements as specific in standards such as ARIB STD-T66.

**Command Parameters**

:RX RF Channel: RF channel of receive frequency.

 :Size: 1 byte(s)
 :Default: 0
 :Range: 0-39

**Events Generated**

When this command has completed, an HCI_EXT_ModemTestRxDone event shall be generated.

HCI_EXT_EnhancedModemTestTxCmd
------------------------------
:Opcode: 0xFC27
:Command Description:  This API is used start the enhanced BLE5 continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel, for a given PHY (1M, 2M, Coded S2, or Coded S8). Use LL_EXT_EndModemTest to end the test.Note: A Controller reset will be issued by the HCI_EXT_EndModemTest command! Note: The BLE device will transmit at the current TX power setting. Note: This API can be used to verify this device meets Japan's TELEC regulations.

**Command Parameters**

:CW Mode: Set Enhanced Modem Test Tx CW modulation.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Modulated Transmit Carrier
         1                     Unmodulated Transmit Carrier
         ===================== ========================================================

:RF PHY: PHY to transmit on

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  1 Mbps Phy
         0x01                  2 Mbps Phy
         0x02                  Coded S8 Phy (125kpbs)
         0x06                  Coded S2 Phy (500 kbps)
         ===================== ========================================================

:RF Channel: RF channel of transmit frequency.

 :Size: 1 byte(s)
 :Default: 0
 :Range: 0-39

**Events Generated**

When this command has completed, an HCI_EXT_EnhancedModemTestTxDone event shall be generated.

HCI_EXT_EnhancedModemHopTestTxCmd
---------------------------------
:Opcode: 0xFC28
:Command Description:  This API is used to start the enhanced continuous transmitter direct test mode test using a modulated carrier wave. A test reference data packet is transmitted on a different frequency (linearly stepping through all RF channels 0..39), for a given PHY (1M, 2M, Coded S2, or Coded S8), every period (depending on the payload length, as given Vol. 6, Part F, section 4.1.6). Use LL_EXT_EndModemTest to end the test. Note: A Controller reset will be issued by the HCI_EXT_EndModemTest command! Note: The BLE device will transmit at the current TX power setting. Note: This API can be used to verify this device meets Japan's TELEC regulations.

**Command Parameters**

:Payload Length: Data payload length in bytes

 :Size: 1 byte(s)
 :Default: 37
 :Range: 0-37

:Payload Type: DTM Packet Pattern Type

 :Size: 1 byte(s)
 :Default: 0x00
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  PRBS9
         0x01                  0x0F
         0x02                  0x55
         0x03                  PRBS15
         0x04                  0xFF
         0x05                  0x00
         0x06                  0xF0
         0x07                  0xAA
         ===================== ========================================================

:RF PHY: PHY to transmit on

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  1 Mbps Phy
         0x01                  2 Mbps Phy
         0x02                  Coded S8 Phy (125kpbs)
         0x06                  Coded S2 Phy (500 kbps)
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_EnhancedModemHopTestTxDone event shall be generated.

HCI_EXT_EnhancedModemTestRxCmd
------------------------------
:Opcode: 0xFC29
:Command Description:  This API is used to start the enhanced BLE5 continuous receiver modem test using a modulated carrier wave tone, at the frequency that corresponds to the specific RF channel, for a given PHY (1M, 2M, Coded S2, or Coded S8). Any received data is discarded. RSSI may be read during this test by using the LL_ReadRssi command. Use LL_EXT_EndModemTest command to end the test. Note: A Controller reset will be issued by LL_EXT_EndModemTest!

**Command Parameters**

:RF PHY: PHY to transmit on

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  1 Mbps Phy
         0x01                  2 Mbps Phy
         0x02                  Coded S8 Phy (125kpbs)
         0x06                  Coded S2 Phy (500 kbps)
         ===================== ========================================================

:RF Channel: RF Channel

 :Size: 1 byte(s)
 :Default: 0
 :Range: 0 to 39

**Events Generated**

When this command has completed, an HCI_EXT_EnhancedModemTestRxDone event shall be generated.

HCI_EXT_EndModemTestCmd
-----------------------
:Opcode: 0xFC0B
:Command Description: This API is used to end a modem test. A Controller reset will take place.

**Events Generated**

When this command has completed, an HCI_EXT_EndModemTestDone event shall be generated.

HCI_EXT_SetBDADDRCmd
--------------------
:Opcode: 0xFC0C
:Command Description: This command is used to set this devices BLE address (BDADDR). This address will override the devices address determined when the device is reset (i.e. a hardware reset, not an HCI Controller Reset). To restore the devices initialized address, issue this command with an invalid address. Note: This command is only allowed when the Controller is in the Standby state. Note: This command is intended to only be used during initialization. Changing the devices BDADDR after various BLE operations have already taken place may cause unexpected problems.

**Command Parameters**

:BDADDR: BLE Public Address (MSB..LSB). Use "FF:FF:FF:FF:FF:FF" to restore the device address to that which was determined at initialization.

 :Size: 6 byte(s)
 :Default: "00:00:00:00:00:00"
 :Range: Any 6 byte value

**Events Generated**

When this command has completed, an HCI_EXT_SetBDADDRDone event shall be generated.

HCI_EXT_SetVirtualAdvAddrCmd
----------------------------
:Opcode: 0xFC73
:Command Description: This API is used to set the advertiser's virtual public address. Note: This command is only allowed when the advertise set is not active and its PDU type is Legacy Non-Connectable and Non-Scanable.

**Command Parameters**

:Handle: Adv handle to which address will be assigned

 :Size: 1 byte(s)
 :Default: "0"
 :Range: From 0 to 20 sets

:BDADDR: Advertiser's virtual public address

 :Size: 6 byte(s)
 :Default: "00:00:00:00:00:00"
 :Range: Any 6 byte value

**Events Generated**

When this command has completed, an HCI_EXT_SetVirtualAdvAddrDone event shall be generated.

HCI_EXT_SetQOSParameters
------------------------
:Opcode: 0xFC75
:Command Description: This API is used to set the QOS Parameters according to the entered parameter type.

**Command Parameters**

:taskType: The type of task: 0=LL_QOS_CONN_TASK_TYPE, 1=LL_QOS_ADV_TASK_TYPE, 2=LL_QOS_SCN_TASK_TYPE, 3=LL_QOS_INIT_TASK_TYPE, 4=LL_QOS_PERIODIC_ADV_TASK_TYPE, 5=LL_QOS_PERIODIC_SCN_TASK_TYPE.

 :Size: 1 byte(s)
 :Default: "0"
 :Range: From 0 to 5.

:paramType: The type of parameter: 0=LL_QOS_TYPE_PRIORITY, 1=LL_QOS_TYPE_CONN_MIN_LENGTH, 2=LL_QOS_TYPE_CONN_MAX_LENGTH. 

 :Size: 1 byte(s)
 :Default: "0"
 :Range: From 0 to 2: LL_QOS_TYPE_PRIORITY, LL_QOS_TYPE_CONN_MIN_LENGTH, LL_QOS_TYPE_CONN_MAX_LENGTH.

:ParamVal: The parameter value. For LL_QOS_TYPE_PRIORITY: 0=Low, 1=Medium, 2=High. For LL_QOS_TYPE_CONN_MIN_LENGTH/LL_QOS_TYPE_CONN_MAX_LENGTH: time in [us].

 :Size: 4 byte(s)
 :Default: "0"
 :Range: For LL_QOS_TYPE_PRIORITY: LL_QOS_LOW_PRIORITY (=0), LL_QOS_MED_PRIORITY (=1), LL_HIGH_LOW_PRIORITY (=2). For LL_QOS_TYPE_CONN_MIN_LENGTH: For coded connection the range LL_MIN_LINK_DATA_TIME_CODED (2704 us) - LL_MAX_LINK_DATA_TIME_CODED (17040 us).For uncoded connection the range LL_MIN_LINK_DATA_TIME (328 us) - LL_MAX_LINK_DATA_TIME_UNCODED (2120 us). For LL_QOS_TYPE_CONN_MAX_LENGTH: For coded connection the range LL_MIN_LINK_DATA_TIME_CODED (2704 us) - connection's interval (us). For uncoded connection the range LL_MIN_LINK_DATA_TIME (328 us) - connection's interval. 

:taskHandle: The task handle to be changed (secondary and primary tasks). For connection enter the connection's Id.

 :Size: 2 byte(s)
 :Default: "0"
 :Range: From 0 to 20

**Events Generated**

When this command has completed, an HCI_EXT_SetQOSParametersDone event shall be generated.

HCI_EXT_SetQOSDefaultParameters
-------------------------------
:Opcode: 0xFC76
:Command Description: This API is used to set the default QOS Parameters values.

**Command Parameters**

:paramDefaultVal: The parameter default value. For LL_QOS_TYPE_PRIORITY: 0=Low, 1=Medium, 2=High.

 :Size: 4 byte(s)
 :Default: "0"
 :Range: For LL_QOS_TYPE_PRIORITY: LL_QOS_LOW_PRIORITY (=0), LL_QOS_MED_PRIORITY (=1), LL_HIGH_LOW_PRIORITY (=2).

:paramType: The type of parameter: 0=LL_QOS_TYPE_PRIORITY

 :Size: 1 byte(s)
 :Default: "0"
 :Range: From 0 to 0: LL_QOS_TYPE_PRIORITY

:taskType: The type of task: 0=LL_QOS_CONN_TASK_TYPE, 1=LL_QOS_ADV_TASK_TYPE, 2=LL_QOS_SCN_TASK_TYPE, 3=LL_QOS_INIT_TASK_TYPE, 4=LL_QOS_PERIODIC_ADV_TASK_TYPE, 5=LL_QOS_PERIODIC_SCN_TASK_TYPE.

 :Size: 1 byte(s)
 :Default: "0"
 :Range: From 0 to 5

**Events Generated**

When this command has completed, an HCI_EXT_SetQOSDefaultParameters event shall be generated.

HCI_EXT_SetHostDefChanClassificationCmd
---------------------------------------
:Opcode: 0xFC79
:Command Description: This API is used to set the default channel map to use in future connections.

**Command Parameters**

:Channel Map: The channel map to set as default. bit map for each channel. 1 to use channel, 0 to not use.

 :Size: 5 byte(s)
 :Default: "00:00:00:00:01"
 :Range: Any 6 byte value, will use only 37 LSb, one for each channel.

**Events Generated**

When this command has completed, an HCI_EXT_SetHostDefChanClassificationCmd event shall be generated.

HCI_EXT_SetHostConnChanClassificationCmd
----------------------------------------
:Opcode: 0xFC7A
:Command Description: This API is used to set the channel map of a specific active connection.

**Command Parameters**

:Channel Map: The channel map to set as default. bit map for each channel. 1 to use channel, 0 to not use.

 :Size: 5 byte(s)
 :Default: "00:00:00:00:01"
 :Range: Any 6 byte value, will use only 37 LSb, one for each channel.

:Handle: Local identifier of the LL connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0x0EFF

**Events Generated**

When this command has completed, an HCI_EXT_SetHostConnChanClassificationCmd event shall be generated.

HCI_EXT_Send_Power_Control_Request
----------------------------------
:Opcode: 0xFC7C
:Command Description: This API is used to trigger the power control procedure and send the power control request packet.

**Command Parameters**

:Connection Handle: Local identifier of the LL connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0xFFFD

:Requested PHY: Phy on which the command is triggered for

 :Size: 1 byte(s)
 :Default: 0x1
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x1                   LE 1M PHY
         0x2                   LE 2M PHY
         0x3                   LE Coded PHY with S=8 data coding
         0x4                   LE Coded PHY with S=2 data coding
         0xC                   LE Coded PHY with S=2 and S=8 data coding
         ===================== ========================================================

:Delta Power dB: The amount of power the peer device need to decrease or increase in dB units

 :Size: 1 byte(s)
 :Default: 0x0
 :Range: -127 to 126

:APR Enable: Flag to enable the APR

 :Size: 1 byte(s)
 :Default: 0x0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x0                   APR disable
         0x1                   APR enable
         ===================== ========================================================

:HCI_Command_Status_Event: HCI Command Status Event with the status of the command.

 :Size: 1 byte(s)
 :Default: HCI_EXT_Send_Power_Control_Request
 :Range: HCI Command Status Event

**Events Generated**

When this command is completed, an LE Transmit Power Reporting event shall be generated.

HCI_EXT_SetDefaultAntennaCmd
----------------------------
:Opcode: 0xFC7D
:Command Description: This API is used to set a default antenna for regular BLE communications.

**Command Parameters**

:Index: Index of the antenna to be set as default.

 :Size: 1 byte(s)
 :Default: 0x00
 :Range: 0x00 to 0x03

**Events Generated**

When this command is completed, an HCI_EXT_SetDefaultAntennaDone event shall be generated.

HCI_EXT_RssiMon_RegCmd
----------------------
:Opcode: 0xFC35
:Command Description: This API registers an RSSI monitoring command for a specific connection.

**Command Parameters**

:Connection Handle: Local identifier of the LL connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0xEFFF

:Low rssi threshold: Lowest allowed rssi value before triggering this calllback

 :Size: 1 byte(s)
 :Default: 0x0
 :Range: -127 to 20

:High rssi threshold: Highest allowed rssi value before triggering this calllback

 :Size: 1 byte(s)
 :Default: 0
 :Range: -127 to 20

**Events Generated**

When this command has completed, an HCI_EXT_RssiMon_RegCmdDone event shall be generated.

HCI_EXT_RssiMon_UnregCmd
------------------------
:Opcode: 0xFC36
:Command Description: This API unregisters an RSSI monitoring command for a specific connection.

**Command Parameters**

:Register Handle: Local identifier handle for the rssi monitor callback

 :Size: 1 byte(s)
 :Default: 0x00
 :Range: 0x00 to 0xFF

**Events Generated**

When this command has completed.

HCI_EXT_RssiMon_SetConfigCmd
----------------------------
:Opcode: 0xFC37
:Command Description: This API sets the configuration for the RSSI monitoring command.

**Command Parameters**

:Income rssi monitor weight: Weight of the income rssi value to be used in the rssi statistic calculation

 :Size: 1 byte(s)
 :Default: 0x1
 :Range: 0x1 to 0xFF

:Minimum number of rssi samples: Minmium number of rssi samples that after this amount the rssi statistic is valid

 :Size: 1 byte(s)
 :Default: 0xA
 :Range: 0x1 to 0xFF

**Events Generated**

When this command has completed

HCI_EXT_RssiMon_GetConfigCmd
----------------------------
:Opcode: 0xFC38
:Command Description: This API gets the configuration for the RSSI monitoring command.

**Events Generated**

When this command has completed, an HCI_EXT_RssiMon_GetConfigCmdDone event shall be generated.

HCI_EXT_RssiMon_GetRssiStatCmd
------------------------------
:Opcode: 0xFC39
:Command Description: This API gets the RSSI statistics for a specific connection.

**Command Parameters**

:Connection Handle: Local identifier of the LL connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0xEFFF

**Events Generated**

When this command has completed, an HCI_EXT_RssiMon_GetRssiStatCmdDone event shall be generated.

HCI_EXT_SetSCACmd
-----------------
:Opcode: 0xFC0D
:Command Description: This command is used to set this devices Sleep Clock Accuracy (SCA) value, in parts per million (PPM), from 0 to 500. For a Central device, the value is converted to one of eight ordinal values representing a SCA range (per [1], Volume 6, Part B, Section 2.3.3.1, Table 2.2), which will be used when a connection is created. For a Peripheral device, the value is directly used. The system default value for a Central and Peripheral device is 50ppm and 40ppm, respectively. Note: This command is only allowed when the device is not in a connection. Note: The devices SCA value remains unaffected by an HCI Reset.

**Command Parameters**

:SCA: BLE Device Sleep Clock Accuracy (PPM).

 :Size: 2 byte(s)
 :Default: "40"
 :Range: (0..500)

**Events Generated**

When this command has completed, an HCI_EXT_SetSCADone event shall be generated.

HCI_EXT_EnablePTMCmd
--------------------
:Opcode: 0xFC0E
:Command Description: This command is used to enable Production Test Mode (PTM). This mode is used by the customer during assembly of their product to allow limited access to the BLE Controller for testing and configuration. This command is only available when the BLE Controller is built without external access to the Controller (i.e. when no transport interface such as RS232 is permitted). This mode will remain enabled until the device is reset. Please see the related application note for additional details. Note: This command is only allowed as a direct function call, and is only intended to be used by an embedded application. No vendor specific Command Complete event will be generated.

**Events Generated**

When this command has completed, will simply return. No vendor specific Command Complete event will be generated.

HCI_EXT_DisconnectImmedCmd
--------------------------
:Opcode: 0xFC13
:Command Description: This command is used to disconnect a connection immediately. This command can be useful for when a connection needs to be ended without the latency associated with the normal BLE Controller Terminate control procedure. Note that the Host issuing the command will still receive the HCI Disconnection Complete event with a Reason status of 0x16 (i.e. Connection Terminated by Local Host), followed by an HCI Vendor Specific Event.

**Command Parameters**

:Connection Handle: Handle used to identify a connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0x0EFF

**Events Generated**

When this command has completed, an HCI_EXT_DisconnectImmedDone event shall be generated.

HCI_EXT_PacketErrorRateCmd
--------------------------
:Opcode: 0xFC14
:Command Description: This command is used to Reset or Read the Packet Error Rate counters for a connection. When Reset, the counters are cleared; when Read, the total number of packets received, the number of packets received with a CRC error, the number of events, and the number of missed events are returned. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended.

**Command Parameters**

:Connection Handle: Handle used to identify a connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0x0EFF

:PER Test Command: Reset or Read the PER counters.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Reset PER Counters
         1                     Read PER Counters
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_PER event shall be generated.

HCI_EXT_SetPeripheralLatencyOverrideCmd
---------------------------------------
:Opcode: 0xFC1A
:Command Description: This command is used to enable or disable the Peripheral Latency Override, allowing the user to ensure that Peripheral Latency is not applied even though it is active. The default value is Disable. Note: This command will be disallowed for no connection, or the connection is not in the Peripheral role.

**Command Parameters**

:Control: Enable or disable suspending peripheral latency.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Disable
         1                     Enable
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_OverridePLDone event shall be generated.

HCI_EXT_BuildRevisionCmd
------------------------
:Opcode: 0xFC1B
:Command Description: This command is used to a) allow the embedded user code to set their own 16 bit revision number, and b) to read the build revision number of the BLE stack library software. The default value of the user revision number is zero. When the user updates a BLE project by adding their own code, they may use this API to set their own revision number. When called with mode set to HCI_EXT_SET_APP_REVISION, the stack will save this value. No event will be returned from this API when used this way as it is intended to be called from within the target itself. Note however that this does not preclude this command from being received via the HCI. However, no event will be returned. When this API is used from the HCI, then the second parameter is ignored, and a vendor specific event is returned with the users revision number and the build revision number of the BLE stack.

**Command Parameters**

:Mode: Set User Revision or Get Build Revision.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Set User Revision Number
         1                     Read Build Revision
         ===================== ========================================================

:UserRevNum: User Revision Number.

 :Size: 2 byte(s)
 :Default: 0
 :Range: Any 16 bit value

**Events Generated**

When this command has completed, an HCI_EXT_BuildRevisionDone event shall be generated but only when the value of mode is HCI_EXT_READ_BUILD_REVISION.

HCI_EXT_ResetSystemCmd
----------------------
:Opcode: 0xFC1D
:Command Description: This command is used to issue a hard or soft system reset. A hard reset is caused by setting the SYSRESET bit in the System Controller Reset Control register. The soft reset is currently not supported on the CC264x.

**Command Parameters**

:type: Reset Type

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  Chip Reset  
         0x01                  Soft Reset  
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_ResetSystemDone event shall be generated.

HCI_EXT_NumComplPktsLimitCmd
----------------------------
:Opcode: 0xFC1F
:Command Description: This command is used to set the limit on the minimum number of complete packets before a Number of Completed Packets event is returned by the Controller. If the limit is not reached by the end of a connection event, then the Number of Completed Packets event will be returned (if non-zero) based on the flushOnEvt flag. The limit can be set from one to the maximum number of HCI buffers (please see the LE Read Buffer Size command in the Bluetooth Core specification). The default limit is one; the default flushOnEvt flag is FALSE.

**Command Parameters**

:Limit: Set Number of Completed Packets Limit.

 :Size: 1 byte(s)
 :Default: 1
 :Range: 0x01 to the value returned from HCI_LE_ReadBufSizeCmd

:flushOnEvt: Enable or disable flush of Number of Completed Packets at end of Event.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Disable
         1                     Enable
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_NumComplPktsLimitDone event shall be generated.

HCI_EXT_GetConnInfoCmd
----------------------
:Opcode: 0xFC20
:Command Description: This command (which replaces Get Number Connections) is used to get the number of allocated connections, the number of active connections, and for each active connection, the connection handle, the connection role, the peer device address and peer device address type. The number of allocated connections is based on a default build value that can be changed in the project using MAX_NUM_BLE_CONNS (please see the software users guide for additional details). The number of active connections refers to active BLE connections. The information per connection is based on the structure hciConnInfo_t provided in hci.h. If all parameters are NULL, then the call to this command is considered a network processor call via a transport layer, and the results will be provided via a vendor specific command complete event.If any parameter is not NULL, then the call to this command is considered a direct function call and the valid pointers will be used to store the result. In this case, it is the users responsibility to ensure there is sufficient memory allocated! Note that partial results can be obtained by selective use of the pointers. For example, if only the number of active connections is desired, this can be obtained as follows:

**Events Generated**

When this command has completed, an HCI_EXT_GetConnInfoDone event shall be generated.

HCI_EXT_SetMaxDataLenCmd
------------------------
:Opcode: 0xFC21
:Command Description: This command is used to set the Data Length Extension internal variables supportedMaxTxOctets, supportedMaxTxTime, supportedMaxRxOctets and supportedMaxRxTime that are normally set exclusively by the Controller to the maximum data length and duration allowed by this device (default Tx and Rx Octets is 251; default Tx and Rx Time is 2120 us [but note that any future change to support PHYs could alter the default values of Time]). 

**Command Parameters**

:Tx Octets: Maximum number of payload octets that the local Controller supports for transmission of a single Link Layer Data Channel PDU.

 :Size: 2 byte(s)
 :Default: 0
 :Range: 0x001B to 0x00FB

:Tx Time: Maximum time, in microseconds, that the local Controller supports for transmission of a single Link Layer Data Channel PDU.

 :Size: 2 byte(s)
 :Default: 0
 :Range: 0x0148 to 0x0848

:Rx Octets: Maximum number of payload octets that the local Controller supports for reception of a single Link Layer Data Channel PDU.

 :Size: 2 byte(s)
 :Default: 0
 :Range: 0x001B to 0x00FB

:Rx Time: Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer Data Channel PDU.

 :Size: 2 byte(s)
 :Default: 0
 :Range: 0x0148 to 0x0848

**Events Generated**

When this command has completed, an HCI_EXT_SetMaxDataLengthDone event shall be generated.

HCI_EXT_SetDtmTxPktCntCmd
-------------------------
:Opcode: 0xFC24
:Command Description: This API is used to set the DTM TX packet count.

**Command Parameters**

:TX Packet Count: Number of DTM packets to transmit

 :Size: 2 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x0000                Continuous Tx
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_SetDtmTxPktCntDone event shall be generated.

HCI_EXT_SetPinOutputCmd
-----------------------
:Opcode: 0xFC2A
:Command Description: This API is used to set GPIO as output.

**Command Parameters**

:Pin: Pin Number

 :Size: 1 byte(s)
 :Default: 0
 :Range: 0x00 to 0x1F

:Value: initialize value 0 or 1

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x00                  Output Low 
         0x01                  Output High
         0xFF                  Input
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_SetPinOutputDone event shall be generated.

HCI_EXT_SetLocationingAccuracyCmd
---------------------------------
:Opcode: 0xFC2B
:Command Description: This API is used to set CTE accuracy.

**Command Parameters**

:handle: connection handle (0x0XXX) or periodic advertising train handle (0x1XXX)

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0x1EFF

:CTE PHY: Indicate which PHY to configure.

 :Size: 0 byte(s)
 :Default: 0x01
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  LE 1M
         0x02                  LE 2M
         ===================== ========================================================

:1M:sample rate: Accuracy between 1 (least accuracy as in 5.1 spec) to 4 (most accuracy)

 :Condition: ( (phyMask & 0x1) == 0x01)
 :Size: 1 byte(s)
 :Default: 1
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  1us AoD transmission
         0x02                  1us AoD reception
         0x04                  1us AoA reception
         ===================== ========================================================

:1M:sample size: Size 8 bits (as in 5.1 spec) or 16 bits (more accurate)

 :Condition: ( (phyMask & 0x1) == 0x01)
 :Size: 1 byte(s)
 :Default: 1
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  8 bits 
         0x02                  16 bits
         ===================== ========================================================

:1M:sample rate: 

 :Condition: ( (phyMask & 0x1) != 0x01)
 :Size: 1 byte(s)
 :Value: 0

:1M:sample size: 

 :Condition: ( (phyMask & 0x1) != 0x01)
 :Size: 1 byte(s)
 :Value: 0

:2M:sample rate: Accuracy between 1 (least accuracy as in 5.1 spec) to 4 (most accuracy)

 :Condition: ( (phyMask & 0x2) == 0x02)
 :Size: 1 byte(s)
 :Default: 1
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  1us AoD transmission
         0x02                  1us AoD reception
         0x04                  1us AoA reception
         ===================== ========================================================

:2M:sample size: Size 8 bits (as in 5.1 spec) or 16 bits (more accurate)

 :Condition: ( (phyMask & 0x2) == 0x02)
 :Size: 1 byte(s)
 :Default: 1
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0x01                  8 bits 
         0x02                  16 bits
         ===================== ========================================================

:2M:sample rate: 

 :Condition: ( (phyMask & 0x2) != 0x02)
 :Size: 1 byte(s)
 :Value: 0

:2M:sample size: 

 :Condition: ( (phyMask & 0x2) != 0x02)
 :Size: 1 byte(s)
 :Value: 0

:sample control: 0x00-default filtering(skip antenna switching samples, ...), 0x01-RAW_RF no filtering

 :Size: 1 byte(s)
 :Default: 0x00
 :Range: 0x00 to 0x01

**Events Generated**

When this command has completed, an HCI_EXT_SetLocationingAccuracyDone event shall be generated.

HCI_EXT_GetActiveConnInfoCmd
----------------------------
:Opcode: 0xFC2C
:Command Description: This API is used to get connection information needed to track an active BLE connection.

**Command Parameters**

:connId: 

 :Size: 1 byte(s)
 :Default: 0
 :Range: 0x0000 to 0x0EFF

**Events Generated**

When this command has completed, an HCI_EXT_GetActiveConnInfoDone event shall be generated.

HCI_EXT_CoexEnableCmd
---------------------
:Opcode: 0xFC2E
:Command Description: This API is used to enable or disable the Coex feature.

**Command Parameters**

:Enable: 1 for enable and 0 for disable

 :Size: 1 byte(s)
 :Default: 1
 :Range: 0x00 to 0x01

**Events Generated**

When this command has completed, an HCI_EXT_CoexEnableDone event shall be generated.

HCI_EXT_SetTxPowerDbmCmd
------------------------
:Opcode: 0xFC2F
:Command Description: This command is used to set the RF transmitter output power value in dBm.

**Command Parameters**

:dBm: Tx power to use.

 :Size: 1 byte(s)
 :Default: 0
 :Range: -127 to 20

:fraction: Tx power fraction (0.5 dBm).

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         False                 
         True                  
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_SetTxPowerDone event shall be generated.

HCI_EXT_SetMaxDtmTxPowerDbmCmd
------------------------------
:Opcode: 0xFC30
:Command Description: This command is used to override the RF transmitter output power used by the Direct Test Mode (DTM). Normally, the maximum transmitter output power setting used by DTM is the maximum transmitter output power setting for the device. This command will change the value used by DTM. Note: When DTM is ended by a call to HCI_LE_TestEndCmd, or a HCI_Reset is used, the transmitter output power setting is restored to the default value of 0 dBm.

**Command Parameters**

:dBm: Tx power to use.

 :Size: 1 byte(s)
 :Default: 0
 :Range: -127 to 20

:fraction: Tx power fraction (0.5 dBm).

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         False                 
         True                  
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_SetMaxDtmTxPowerDone event shall be generated.

HCI_EXT_GetRxStatisticsCmd
--------------------------
:Opcode: 0xFC31
:Command Description: This command is used to Reset or Read the RX statistics counters for a connection. When Reset, the counters are cleared; when Read, the total number of ok packets received, the number of control packets received, the number of control packets received that were ACKed, the number of packets received with a CRC error, the number of packets that were ignored, the number of empty packets that were received, and the number of discarded packets are returned. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended.

**Command Parameters**

:Connection Handle: Handle used to identify a connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0x0EFF

:RX Stats Test Command: Reset or Read the RX statistics counters.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Reset Statistics Counters
         1                     Read Statistics Counters
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_GET_RX_STATS event shall be generated.

HCI_EXT_GetTxStatisticsCmd
--------------------------
:Opcode: 0xFC32
:Command Description: This command is used to Reset or Read the RX statistics counters for a connection. When Reset, the counters are cleared; when Read, the total number of ok packets transmitted, the number of transmitted packets ACKed, the number of control packets transmitted, the number of control packets transmitted ACKed, the number of control packets transmitted ACKed that were ACKed, the number of  packets retransmissions, and the number of packets on Tx queue that are finished. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended.

**Command Parameters**

:Connection Handle: Handle used to identify a connection

 :Size: 2 byte(s)
 :Default: 0x0000
 :Range: 0x0000 to 0x0EFF

:TX Stats Test Command: Reset or Read the TX statistics counters.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Reset Statistics Counters
         1                     Read Statistics Counters
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_GET_TX_STATS event shall be generated.

HCI_EXT_GetCoexStatisticsCmd
----------------------------
:Opcode: 0xFC33
:Command Description: This command is used to Reset or Read the COEX statistics counters for a connection. When Reset, the counters are cleared; when Read, the total number of grants (CC33xx: grants_asserted), the total number of rejects (CC33xx: request_deassrted), the total number of continuously rejected requests (CC33xx: grants_deasserted), and the number of max continuously rejected requests (CC33xx: request_assrted). The system default value upon hardware reset is Reset.

**Command Parameters**

:Coex Stats Test Command: Reset or Read the Coex statistics counters.

 :Size: 1 byte(s)
 :Default: 0
 :Range:
         ===================== ========================================================
         Value                 Description
         ===================== ========================================================
         0                     Reset Statistics Counters
         1                     Read Statistics Counters
         ===================== ========================================================

**Events Generated**

When this command has completed, an HCI_EXT_GET_COEX_STATS event shall be generated.

HCI_EXT_HostToControllerCmd
---------------------------
:Opcode: 0xFC34
:Command Description: This API is used to send the controller a raw HCI packet.

**Command Parameters**

:HciPacketLength: The hci packet length.

 :Size: 2 byte(s)
 :Default: 4
 :Range: 4 to 255

:HciPacket: The raw hci packet.

 :Size: pktLen byte(s)
 :Default: "01:03:0c:00"
 :Range: Any value

**Events Generated**

When this command has completed the corrsponding event shall be generated.