************************
GATT Vendor Specific API
************************

GATT Commands
=============

All GATT commands have the following format:

================= ============ =============================
Name              Size (bytes) Description
----------------- ------------ -----------------------------
Opcode            2            PDU operation code
Connection Handle 2            Connection handle of the link
Command PDU       Variable     Command Parameters
================= ============ =============================

For the command parameters, please see the corresponding section below.

Note: The connection handle of 0xFFFE is considered as the loopback connection.
All messages sent to this connection will be loop backed to the local host.

**Events Generated**

For each GATT command,when it is received, the host will send the CommandStatus
Event with the Status parameter.  If a command will return additional
events, it will be noted in the description below.

.. include:: /BLE_Vendor_Specific_HCI_Guide/gatt_cmd_extracted.rst

GATT Events
===========

All GATT events have the following format:

================= ============ =============================
Name              Size (bytes) Description
----------------- ------------ -----------------------------
Opcode            2            PDU operation code
Status            1            Event status
Connection Handle 2            Connection handle of the link
PDU length        1            Length of event PDU
Event PDU         Variable     Event parameters
================= ============ =============================

For the event parameters, please see the corresponding section below.

Note: The connection handle of 0xFFFE is considered as the loopback connection.
All messages sent to this connection will be loop backed to the local host.

.. include:: /BLE_Vendor_Specific_HCI_Guide/gatt_event_extracted.rst