UTIL_NV_Read

Opcode:

0xFE81

Command Description:

Send this command to read an NV parameter.

Command Parameters

nvID:
Size:

2 byte(s)

Default:

0

Range:

Any 2-byte value

nvLen:
Size:

1 byte(s)

Default:

0

Range:

Any 1-byte value

Events Generated

When this command is received, the host will send the CommandStatus Event.

UTIL_NV_Write

Opcode:

0xFE82

Command Description:

Send this command to write an NV parameter.

Command Parameters

nvID:
Size:

2 byte(s)

Default:

0

Range:

Any 2-byte value

nvDataLen:

Size of NV data

Size:

1 byte(s)

Value:

size(nvData)

nvData:

NV Data Field. Structure can be different for each NV item

Size:

input byte(s)

Default:

“00”

Range:

Any 1-byte value

Events Generated

When this command is received, the host will send the CommandStatus Event.

UTIL_ForceBoot

Opcode:

0xFE83

Command Description:

Force the boot loader to run.

Events Generated

When this command is received, the device resets if the boot loader is present. Otherwise, the host will send the CommandStatus Event.

UTIL_BuildRevision

Opcode:

0xFE84

Command Description:

This command is used to read the build revision information of the BLE stack software.

Events Generated

When this command is received, the host will send the CommandStatus Event.

Additional Command Status Return Parameters

dataLen:
Size:

1 byte(s)

Range:

stk ver (mj/mn/ph):
Condition:

( StatStatus==0x00)

Size:

3 byte(s)

Range:

bld ver:
Condition:

( StatStatus==0x00)

Size:

2 byte(s)

Range:

stk info:
Condition:

( StatStatus==0x00)

Size:

1 byte(s)

Range:

Value

Description

0x01

IARProject

0x02

CCSProject

0x10

IARLibrary

0x80

ROMBuild

ctrl info:
Condition:

( StatStatus==0x00)

Size:

2 byte(s)

Range:

Value

Description

0x01

ADV_NCONN

0x02

ADV_CONN

0x04

SCAN

0x08

INIT

0x10

PING

0x20

SLV_FEAT_EXCHG

0x40

CONN_PARAM_REQ

host info:
Condition:

( StatStatus==0x00)

Size:

2 byte(s)

Range:

Value

Description

0x01

BROADCASTER

0x02

OBSERVER

0x04

PERIPHERAL

0x08

CENTRAL

UTIL_GetMemStats

Opcode:

0xFE87

Command Description:

Get memory statistics

Command Parameters

command ID:
Size:

1 byte(s)

Default:

2

Range:

Value

Description

0x01

Light Heap Statistic

0x02

Full Heap Statistic (requieres HEAPMGR_METRICS)

0x04

Thread usage Statistic (requieres HEAPMGR_METRICS)

Events Generated

When this command is received, the host will send the CommandStatus Event.

Additional Command Status Return Parameters

dataLen:
Size:

1 byte(s)

Range:

:all cmdID receive :

Size:

1 byte(s)

Range:

Value

Description

0x01

Light Heap Statistic

0x02

Full Heap Statistic (requieres HEAPMGR_METRICS)

0x04

Thread usage Statistic (requieres HEAPMGR_METRICS)

cmdID:
Condition:

( (cmdID & 0x01) == 0x01)

Size:

1 byte(s)

Range:

Value

Description

0x01

Light Heap Statistic

0x02

Full Heap Statistic (requieres HEAPMGR_METRICS)

0x04

Thread usage Statistic (requieres HEAPMGR_METRICS)

Heap Size:
Condition:

( (cmdID & 0x01) == 0x01)

Size:

4 byte(s)

Range:

Heap Size Free:
Condition:

( (cmdID & 0x01) == 0x01)

Size:

4 byte(s)

Range:

Biggest free buffer Available:
Condition:

( (cmdID & 0x01) == 0x01)

Size:

4 byte(s)

Range:

cmdID:
Condition:

( (cmdID & 0x02) == 0x02)

Size:

1 byte(s)

Range:

Value

Description

0x01

Light Heap Statistic

0x02

Full Heap Statistic (requieres HEAPMGR_METRICS)

0x04

Thread usage Statistic (requieres HEAPMGR_METRICS)

Heap Fail number:
Condition:

( (cmdID & 0x02) == 0x02)

Size:

2 byte(s)

Range:

Heap Allocated:
Condition:

( (cmdID & 0x02) == 0x02)

Size:

4 byte(s)

Range:

Heap Max Allocated:
Condition:

( (cmdID & 0x02) == 0x02)

Size:

4 byte(s)

Range:

cmdID:
Condition:

( (cmdID & 0x04) ==0x04)

Size:

1 byte(s)

Range:

Value

Description

0x01

Light Heap Statistic

0x02

Full Heap Statistic (requieres HEAPMGR_METRICS)

0x04

Thread usage Statistic (requieres HEAPMGR_METRICS)

Number of Thread:
Condition:

( (cmdID & 0x04) ==0x04)

Size:

1 byte(s)

Range:

An array of size “Count” will be returned containing the parameters starting here:

Priority:
Condition:

( (cmdID & 0x04) ==0x04)

Size:

1 byte(s)

Range:

Handle:
Condition:

( (cmdID & 0x04) ==0x04)

Size:

2 byte(s)

Range:

max Stack used:
Condition:

( (cmdID & 0x04) ==0x04)

Size:

2 byte(s)

Range:

stack size:
Condition:

( (cmdID & 0x04) ==0x04)

Size:

2 byte(s)

Range:

The array of parameters ends here.