L2CAP Extension Vendor Specific API¶
L2CAP Extension Commands¶
All L2CAP commands have the following format (this is also displayed for each command description):
Name |
Size (bytes) |
Description |
Opcode |
2 |
|
connectionHandle, CID, or PSM |
2 |
Connection Handle, Channel ID, or Protocol/Service Multiplexer |
Command PDU |
Variable |
Command Parameters |
For the command parameters, please see the corresponding command description below.
Note: The connection handle of 0xFFFE is considered as the loopback connection. All message sent to this connection will be looped back to the local host.
LE Protocol/Service Multiplexer (PSM) values are separated into two ranges: - Fixed (0x0001 – 0x007F): Values in the first range are assigned by the Bluetooth SIG and indicate protocols. - Dynamic (0x0080 – 0x00FF): Values in the second rage are dynamically allocated and used in conjunction with services defined in the GATT server.
L2CAP_SendData¶
- Opcode:
0xFCF0
- Command Description:
The L2CAP Data command is used to send an SDU on a Connection Oriented Channel established with the peer device.
Command Parameters
- Layer:
- Size:
1 byte(s)
- Value:
9
- Event Opcode:
- Size:
2 byte(s)
- Value:
0xFCF0
- Payload Length(including CID):
- Size:
2 byte(s)
- Value:
size(dataLen)+size(cid)+size(connHandle)
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- CID:
Local Channel ID
- Size:
2 byte(s)
- Default:
0x0040
- Range:
0x0040 - 0x007F
- SDU:
SDU to be sent on the channel
- Size:
input byte(s)
- Default:
“”
- Range:
to L2CAP_SDU_SIZE octets
Events Generated
When this command is received, the host will send the CommandStatus Event. When the SDU transmission is done to the peer device, the L2CAP Send SDU Done Event (L2CAP_SendSduDone) will be generated. If the local channel runs out of credits required to send the SDU, the L2CAP Out of Credit Event (L2CAP_OutOfCredit) will be generated.
L2CAP_RegisterPsm¶
- Opcode:
0xFCF1
- Command Description:
The L2CAP Register PSM command is used to register a Protocol/Service Multiplexer (PSM) with the L2CAP layer.
Command Parameters
- PSM:
Local Protocol/Service Multiplexer (PSM)
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0x00FF
- MTU:
Maximum SDU size that can be received by PSM
- Size:
2 byte(s)
- Default:
0x0017
- Range:
Any 2 byte value
- initialPeerCredits:
Number of packets that peer device can send to local device
- Size:
2 byte(s)
- Default:
0x0001
- Range:
Any 2 byte value
- peerCreditThreshold:
Low threshold for peer credits
- Size:
2 byte(s)
- Default:
0x0000
- Range:
Any 2 byte value
- maxNumChannels:
Maximum number of Connection Oriented Channels supported by PSM
- Size:
1 byte(s)
- Default:
0x01
- Range:
Any 1 byte value
- enableSecurityVerification:
Indicates whether to enable security verification by the application for any incoming connection request
- Size:
1 byte(s)
- Default:
0x00
- Range:
Value
Description
0x00
No
0x01
Yes
Events Generated
When this command is received, the local device will send the CommandStatus Event. If the application wishes to perform its own security verification (by setting enableSecurityVerification to TRUE) for any incoming connection request then an L2CAP Connection Request (L2CAP_ConnectReq) event will be sent up to the application, which must then send an L2CAP Connection Response (L2CAP_ConnectRsp) command back. When the peer credit count reaches the peer credit threshold (specified by peerCreditThreshold), the L2CAP Peer Credit Threshold Event (L2CAP_PeerCreditThreshold) will be generated.
L2CAP_DeregisterPsm¶
- Opcode:
0xFCF2
- Command Description:
The L2CAP Deregister PSM command is sent to deregister a Protocol/Service Multiplexer (PSM) with the L2CAP layer.
Command Parameters
- PSM:
Local Protocol/Service Multiplexer (PSM) to be deregistered with L2CAP
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0x00FF
Events Generated
When this request is received, the local device will send the CommandStatus Event.
L2CAP_PsmInfo¶
- Opcode:
0xFCF3
- Command Description:
The L2CAP PSM Info command is used to get the current information about a given PSM registered with the L2CAP layer.
Command Parameters
- PSM:
Local Protocol/Service Multiplexer (PSM)
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0x00FF
Events Generated
When this request is received, the local device will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen:
- Size:
1 byte(s)
- Range:
- MTU:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- MPS:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- initialPeerCredits:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerCreditThreshold:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- maxNumChannels:
- Condition:
( StatStatus==0x00)
- Size:
1 byte(s)
- Range:
- numActiveChannels:
- Condition:
( StatStatus==0x00)
- Size:
1 byte(s)
- Range:
L2CAP_PsmChannels¶
- Opcode:
0xFCF4
- Command Description:
The L2CAP PSM Channels command is used to get the list of all the active Connection Oriented Channels for a given PSM registered with the L2CAP layer.
Command Parameters
- PSM:
Local Protocol/Service Multiplexer (PSM)
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0x00FF
Events Generated
When this request is received, the local device will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen:
- Size:
1 byte(s)
- Range:
An array of size “dataLen/4” will be returned containing the parameters starting here:
- connHandle:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- CID:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
The array of parameters ends here.
L2CAP_ChannelInfo¶
- Opcode:
0xFCF5
- Command Description:
The L2CAP Channel Info command is used to get the current information about an active Connection Oriented Channel.
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- CID:
Local Channel ID
- Size:
2 byte(s)
- Default:
0x0040
- Range:
0x0040 - 0x007F
Events Generated
When this request is received, the local device will send the CommandStatus Event.
Additional Command Status Return Parameters
- dataLen:
- Size:
1 byte(s)
- Range:
- state:
- Condition:
( StatStatus==0x00)
- Size:
1 byte(s)
- Range:
Value
Description
0x0000
L2CAP_CLOSED
0x0001
L2CAP_OPEN
0x0002
L2CAP_PENDING_CONN_RSP
0x0003
L2CAP_PENDING_DISCONN_RSP
0x0004
L2CAP_PENDING_PARAM_UPDATE_RSP
0x0005
L2CAP_PENDING_INFO_RSP
0x0006
L2CAP_PENDING_SEC_VERIFY
- connHandle:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- PSM:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- CID:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- MTU:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- MPS:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- credits:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerCID:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerMTU:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerMPS:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerCredits:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerCreditThreshold:
- Condition:
( StatStatus==0x00)
- Size:
2 byte(s)
- Range:
L2CAP_ConnectReq¶
- Opcode:
0xFC94
- Command Description:
The L2CAP Connection Request command is used to create and configure a Connection Oriented Channel between the local and the peer device.
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- PSM:
Local Protocol/Service Multiplexer (PSM)
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0x00FF
- peerPSM:
Peer Protocol/Service Multiplexer (PSM)
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0x00FF
Events Generated
When this command is received, the local device will send the CommandStatus Event with the Status parameter after sending an LE Credit Based Connection Request to the peer device. When a new channel has been established, the L2CAP Channel Established Event (L2CAP_ChannelEstablished) will be generated.
L2CAP_ConnectRsp¶
- Opcode:
0xFC95
- Command Description:
When a device receives an LE Credit Based Connection Request, it must send an LE Credit Based Connection Response back, which is done automatically by the L2CAP layer. However, if the application wishes to perform its own security verification (configurable at PSM registration), then a Connection Request (L2CAP_ConnectReq) event will be sent up to the application which must then send a Connection Response (L2CAP_ConnectRsp) command back indicating the outcome of the connection request.
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- id:
Identifier to match responses with requests
- Size:
1 byte(s)
- Default:
0x01
- Range:
0x01 - 0xFF
- result:
Indicates outcome of connection request
- Size:
2 byte(s)
- Default:
0x0000
- Range:
Value
Description
0x0000
L2CAP_CONN_SUCCESS
0x0001
Reserved
0x0002
L2CAP_CONN_PSM_NOT_SUPPORTED
0x0003
Reserved
0x0004
L2CAP_CONN_NO_RESOURCES
0x0005
L2CAP_CONN_INSUFFICIENT_AUTHEN
0x0006
L2CAP_CONN_INSUFFICIENT_AUTHOR
0x0007
L2CAP_CONN_INSUFFICIENT_KEY_SIZE
0x0008
L2CAP_CONN_INSUFFICIENT_ENCRYPT
0x0009
L2CAP_CONN_INVALID_SRC_CID
0x000A
L2CAP_CONN_SRC_CID_ALREADY_ALLOC
Events Generated
When this request is received, the local device will send the CommandStatus Event with the Status parameter after sending an LE Credit Based Connection Response back to the peer device.
L2CAP_DisconnectReq¶
- Opcode:
0xFC86
- Command Description:
The L2CAP Disconnection Request is sent to terminate a Connection Oriented Channel established between the local and the peer device.
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- CID:
Local Channel ID
- Size:
2 byte(s)
- Default:
0x0040
- Range:
0x0040 - 0x007F
Events Generated
When this command is received, the local device will send the CommandStatus Event with the Status parameter after forwarding the request to the peer device. When the channel is terminated, the L2CAP Channel Terminated Event (L2CAP_ChannelTerminated) will be generated.
L2CAP_FlowCtrlCredit¶
- Opcode:
0xFC96
- Command Description:
The LE Flow Control Credit commands are sent when the local device is capable of receiving additional LE-frames on an established L2CAP channel.
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- CID:
Local Channel ID
- Size:
2 byte(s)
- Default:
0x0040
- Range:
0x0040 - 0x007F
- peerCredits:
Number of LE-frames that can be sent to local device
- Size:
2 byte(s)
- Default:
0x0001
- Range:
0x0001 - 0xFFFF
Events Generated
When this request is received, the local device will send the CommandStatus Event with the Status parameter after forwarding the request to the peer device. When the peer credit count reaches a specified low threshold (configurable at PSM registration), the L2CAP Peer Credit Threshold Event (L2CAP_PeerCreditThreshold) will be generated.
L2CAP_InfoReq¶
- Opcode:
0xFC8A
- Command Description:
L2CAP Info Request
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- infoType:
The type of implementation specific information being requested
- Size:
2 byte(s)
- Default:
0x0002
- Range:
Value
Description
0x0001
CONNECTIONLESS_MTU
0x0002
EXTENDED_FEATURES
0x0003
FIXED_CHANNELS
Events Generated
When this request is received, the local device will send the CommandStatus Event with the Status parameter after forwarding the request to the peer device. After receiving a response from the peer device, the L2CAP_InfoRsp will be generated.
L2CAP_ConnParamUpdateReq¶
- Opcode:
0xFC92
- Command Description:
The Connection Parameter Update Request is sent from the LE peripheral device to the LE central device. This request allows the LE peripheral Host to request a set of new connection parameters.
Command Parameters
- Connection Handle:
Identifies the connection.
- Size:
2 byte(s)
- Default:
0x0000
- Range:
0x0000 to 0xFFFD
- intervalMin:
The minimum value for the connection event interval
- Size:
2 byte(s)
- Default:
80
- Range:
6 - 3200
- intervalMax:
The maximum value for the connection event interval
- Size:
2 byte(s)
- Default:
160
- Range:
6 - 3200
- peripheralLatency:
The peripheral latency parameter
- Size:
2 byte(s)
- Default:
0
- Range:
0 - 500
- timeoutMultiplier:
The connection timeout parameter
- Size:
2 byte(s)
- Default:
1000
- Range:
10 - 3200
Events Generated
When this request is received, the LE peripheral host will send the CommandStatus Event with the Status parameter after forwarding the request to the LE central host. The LE central host will send the Connection Parameter Update Response (L2CAP_ConnParamUpdateRsp) event back. If the LE peripheral host receives this request, it will respond with a Command Reject (L2CAP_CmdReject) with reason 0x0000 (command not understood).
L2CAP Extension Events¶
All L2CAP event have the following format (this is also displayed for each event description):
Name |
Size (bytes) |
Description |
Opcode |
2 |
PDU operation code |
Status |
1 |
Event Status |
Connection Handle |
2 |
Connection handle of the link |
Event PDU |
Variable |
Event parameters |
For the event parameters, please see the corresponding section below.
L2CAP_CmdReject¶
- Opcode:
0x0481
- Event Description:
The Command Reject is sent in response to a command with an unknown command code or when sending the corresponding response is inappropriate
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link.
- Size:
2 byte(s)
- Range:
- reason:
Reason for rejection.
- Size:
2 byte(s)
- Range:
Value
Description
0x0000
CMD_NOT_UNDERSTOOD
0x0001
SIGNAL_MTU_EXCEED
0x0002
REJECT_INVALID_CID
- signalingMTU:
- Condition:
( CmdRejectReason==0x0001)
- Size:
2 byte(s)
- Range:
- localCID:
- Condition:
( CmdRejectReason==0x0002)
- Size:
2 byte(s)
- Range:
- remoteCID:
- Condition:
( CmdRejectReason==0x0002)
- Size:
2 byte(s)
- Range:
L2CAP_ConnectReq¶
- Opcode:
0x0494
- Event Description:
This Connection Request event is sent to the application since the application has wished to perform its own security verification (configured at PSM registration). After receiving a Connection Request, the application must respond back with a Connection Response (L2CAP_ConnectRsp) command indicating the outcome of the connection request.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- id:
Identifier to match responses with requests (i.e., id to send back with L2CAP Connect Response command)
- Condition:
( bStatus==0x00)
- Size:
1 byte(s)
- Range:
- PSM:
Local PSM receiving connect request
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
- sourceCID:
Represents CID on device sending connect request and receiving connect response (i.e., peer CID)
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
- MTU:
Specifies maximum SDU size that can be received on this channel on the peer device
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
- MPS:
Specifies maximum payload size that can be received on this channel on the peer device
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
- initialCredits:
Indicates number of LE-frames that peer device can receive on this channel
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
L2CAP_ConnParamUpdateRsp¶
- Opcode:
0x0493
- Event Description:
This Connection Parameter Update Response is sent from the LE central device to the LE peripheral device. This response is sent by the central Host when it receives a Connection Parameter Update Request packet.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- result:
Result of the update.
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
Value
Description
0x0000
CONN_PARAMS_ACCEPTED
0x0001
CONN_PARAMS_REJECTED
L2CAP_ChannelEstablished¶
- Opcode:
0x04E0
- Event Description:
This Channel Established Event is generated when a Connection Oriented Channel has been established with the peer device. If result is successful (0x0000) then all other fields of the event will be present and can be accessed.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- result:
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
Value
Description
0x0000
L2CAP_CONN_SUCCESS
0x0001
Reserved
0x0002
L2CAP_CONN_PSM_NOT_SUPPORTED
0x0003
Reserved
0x0004
L2CAP_CONN_NO_RESOURCES
0x0005
L2CAP_CONN_INSUFFICIENT_AUTHEN
0x0006
L2CAP_CONN_INSUFFICIENT_AUTHOR
0x0007
L2CAP_CONN_INSUFFICIENT_KEY_SIZE
0x0008
L2CAP_CONN_INSUFFICIENT_ENCRYPT
0x0009
L2CAP_CONN_INVALID_SRC_CID
0x000A
L2CAP_CONN_SRC_CID_ALREADY_ALLOC
- PSM:
Local PSM that channel belongs to
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- CID:
Local Channel ID
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- MTU:
Maximum SDU size that can be received by the local device on this channel
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- MPS:
Maximum payload size that can be received by the local device
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- credits:
Number of LE-frames that the local device can send
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- peerCID:
Remote Channel ID
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- peerMTU:
Maximum SDU size that can be received by the peer device
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- peerMPS:
Maximum payload size that can be received by the peer device
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- peerCredits:
Number of LE-frames that the peer device can send
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
- peerCreditThreshold:
Low threshold for the peer credit count
- Condition:
( bStatus==0x00 resultValue==0x0000)
- Size:
2 byte(s)
- Range:
L2CAP_ChannelTerminated¶
- Opcode:
0x04E1
- Event Description:
This Channel Terminated Event is generated when a Connection Oriented Channel has been terminated between the local and the peer device.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- CID:
Local Channel ID
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
- peerCID:
Remote Channel ID
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
- reason:
Reason Channel was termianted
- Condition:
( bStatus==0x00)
- Size:
2 byte(s)
- Range:
Value
Description
0x0000
L2CAP_TERM_LINK_DOWN
0x0001
L2CAP_TERM_BY_PSM
0x0002
L2CAP_TERM_BY_PEER_PSM
0x0003
L2CAP_TERM_MAX_CREDIT_EXCEED
0x0004
L2CAP_TERM_SDU_LEN_EXCEED
0x0005
L2CAP_TERM_PSM_MTU_EXCEED
0x0006
L2CAP_TERM_RX_PKT_NO_CREDIT
0x0007
L2CAP_TERM_RX_ERROR
0x0008
L2CAP_TERM_TX_ERROR
0x0009
L2CAP_TERM_MEM_ALLOC_ERROR
L2CAP_OutOfCredit¶
- Opcode:
0x04E2
- Event Description:
This Out Of Credit Event is generated when a Connection Oriented Channel runs out of credits needed to transmit an SDU to the peer device.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- CID:
Local Channel ID
- Size:
2 byte(s)
- Range:
- peerCID:
Remote Channel ID
- Size:
2 byte(s)
- Range:
- creditsNeeded:
Number of credits needed to transmit the remaining part of the current SDU
- Size:
2 byte(s)
- Range:
L2CAP_PeerCreditThreshold¶
- Opcode:
0x04E3
- Event Description:
This Peer Credit Threshold Event is generated when an L2CAP Connection Oriented Channel reaches a low threshold specified for the peer credit count (configured at PSM registration).
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- CID:
Local Channel ID
- Size:
2 byte(s)
- Range:
- peerCID:
Remote Channel ID
- Size:
2 byte(s)
- Range:
- peerCreditThreshold:
Low threshold for the peer credit count
- Size:
2 byte(s)
- Range:
L2CAP_SendSduDone¶
- Opcode:
0x04E4
- Event Description:
This Send SDU Done Event is generated when the transmission of an SDU is completed on a Connection Oriented Channel established with the peer device.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- CID:
Local Channel ID
- Size:
2 byte(s)
- Range:
- credits:
Remaining local credits
- Size:
2 byte(s)
- Range:
- peerCID:
Remote Channel ID
- Size:
2 byte(s)
- Range:
- peerCredits:
Remaining peer credits
- Size:
2 byte(s)
- Range:
- totalLen:
Total length of the SDU being transmitted
- Size:
2 byte(s)
- Range:
- txLen:
Total number of octets transmitted
- Size:
2 byte(s)
- Range:
L2CAP_PeerCreditReceived¶
- Opcode:
0x04E6
- Event Description:
This Peer Credit Received Event is generated when a peer device with Connection Oriented Channel send to local device additional credits.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- CID:
Local Channel ID
- Size:
2 byte(s)
- Range:
- creditsReceived:
Number of credits received from peer device
- Size:
2 byte(s)
- Range:
L2CAP_SendData¶
- Opcode:
0x04F0
- Event Description:
This Data Event is generated when an SDU is received on a Connection Oriented Channel from the peer device.
Event Parameters
- Status:
- Size:
1 byte(s)
- Range:
Value
Description
0x00
SUCCESS
0x12
bleIncorrectMode
0x02
INVALIDPARAMETER
- connectionHandle:
Connection handle of the link
- Size:
2 byte(s)
- Range:
Any 2 byte value
- CID:
Local Channel ID
- Size:
2 byte(s)
- Range:
- len:
Total length of the SDU being received
- Size:
2 byte(s)
- Range:
- SDU:
Received SDU
- Size:
payloadLen byte(s)
- Range: