HCI Interface

HCI Overview

The HCI is a standardized Bluetooth interface for sending commands, receiving events, and for sending and receiving data. It is typically realized as a serial interface, using either RS232 or USB communication devices. As the name implies, the HCI is used to bridge the Host and Controller devices. Commands and Events can either be specified, or can be vendor specific for extensibility. The following sections summarize the HCI protocol, the specification defined commands and events used by BLE, and a detailed description of the vendor specific commands and events defined by Texas Instruments Inc. For complete details on the HCI as specified by the Special Interest Group (SIG), please see the Core specification [1].

Specification Interface

HCI Interface Protocol

The HCI supports four types of packets: Command Packet, Asynchronous Data Packet, Synchronous Data Packet, and Event Packet. The packet type is a one byte value that precedes the HCI packet. The packet type has the following values:

Packet

Packet Type

Command

0x01

Asynchronous Data

0x02

Synchronous Data

0x03

Event

0x04

Extended Command

0x09

The contents of each packet are shown as follows (please see section 5.4 of [1], Vol. 2, Part E for additional details).

Command Packet

The command packet is comprised of the opcode, the number of parameters, and parameters themselves.

../_images/command-packet.png

Fig. 5 Command Packet

Asynchronous Data Packet

The asynchronous data packet is comprised of the connection handle, fragmentation bits, the number of data bytes, and the data bytes themselves.

../_images/async-data-packet.png

Fig. 6 Asynchronous Data Packet

Synchronous Data Packet

This synchronous data packet is not used in BLE.

Event Packet

The event packet is comprised of the event code, the number of event parameters, and the event parameters themselves.

../_images/event-packet.png

Fig. 7 Event Packet

Extended Command

This packet is used to allow more than the HCI limit of 256 bytes. It includes a two-byte length field which states the payload length:

Offset

Description

0

packet type (0x09)

1

LSB opcode

2

MSB opcode

3

LSB payload length

4

MSB payload length

5..(length-3)

Payload

See each individual command for payload formatting.

HCI Commands

HCI commands use a 16-bit opcode for identification. The opcode is subdivided into two parts: a 10-bit Opcode Command Field (OCF) and a 6-bit Opcode Group Field (OGF).

../_images/hci-command-opcode.png

Fig. 8 HCI Command Opcode

The OGF values are defined by the Bluetooth (BT) Core specification. The LE specification has its own OGF value. Also, there is an escape OGF value so that vendor specific OCF codes can be used. The following OGF values are valid for BLE: # Link Control Commands: 1 # Link Policy Commands: 2 # Controller and Baseband Commands: 3 # Informational Parameters: 4 # Status Parameters: 5 # Testing Commands: 6 # LE Only Commands: 8 # Vendor Specific Commands: 63

The following table, Table 2, lists all specification LE HCI commands and their opcodes. Note that while all commands can be sent by the application processor to the Network Processor using HCI, not all events will be returned as they will be trapped and possibly discarded by the Host layer of the BLE Stack. Therefore, it is not possible to support an external BLE Host in the Network Processor configuration. Network Processor based designs should use the respective Vendor Extension commands detailed in the following sections to implement an off-chip application.

LE Commands

OGF

OCF

Opcdoe

LE Set Event Mask

8

1

0x2001

LE Read Buffer Size

8

2

0x2002

LE Read Local Supported Features

8

3

0x2003

LE Set Random Address

8

5

0x2005

LE Set Advertising Parameters

8

6

0x2006

LE Read Advertising Channel TX Power

8

7

0x2007

LE Set Advertising Data

8

8

0x2008

LE Set Scan Response Data

8

9

0x2009

LE Set Advertise Enable

8

10

0x200A

LE Set Scan Parameters

8

11

0x200B

LE Set Scan Enable

8

12

0x200C

LE Create Connection

8

13

0x200D

LE Create Connection Cancel

8

14

0x200E

LE Read White List Size

8

15

0x200F

LE Clear White Lis

8

16

0x2010

LE Add Device To White List

8

17

0x2011

LE Remove Device From White List

8

18

0x2012

LE Connection Update

8

19

0x2013

LE Set Host Channel Classification

8

20

0x2014

LE Read Channel Map

8

21

0x2015

LE Read Remote Used Features

8

22

0x2016

LE Encrypt

8

23

0x2017

LE Rand

8

24

0x2018

LE Start Encryption

8

25

0x2019

LE Long Term Key Requested Reply

8

26

0x201A

LE Long Term Key Requested Negative Reply

8

27

0x201B

LE Read Supported States

8

28

0x201C

LE Receiver Test

8

29

0x201D

LE Transmitter Test

8

30

0x201E

LE Test End Command

8

31

0x201F

LE Remote Connection Parameter Request Reply

8

32

0x2020

LE Remote Connection Parameter Request Negative Reply

8

33

0x2021

LE Set Data Length

8

34

0x2022

LE Read Suggested Default Data Length

8

35

0x2023

LE Write Suggested Default Data Length

8

36

0x2024

LE Read Local P256 Public Key 37 0x2025 LE Generate DHKey

8

38

0x2026

LE Add Device to Resolving List

8

39

0x2027

LE Remove Device from Resolving List

8

40

0x2028

LE Clear Resolving List

8

41

0x2029

LE Read Resolving List Size

8

42

0x202A

LE Read Peer Resolvable Address

8

43

0x202B

LE Read Local Resolvable Address

8

44

0x202C

LE Set Address Resolution Enable

8

45

0x202D

LE Set Resolvable Private Address Timeout

8

46

0x202E

LE Read Maximum Data Length

8

47

0x202F

BT Commands for LE

OGF

OCF

Opcode

Disconnect

1

6

0x0406

Read Remote Version Information

1

29

0x041D

Set Event Mask

3

1

0x0C01

Reset

3

3

0x0C03

Read Transmit Power Level

3

45

0x0C2D

Set Controller To Host Flow Control (optional)

3

49

0x0C31

Host Buffer Size (optional)

3

51

0x0C33

Host Number Of Completed Packets (optional)

3

53

0x0C35

Set Event Mask Page

3

63

0x0C63

Read Authenticated Payload Timeout

4

123

0x0C7B

Write Authenticated Payload Timeout

4

124

0x0C7C

Read Local Version Information

4

1

0x1001

Read Local Supported Commands (optional)

4

2

0x1002

Read Local Supported Features

4

3

0x1003

Read BD_ADDR

4

9

0x1009

Read RSSI

5

5

0x1405

HCI Events

HCI events use an 8-bit event code. All event codes are unique for BT and BLE. Only event code 255 is reserved for vendor specific events. There is only one event code for all LE events. The first event parameter is used as the subevent code to distinguish the LE event types.

The following table lists all the BLE events and their event codes, and subevent codes when applicable:

LE Events

Event Code

Subevent Code

LE Connection Complete

0x3E

0x01

LE Advertising Report

0x3E

0x02

LE Connection Update Complete

0x3E

0x03

LE Read Remote Used Features Complete

0x3E

0x04

LE Long Term Key Requested

0x3E

0x05

LE Remote Connection Parameter Request

0x3E

0x06

LE Data Length Change

0x3E

0x07

LE Read Local P256 Public Key Complete

0x3E

0x08

LE Generate DHKey Complete

0x3E

0x09

LE Enhanced Connection Complete

0x3E

0x0A

LE Direct Advertising Report

0x3E

0x0B

BT Events

Event Code

Disconnection Complete

0x05

Encryption Change

0x08

Read Remote Version Information Complete

0x0C

Command Complete

0x0E

Command Status

0x0F

Hardware Error (optional)

0x10

Number Of Completed Packets

0x13

Data Buffer Overflow

0x1A

Encryption Key Refresh Complete

0x30

Authenticated Payload Timeout Expired

0x57

Vendor Specific Interface

As mentioned, vendors can specify their own HCI commands and events by using the predefined vendor specific opcode and vendor specific event code.

Vendor Specific Commands

A vendor specific opcode is indicated by an OGF value of 63. The vendor can use the remaining 10 bits (i.e. the OCF) as they like. TI defines its vendor specific OCF values by subdividing the 10 bits into a 3 MSB Command Subgroup (CSG) and a 7 LSB Command (CMD). The CSG is used by the HCI to route the commands to a designated subsystem within the BLE stack. In this way, vendor specific commands can be specified for any BLE stack layer.

../_images/vendor-specific-opcode-0-6.png

Fig. 9 HCI Vendor Specific Command Opcode, CSG=0..6

The Command Subgroups are defined as follows:

CSG

Subgroup

0

HCI

1

L2CAP

2

ATT

3

GATT

4

GAP

5

UTIL

6

Reserved

7

User Profile

For Command Subgroups 0 to 6, the remaining 7 bits of Command provide up to 128 commands for each subgroup. For Subgroup 7, the remaining 7 bits specify one of 128 profiles and indicates that the subsequent byte is to be used as the command for that particular profile (i.e. up to 256 commands per profile).

../_images/vendor-specific-opcode-7.png

Fig. 10 HCI Vendor Specific Command Opcode, CSG=7

The following table lists all TI-specific HCI commands:

Vendor Specific Command

OGF

CSG

CMD

Opcode

HCI_EXT_SetRxGainCmd

63

0

0

0xFC00

HCI_EXT_OnePktPerEvtCmd

63

0

2

0xFC02

HCI_EXT_ClkDivideOnHaltCmd

63

0

3

0xFC03

HCI_EXT_DeclareNvUsageCmd

63

0

4

0xFC04

HCI_EXT_DecryptCmd

63

0

5

0xFC05

HCI_EXT_SetLocalSupportedFeaturesCmd

63

0

6

0xFC06

HCI_EXT_SetFastTxRespTimeCmd

63

0

7

0xFC07

HCI_EXT_ModemTestTxCmd

63

0

8

0xFC08

HCI_EXT_ModemHopTestTxCmd

63

0

9

0xFC09

HCI_EXT_ModemTestRxCmd

63

0

10

0xFC0A

HCI_EXT_EndModemTestCmd

63

0

11

0xFC0B

HCI_EXT_SetBDADDRCmd

63

0

12

0xFC0C

HCI_EXT_SetVirtualAdvAddrCmd

63

0

115

0xFC73

HCI_EXT_SetSCACmd

63

0

13

0xFC0D

HCI_EXT_EnablePTMCmd

63

0

14

0xFC0E

HCI_EXT_MapPmIoPortCmd

63

0

18

0xFC12

HCI_EXT_DisconnectImmedCmd

63

0

19

0xFC13

HCI_EXT_PacketErrorRateCmd

63

0

20

0xFC14

HCI_EXT_PERbyChanCmd

63

0

21

0xFC15

HCI_EXT_ExtendRfRangeCmd

63

0

22

0xFC16

HCI_EXT_HaltDuringRfCmd

63

0

25

0xFC19

HCI_EXT_SetPeripheralLatencyOverrideCmd

63

0

26

0xFC1A

HCI_EXT_BuildRevisionCmd

63

0

27

0xFC1B

HCI_EXT_DelaySleepCmd

63

0

28

0xFC1C

HCI_EXT_ResetSystemCmd

63

0

29

0xFC1D

HCI_EXT_OverlappedProcessingCmd

63

0

30

0xFC1E

HCI_EXT_NumComplPktsLimitCmd

63

0

31

0xFC1F

HCI_EXT_GetConnInfoCmd

63

0

32

0xFC20

HCI_EXT_SetMaxDataLenCmd

63

0

33

0xFC21

HCI_EXT_SetDtmTxPktCntCmd

63

0

36

0xFC24

HCI_EXT_EnhancedModemTestTxCmd

63

0

39

0xFC27

HCI_EXT_EnhancedModemHopTestTxCmd

63

0

40

0xFC28

HCI_EXT_EnhancedModemTestRxCmd

63

0

41

0xFC29

HCI_EXT_SetPinOutputCmd

63

0

42

0xFC2A

HCI_EXT_SetLocationingAccuracyCmd

63

0

43

0xFC2B

HCI_EXT_GetActiveConnInfoCmd

63

0

44

0xFC2C

HCI_EXT_CoexEnableCmd

63

0

46

0xFC2E

HCI_EXT_SetTxPowerDbmCmd

63

0

47

0xFC2F

HCI_EXT_SetMaxDtmTxPowerDbmCmd

63

0

48

0xFC30

HCI_EXT_GetRxStatisticsCmd

63

0

49

0xFC31

HCI_EXT_GetTxStatisticsCmd

63

0

50

0xFC32

HCI_EXT_GetCoexStatisticsCmd

63

0

51

0xFC33

HCI_EXT_HostToControllerCmd

63

0

52

0xFC34

HCI_EXT_RssiMon_RegCmd

63

0

53

0xFC35

HCI_EXT_RssiMon_UnregCmd

63

0

54

0xFC36

HCI_EXT_RssiMon_SetConfigCmd

63

0

55

0xFC37

HCI_EXT_RssiMon_GetConfigCmd

63

0

56

0xFC38

HCI_EXT_RssiMon_GetRssiStatCmd

63

0

57

0xFC39

HCI_EXT_LLTestModeCmd

63

0

112

0xFC70

HCI_EXT_SetQOSParameters

63

0

117

0xFC75

HCI_EXT_SetQOSDefaultParameters

63

0

118

0xFC76

HCI_EXT_SetHostDefChanClassificationCmd

63

0

121

0xFC79

HCI_EXT_SetHostConnChanClassificationCmd

63

0

122

0xFC7A

HCI_EXT_SendPowerControlRequestCmd

63

0

124

0xFC7C

HCI_EXT_SetDefaultAntennaCmd

63

0

125

0xFC7D

L2CAP_DisconnectReq

63

1

6

0xFC86

L2CAP_InfoReq

63

1

10

0xFC8A

L2CAP_ConnParamUpdateReq

63

1

18

0xFC92

L2CAP_ConnectReq

63

1

20

0xFC94

L2CAP_ConnectRsp

63

1

21

0xFC95

L2CAP_FlowCtrlCredit

63

1

22

0xFC96

L2CAP_SendData

63

1

112

0xFCF0

L2CAP_RegisterPsm

63

1

113

0xFCF1

L2CAP_DeregisterPsm

63

1

114

0xFCF2

L2CAP_PsmInfo

63

1

115

0xFCF3

L2CAP_PsmChannels

63

1

116

0xFCF4

L2CAP_ChannelInfo

63

1

117

0xFCF5

ATT_ErrorRsp

63

2

1

0xFD01

ATT_ExchangeMTUReq

63

2

2

0xFD02

ATT_ExchangeMTURsp

63

2

3

0xFD03

ATT_FindInfoReq

63

2

4

0xFD04

ATT_FindInfoRsp

63

2

5

0xFD05

ATT_FindByTypeValueReq

63

2

6

0xFD06

ATT_FindByTypeValueRsp

63

2

7

0xFD07

ATT_ReadByTypeReq

63

2

8

0xFD08

ATT_ReadByTypeRsp

63

2

9

0xFD09

ATT_ReadReq

63

2

10

0xFD0A

ATT_ReadRsp

63

2

11

0xFD0B

ATT_ReadBlobReq

63

2

12

0xFD0C

ATT_ReadBlobRsp

63

2

13

0xFD0D

ATT_ReadMultiReq

63

2

14

0xFD0E

ATT_ReadMultiRsp

63

2

15

0xFD0F

ATT_ReadByGrpTypeReq

63

2

16

0xFD10

ATT_ReadByGrpTypeRsp

63

2

17

0xFD11

ATT_WriteReq

63

2

18

0xFD12

ATT_WriteRsp

63

2

19

0xFD13

ATT_PrepareWriteReq

63

2

22

0xFD16

ATT_PrepareWriteRsp

63

2

23

0xFD17

ATT_ExecuteWriteReq

63

2

24

0xFD18

ATT_ExecuteWriteRsp

63

2

25

0xFD19

ATT_HandleValueNoti

63

2

27

0xFD1B

ATT_HandleValueInd

63

2

29

0xFD1D

ATT_HandleValueCfm

63

2

30

0xFD1E

GATT_ExchangeMTU

63

3

2

0xFD82

GATT_DiscAllCharDescs

63

3

4

0xFD84

GATT_DiscPrimaryServiceByUUID

63

3

6

0xFD86

GATT_DiscCharsByUUID

63

3

8

0xFD88

GATT_ReadCharValue

63

3

10

0xFD8A

GATT_ReadLongCharValue

63

3

12

0xFD8C

GATT_ReadMultiCharValues

63

3

14

0xFD8E

GATT_DiscAllPrimaryServices

63

3

16

0xFD90

GATT_WriteCharValue

63

3

18

0xFD92

GATT_WriteLongCharValue

63

3

22

0xFD96

GATT_Notification

63

3

27

0xFD9B

GATT_Indication

63

3

29

0xFD9D

GATT_FindIncludedServices

63

3

48

0xFDB0

GATT_DiscAllChars

63

3

50

0xFDB2

GATT_ReadUsingCharUUID

63

3

52

0xFDB4

GATT_WriteNoRsp

63

3

54

0xFDB6

GATT_SignedWriteNoRsp

63

3

56

0xFDB8

GATT_ReliableWrites

63

3

58

0xFDBA

GATT_ReadCharDesc

63

3

60

0xFDBC

GATT_ReadLongCharDesc

63

3

62

0xFDBE

GATT_WriteCharDesc

63

3

64

0xFDC0

GATT_WriteLongCharDesc

63

3

66

0xFDC2

GATT_AddService

63

3

124

0xFDFC

GATT_DelService

63

3

125

0xFDFD

GATT_AddAttribute

63

3

126

0xFDFE

GATT_UpdateMTU

63

3

127

0xFDFF

GAP_DeviceInit

63

4

0

0xFE00

GAP_TerminateLinkReq

63

4

10

0xFE0A

GAP_Authenticate

63

4

11

0xFE0B

GAP_PasskeyUpdate

63

4

12

0xFE0C

GAP_PeripheralSecurityRequest

63

4

13

0xFE0D

GAP_Signable

63

4

14

0xFE0E

GAP_Bond

63

4

15

0xFE0F

GAP_TerminateAuth

63

4

16

0xFE10

GAP_UpdateLinkParamReq

63

4

17

0xFE11

GAP_UpdateLinkParamReqReply

63

4

18

0xFE12

Gap_RegisterConnEvent

63

4

19

0xFE13

GapAdv_SetPeriodicAdvParams

63

4

20

0xFE14

GapAdv_SetPeriodicAdvData

63

4

21

0xFE15

GapAdv_SetPeriodicAdvEnable

63

4

22

0xFE16

GapScan_PeriodicAdvCreateSync

63

4

23

0xFE17

GapScan_PeriodicAdvCreateSyncCancel

63

4

24

0xFE18

GapScan_PeriodicAdvTerminateSync

63

4

25

0xFE19

GapScan_SetPeriodicAdvReceiveEnable

63

4

26

0xFE1A

GapScan_AddDeviceToPeriodicAdvList

63

4

27

0xFE1B

GapScan_RemoveDeviceFromPeriodicAdvList

63

4

28

0xFE1C

GapScan_ReadPeriodicAdvListSize

63

4

29

0xFE1D

GapScan_ClearPeriodicAdvList

63

4

30

0xFE1E

GapConfig_SetParameter

63

4

47

0xFE2F

GAP_SetParamValue

63

4

48

0xFE30

GAP_GetParamValue

63

4

49

0xFE31

GAPBondMgr_SetParameter

63

4

54

0xFE36

GAPBondMgr_GetParameter

63

4

55

0xFE37

GAPBondMgr_ServiceChangeInd

63

4

56

0xFE38

GAPBondMgr_SCGetLocalOOBParameters

63

4

76

0xFE4C

GAPBondMgr_SCSetRemoteOOBParameters

63

4

77

0xFE4D

SM_RegisterTask

63

4

57

0xFE39

SM_GetEccKeys

63

4

58

0xFE3A

SM_GetDHKey

63

4

59

0xFE3B

SM_GetScConfirmOob

63

4

60

0xFE3C

GapAdv_create

63

4

62

0xFE3E

GapAdv_enable

63

4

63

0xFE3F

GapAdv_disable

63

4

64

0xFE40

GapAdv_destroy

63

4

65

0xFE41

GapAdv_setParam

63

4

66

0xFE42

GapAdv_getParam

63

4

67

0xFE43

GapAdv_loadData

63

4

68

0xFE44

GapAdv_setEventMask

63

4

69

0xFE45

GapAdv_setVirtualAdvAddr

63

4

75

0xFE4B

GAPBondMgr_Pair

63

4

72

0xFE48

GAPBondMgr_FindAddr

63

4

73

0xFE49

GAPBondMgr_PasscodeRsp

63

4

74

0xFE4A

GapScan_enable

63

4

81

0xFE51

GapScan_disable

63

4

82

0xFE52

GapScan_setPhyParams

63

4

83

0xFE53

GapScan_getPhyParams

63

4

84

0xFE54

GapScan_setParam

63

4

85

0xFE55

GapScan_getParam

63

4

86

0xFE56

GapScan_setEventMask

63

4

87

0xFE57

GapScan_getAdvReport

63

4

88

0xFE58

GapInit_setPhyParam

63

4

96

0xFE60

GapInit_getPhyParam

63

4

97

0xFE61

GapInit_connect

63

4

98

0xFE62

GapInit_connectAl

63

4

99

0xFE63

GapInit_cancelConnect

63

4

100

0xFE64

UTIL_NV_Read

63

5

1

0xFE81

UTIL_NV_Write

63

5

2

0xFE82

UTIL_ForceBoot

63

5

3

0xFE83

UTIL_BuildRevision

63

5

4

0xFE84

UTIL_GetMemStats

63

5

7

0xFE87

Vendor Specific Events

A vendor specific event code is indicated by a value of 255. The vendor must then use event parameters (following the length byte) to specify vendor specific events. TI defines the following two bytes as the Event Opcode.

../_images/vendor-specific-event-1.png

The Event Opcode was chosen to mirror the Command Opcode by dividing it into two parts: a 6 bit Event Opcode Group Field (EOGF), and a 10 bit Event Opcode Event Field (EOEF).

../_images/vendor-specific-event-2.png

The EOEF is again chosen to mirror the Command OCF by dividing it into two parts: the Event Subgroup (ESG) and the Event.

../_images/vendor-specific-event-3.png

The EOGF is defined as follows:

EOGF

Group

0

Embedded Opcode

1

Core Opcode

2

Profile Request

3

Profile Response

4-63

Reserved

The ESG is defined as in Table 4. The Events are as defined in the following table. Please note that the value of the Events cannot be less than 0x400 as the first 1024 values are reserved. The reason for this has to do with Client/Server Request/Response Tunneling, which is described in the following section. Tunneling requires embedding Command Opcodes in HCI Events. When this is done, the EOGF is zero, and the remaining 10 bits is the Command Opcode. In order to prevent Command and Event Opcode overlap, the first 1024 values are reserved in the Event Opcode space. Also note that the Event Code (EC) is always 0xFF since normally only Controller events are returned via the HCI.

Vendor Specific Event

EC

EOGF

ESG

Event

Opcode

HCI_EXT_SetRxGainDone

0xFF

1

0

0

0x0400

HCI_EXT_SetTxPowerDone

0xFF

1

0

1

0x0401

HCI_EXT_OnePacketPerEventDone

0xFF

1

0

2

0x0402

HCI_EXT_DecryptCommandDone

0xFF

1

0

5

0x0405

HCI_EXT_WriteLocalFeatureSupportDone

0xFF

1

0

6

0x0406

HCI_EXT_SetFastTxResponseTimeDone

0xFF

1

0

7

0x0407

HCI_EXT_ModemTestTxDone

0xFF

1

0

8

0x0408

HCI_EXT_ModemHopTestTxDone

0xFF

1

0

9

0x0409

HCI_EXT_ModemTestRxDone

0xFF

1

0

10

0x040A

HCI_EXT_EndModemTestDone

0xFF

1

0

11

0x040B

HCI_EXT_SetBDADDRDone

0xFF

1

0

12

0x040C

HCI_EXT_SetVirtualAdvAddrDone

0xFF

1

0

45

0x042D

HCI_EXT_SetSCADone

0xFF

1

0

13

0x040D

HCI_EXT_EnablePTMDone

0xFF

1

0

14

0x040E

HCI_EXT_SetMaxDtmTxPowerDone

0xFF

1

0

17

0x0411

HCI_EXT_MapPmIoPortDone

0xFF

1

0

18

0x0412

HCI_EXT_DisconnectImmedDone

0xFF

1

0

19

0x0413

HCI_EXT_PER

0xFF

1

0

20

0x0414

HCI_EXT_PerByChanDone

0xFF

1

0

21

0x0415

HCI_EXT_OverridePLDone

0xFF

1

0

26

0x041A

HCI_EXT_BuildRevisionDone

0xFF

1

0

27

0x041B

HCI_EXT_ResetSystemDone

0xFF

1

0

29

0x041D

HCI_EXT_NumComplPktsLimitDone

0xFF

1

0

31

0x041F

HCI_EXT_GetConnInfoDone

0xFF

1

0

32

0x0420

HCI_EXT_SetMaxDataLengthDone

0xFF

1

0

33

0x0421

HCI_EXT_SetDtmTxPktCntDone

0xFF

1

0

36

0x0424

HCI_EXT_LE_ADV_EVENT

0xFF

1

0

37

0x0425

HCI_EXT_LE_SCAN_EVENT

0xFF

1

0

38

0x0426

HCI_EXT_EnhancedModemTestTxDone

0xFF

1

0

39

0x0427

HCI_EXT_EnhancedModemHopTestTxDone

0xFF

1

0

40

0x0428

HCI_EXT_EnhancedModemTestRxDone

0xFF

1

0

41

0x0429

HCI_EXT_SetPinOutputDone

0xFF

1

0

42

0x042A

HCI_EXT_SetLocationingAccuracyDone

0xFF

1

0

43

0x042B

HCI_EXT_GetActiveConnInfoDone

0xFF

1

0

44

0x042C

HCI_EXT_CoexEnableDone

0xFF

1

0

46

0x042E

HCI_EXT_SetDefaultChannelMapDone

0xFF

1

0

47

0x042F

HCI_EXT_SetConnectionChannelMapDone

0xFF

1

0

48

0x0430

HCI_EXT_GetRxStatisticsDone

0xFF

1

0

49

0x0431

HCI_EXT_GetTxStatisticsDone

0xFF

1

0

50

0x0432

HCI_EXT_GetCoexStatisticsDone

0xFF

1

0

51

0x0433

HCI_EXT_SetDefaultAntennaDone

0xFF

1

0

53

0x0435

HCI_EXT_RssiMon_RegCmdDone

0xFF

1

0

54

0x0436

HCI_EXT_RssiMon_GetConfigCmdDone

0xFF

1

0

55

0x0437

HCI_EXT_RssiMon_GetRssiStatCmdDone

0xFF

1

0

56

0x0438

HCI_EXT_RssiMon_ReportCB

0xFF

1

0

57

0x0439

HCI_EXT_LLTestModeDone

0xFF

1

0

112

0x0470

HCI_EXT_SendPowerControlRequestevent

0xFF

1

0

113

0x0471

L2CAP_CmdReject

0xFF

1

1

1

0x0481

L2CAP_InfoRsp

0xFF

1

1

11

0x048B

L2CAP_ConnParamUpdateRsp

0xFF

1

1

19

0x0493

L2CAP_ConnectReq

0xFF

1

1

20

0x0494

L2CAP_ChannelEstablished

0xFF

1

1

96

0x04E0

L2CAP_ChannelTerminated

0xFF

1

1

97

0x04E1

L2CAP_OutOfCredit

0xFF

1

1

98

0x04E2

L2CAP_PeerCreditThreshold

0xFF

1

1

99

0x04E3

L2CAP_PeerCreditReceived

0xFF

1

1

102

0x04E6

L2CAP_SendSduDone

0xFF

1

1

100

0x04E4

L2CAP_SendData

0xFF

1

1

112

0x04F0

ATT_ErrorRsp

0xFF

1

2

1

0x0501

ATT_ExchangeMTUReq

0xFF

1

2

2

0x0502

ATT_ExchangeMTURsp

0xFF

1

2

3

0x0503

ATT_FindInfoReq

0xFF

1

2

4

0x0504

ATT_FindInfoRsp

0xFF

1

2

5

0x0505

ATT_FindByTypeValueReq

0xFF

1

2

6

0x0506

ATT_FindByTypeValueRsp

0xFF

1

2

7

0x0507

ATT_ReadByTypeReq

0xFF

1

2

8

0x0508

ATT_ReadByTypeRsp

0xFF

1

2

9

0x0509

ATT_ReadReq

0xFF

1

2

10

0x050A

ATT_ReadRsp

0xFF

1

2

11

0x050B

ATT_ReadBlobReq

0xFF

1

2

12

0x050C

ATT_ReadBlobRsp

0xFF

1

2

13

0x050D

ATT_ReadMultiReq

0xFF

1

2

14

0x050E

ATT_ReadMultiRsp

0xFF

1

2

15

0x050F

ATT_ReadByGrpTypeReq

0xFF

1

2

16

0x0510

ATT_ReadByGrpTypeRsp

0xFF

1

2

17

0x0511

ATT_WriteReq

0xFF

1

2

18

0x0512

ATT_WriteRsp

0xFF

1

2

19

0x0513

ATT_PrepareWriteReq

0xFF

1

2

22

0x0516

ATT_PrepareWriteRsp

0xFF

1

2

23

0x0517

ATT_ExecuteWriteReq

0xFF

1

2

24

0x0518

ATT_ExecuteWriteRsp

0xFF

1

2

25

0x0519

ATT_HandleValueNoti

0xFF

1

2

27

0x051B

ATT_HandleValueInd

0xFF

1

2

29

0x051D

ATT_HandleValueCfm

0xFF

1

2

30

0x051E

ATT_FlowCtrlViolatedEvt_t

0xFF

1

2

126

0x057E

ATT_MtuUpdatedEvt

0xFF

1

2

127

0x057F

GATT_ClientCharCfgUpdated

0xFF

1

3

0

0x0580

GAP_DeviceInitDone

0xFF

1

4

0

0x0600

GAP_LinkEstablished

0xFF

1

4

5

0x0605

GAP_LinkTerminated

0xFF

1

4

6

0x0606

GAP_LinkParamUpdate

0xFF

1

4

7

0x0607

GAP_SignatureUpdated

0xFF

1

4

9

0x0609

GAP_AuthenticationComplete

0xFF

1

4

10

0x060A

GAP_PasskeyNeeded

0xFF

1

4

11

0x060B

GAP_PeripheralRequestedSecurity

0xFF

1

4

12

0x060C

GAP_BondComplete

0xFF

1

4

14

0x060E

GAP_PairingRequested

0xFF

1

4

15

0x060F

SM_GetEccKeys

0xFF

1

4

16

0x0610

SM_GetDHKey

0xFF

1

4

17

0x0611

GAP_LinkParamUpdateRequest

0xFF

1

4

18

0x0612

GAP_Advertiser/Scanner_Event

0xFF

1

4

19

0x0613

GAP_ConnectingCancelled

0xFF

1

4

21

0x0615

GAP_ConnectionEventNotice

0xFF

1

4

22

0x0616

GAP_BondLost

0xFF

1

4

23

0x0617

GAPAdv_SetPeriodicAdvParams

0xFF

1

4

25

0x0619

GAPAdv_SetPeriodicAdvData

0xFF

1

4

26

0x061A

GAPAdv_SetPeriodicAdvEnable

0xFF

1

4

27

0x061B

GAP_PeriodicAdvSyncEstablishEvent

0xFF

1

4

28

0x061C

GAP_PeriodicAdvReportEvent

0xFF

1

4

29

0x061D

GAP_PeriodicAdvSyncLostEvent

0xFF

1

4

30

0x061E

GAPScan_PeriodicAdvCreateSync

0xFF

1

4

31

0x061F

GAPScan_PeriodicAdvCreateSyncCancel

0xFF

1

4

32

0x0620

GAPScan_PeriodicAdvTerminateSync

0xFF

1

4

33

0x0621

GAPScan_SetPeriodicAdvReceiveEnable

0xFF

1

4

34

0x0622

GAPScan_AddDeviceToPeriodicAdvList

0xFF

1

4

35

0x0623

GAPScan_RemoveDeviceFromPeriodicAdvList

0xFF

1

4

36

0x0624

GAPScan_ReadPeriodicAdvListSize

0xFF

1

4

37

0x0625

GAPScan_ClearPeriodicAdvList

0xFF

1

4

38

0x0626

CommandStatus

0xFF

1

4

127

0x067F

UTIL_GetMemStats

0xFF

1

5

1

0x0681

UTIL_SystemError

0xFF

1

5

2

0x0682

You will note that there are two EOGF values for Profiles. At this time, no profiles are defined well enough to document here. These values are defined in anticipation of not only needing large numbers of profiles and their commands, but also of needing the direction the command is travelling when embedded in an HCI Command or Event. You can see that ATT does not have this issue as these commands are already defined using even values for commands and odd values for events, and thus, direction is distinguishable. For profiles, it is not yet known how the commands and events will be defined.

Request and Response Tunneling

In the Client/Server model defined and supported by the BLE stack, the Client sends Requests to the Server and the Server sends Responses back to the Client. The Requests sent by the Client may be handled by a Server on the same device, or they may travel OTA to the Server on another device. Similarly, the Response sent by the Server may be handled by a Client on the same device, or may be sent OTA to a Client on another device from which the request came. But in either case, as long as the Requests and Responses remain within the scope of the BLE stack software (i.e. the BLE Server database is on the device), the BLE stack remains unconcerned about whether the Requests and Responses are sent/received by the same device or are from another device. Please see Fig. 14.

../_images/tunneling-1.png

Fig. 14 Request/Response with Server Database in BLE Stack

However, when using the Network Processor Configuration with HCI such that the Server database is not located on the device, then Requests and Reponses have to be mapped into HCI Commands and Events. The HCI is specified such that only Commands are sent from the Host to the Controller, and only Events are sent from the Controller to the Host. If the Server database is located on say a PC, then when an OTA Request is received by the Server device, it must be sent to the PC via the HCI. Even though the Request started out on one end as an HCI Command, it must be provided to the remote PC as an HCI event on the other. Similarly, when the PC sends the Response on one end, which will be an HCI Event to the remote PC on the other, it must be sent to the device as an HCI Command. Thus, the Request, which starts out as an HCI Command, must be embedded in an HCI Event when received by the remote PC, and the Response, which starts out as an HCI Command, must be embedded in an HCI Event when received by the remote PC. In this way, Requests and Responses are being tunneled in HCI Commands and Events. Please see Fig. 15.

../_images/tunneling-2.png

Fig. 15 Request/Response with Server Database not in BLE Stack