Connection Monitor

This section introduces the functionality of the Connection Monitoring feature provided through TI’s BLE Stack. This section is set up into the following parts:

  1. Connection Monitor Introduction.

  2. Connection Monitor Feature.

  3. Connection Monitor Demo.

  4. Setting up Host PC.

  5. Loading FW Images.

  6. Running the Connection Monitor Demo.

Connection Monitor Introduction

The Connection Monitoring feature allows the CC23xx or CC27xx to follow, and monitor, active BLE connections. When the CC23xx or CC27xx is actively monitoring a connection, it is said to be in the Connection Monitoring Role (CMR). The CMR is not the same as the Peripheral, Central, Broadcaster or Observer roles, which the BLE device can be configured through SysConfig. Any CC23xx or CC27xx which has the Connection Monitoring feature enabled can enter the CMR at any point of it’s liftime. The CMR can co-exist with any BLE role that the CC23xx or CC27xx is configured to be in. In other words, if the CC23xx or CC27xx is configured to be a Peripheral upon startup, the CMR will work without compromising the functionality of the Peripheral role, given that there is no conflict of radio time.

Connection Monitor Feature

The Connection Monitor (CM), refers to any device that can monitor an ongoing connection between two external devices. This is enabled by the connection monitoring device receiving the connection information from one of the two external devices, in order to start tracking the connection. This connection information may be sent to the CM over UART, SPI, I2C, CAN, or any other protocol. Here is an example block diagram for the Connection Monitor feature, where the CM receives connection information over the UART protocol:

Note

The choice of UART is arbitrary, and only to demonstrate the block diagram. The user is free to choose any protocol of choice.

../_images/ditaa-d24dccd1baf6084eeb90b2dc52c00bcee02bd875.png

Since the CM is only “monitoring” an ongoing connection, it does not participate in the connection’s data exchange. The CM, in practicality, is a sniffer that is setup to scan for connection event packets between two devices that are in an active connection. If the CM is, successfully, able to receive the first two connection event packets from every connection event (One from the peripheral to the central, and the other from the central to the peripheral), the CM considers that connection event to be successfully monitored. This happens because every connection event starts with the central device sending a packet to the peripheral. If the peripheral receives this packet successfully, the peripheral replies to the central with its packet in response. There may be more packets that are sent in that connection event, but after the CM receives the initial two packets, it closes the monitoring session. It then waits until the next connection event to start monitoring again for the packets from that connection event, and this continues for as long as the connection information doesn’t change. The packets that are received per connection event are not parsed/decrypted by the CM. This means that the CM is, purely, observing an active connection, with no information about the data being exchanged between the two devices. The connection information that is needed by the CM to monitor a connection must therefore be explicitly provided to the CM via a communication medium, as shown above. Every time the CM scans, and successfully receives a packet, an event is raised to the application layer to report the following things in the form of a connection monitor report, and more:

  1. RSSI of the received packet.

  2. The origin of the packet (whether the sender was the central or the peripheral).

  3. The channel that the packet was received on.

When the CM starts monitoring a connection it assigns a connection handle to the connection monitoring session that has just started. This handle is used to uniquely identify the connection monitoring session. The assigned handle is stored in the same array that also tracks active connections. This implicitly means that the CM treats every connection monitoring session as a connection. This has no practical impact on the connection monitoring session itself. The only effect of this is that the total number of connections (active + connection monitoring) need to be less than or equal to the maximum number of connections as defined in the project’s SysConfig file.

Note

The size of the CM data is now reduced to 56 bytes.

Warning

  • CMS_GetConnDataSize(void) returns uint8_t instead of uint16_t.

  • cmErrorCodes_e CMS_GetConnData(uint16_t connHandle, cmsConnDataParams_t *pData) adds uint32_t accessAddr to the CMS_GetConnData struct.

  • dataSize is changed from uint16_t to uint8_t.

  • cmErrorCodes_e CM_StartMonitor(cmStartMonitorParams_t *pParams) adds to the paramters structure. cmStartMonitorParams_t, adjustementEvtTries and cmConnectionMaskRole_e connRole were removed from the struct.

  • cmDataSize was changed from uint16_t to uint8_t.

  • cmReportEvt_t now contains 2 packets with status of CM_PKT_STATUS_NOT_RECEIVED, CM_PKT_VALID_CENTRAL, CM_PKT_VALID_PERIPHERAL and CM_PKT_STATUS_UNDETERMINED.

Connection Monitor Demo

The SimpleLink Low Power F3 SDK ® ships with a demo that enables the user to run the Connection Monitoring functionality. This demo helps orient the user with the Connection Monitor feature, and with visualizing the output from the Connection Monitor.

In order to run the demo, the following pre-requisites must be fulfilled:

  • HW required to run the demo can be either of the combinations listed under:

    • 2 CC23xx or CC27xx launchpads + 1 phone

    • 3 CC23xx or CC27xx launchpads

  • The latest SimpleLink Low Power F3 SDK ®, using 9.11.xx.xx and above.

  • Installation of Python, version 3.10.xx, on your computer. Python version 3.10.11 can be downloaded from here

The following sections will list the necessary steps to prepare the host PC, and the CC23xx or CC27xx launchpads to successfully run the Connection Monitor Demo. Before getting into that, it is worthwhile to look at the block diagram for the Connection Monitor Demo, and understand the role of each block.

../_images/ditaa-149897c7ecae2586ac9655f53f6ef8621a8fbfb8.png

Notice that this block diagram looks different than the one shown earlier in this document where the Connection Monitor Node was directly connected to one of the BLE devices. Both ways are correct. What is important is that the Connection Monitor receives the connection information to start tracking the connection.

The Car Node behaves as a multi-role device (Central + Peripheral), while the Key Node, and the CM nodes are peripheral devices. Note that there are no limitations when it comes to which role the CMR device needs to be in. This demo is setup to use the Host PC as this can help emulate the presence of an external MCU which may act as the controller in applications like Car Access.

In the Out-of-Box Connection Monitor Demo, the Car Node, and the Connection Monitor (CM) node devices are controlled entirely by the Host PC, over UART. This means that these node devices wait to get UART commands from the Host PC, which controls the BLE behavior of these nodes. This includes controlling when the Car Node starts scanning, advertising, initiating a connection etc. Additionally, the Host PC provides the CM node with the connection information of the connection that needs to be monitored. The Host PC is also responsible for configuring the duration for which the connection needs to be monitored. Lastly, it is the Host PC that triggers the start of a connection monitoring session on the CM node. The Host PC, gets the connection information from the Car Node, which is then forwarded to the CM Node.

../_images/ditaa-c716f969af1e785b48fdcdd1266a6118a07bfa8c.png

Car Node, and the Connection Monitor nodes send event notifications to the Host PC over UART, which includes events like advertising reports, connection establishment events, connection monitor reports, and more. An example of what the information flow looks like is showcased in the figure above.

Setting up to run the Connection Monitor Demo

Setting up Host PC

Follow the steps mentioned below to prepare your host PC for running the Connection Monitor Demo:

  • With the SDK, and Python installed, using either Powershell or CMD Prompt, open the SDK installation folder. The SDK should normally be placed under C:/ti/.

    • With the terminal open, check to see that the correct version of Python is installed, and ready to use. You should see something similar to the image below:

../_images/Powershell_sdk.png

Figure 126. Powershell session with the SDK opened.

  • Navigate then to the tools\ble\ble_agent folder to setup the necessary python environment for running the demo by doig the following:

    • Run python -m pip install virtualenv to install the virtual environment module for Python. Using a virtual environment ensures that the Python modules installed inside of a virtual environment do not affect the global Python setup on your computer.

Note

The exact alias for running python through powershell command prompt may vary, for instance python3, py, python etc. Please check whichever one works for your system, and use the same

  • If your network is behind a proxy, then add the proxy flag like so: --proxy YOUR_PROXY_HERE to all the python commands. For instance: python -m pip install virtualenv --proxy YOUR_PROXY_HERE

  • Once the installation of the venv module is complete, initialize a virtual environment (venv) by running the following command in the shell terminal python -m venv .venv. This creates a venv in the YOUR_SDK\tools\ble\ble_agent folder.

  • Once the venv has been created, activate it by typing the following: .venv\Scripts\activate These steps are captured in the screenshot below:

../_images/Powershell_venv.png

Figure 127. Powershell session with the venv module installed and venv activated.

  • Once the venv is installed and activated, install the required python modules to run the demo by doing the following: pip install -r requirements.txt

Warning

If the previous step is not run, and the necessary requirements are not installed, it will cause the demo to fail, due to a lack of the required modules needed by the python code!

That wraps up the necessary steps required to setup your host PC for running the CM demo. Now, the launchpads need to be loaded with the correct FW to be enable them to run the Connection Monitor Demo.

Loading FW Images Onto launchpads

With the Host PC prepared with python installation, and the virtual environments, the next step is to prepare the CC23xx or CC27xx launchpads. In order to do so, follow these steps:

  • Start with opening Device Manger, and note down the Com Port for each of the 3 launchpads. This step is very essential for running the demo. It is essential that you note down the Com Port for the UART, and not the XDS. When using the Windows Device Manager to figure out the Com Ports for the launchpads, beware that each launchpad shows up as 2 Com Ports, where the XDS110 Class Application/UART Com Port is the one we need to use, not the XDS110 Class Auxiliary. Refer to the image below for an example:

../_images/choosing_comPorts.png

Figure 128. Choosing the correct Com Port

  • Start with importing the key_node example into CCS. Open SysConfig for this project, navigate to RCL under TI Drivers, and find the RF Observables setting. Here, enable the PA/LNA Pins (See highlighted rectangle in image below). It is recommended to enable these as this makes it easy to visualize what the radio is doing. This, in turn makes it easy to understand the CM’s behavior.

../_images/CM_LNA_PA.png

Figure 129. Enabling PA and LNA

  • Save the sysconfig changes, and build your project. Once the build succeeds, flash one of the launchpads with the key_node .out file. Make sure you have noted the Com port of this device.

  • Now import the car_node example from the SDK. As with the key_node example above, enables the PA/LNA pins for the car node example too. Save your changes, build and flash this project to the second and third launchpad. Note the com Ports for the two launchpads, and pick one to use as your car node. The com port will be used in the python script mentioned in the next section to run the connection monitoring demo. Make sure to note the Com port of the CM Node, as this will be used later.

This now concludes loading of the correct FW images onto the launchpad. The next step, is running the Connection Monitor Demo!

Running the Connection Monitor Demo

With the python environment prepped, and the necessary firmware loaded onto the launchpads, the Connection Monitor Demo can now be run. In order to do so, follow the steps listed hereunder:

  • Open the ble_device_car_node.py file which is available inside the SDK at the following location: YOUR_SDK\tools\ble\ble_agent\examples

  • In the ble_device_car_node.py script, find the line that says car_node = BleDevice( and here, for the device_comport, replace the com port with the actual com port of the car node device, for instance “COM13” if the car node device you chose uses the Com Port 13. For the car_node device, we want the Com Port of the device that was flashed with Connection Monitor feature disabled via SysConfig.

  • Do the same for the cmr_node, which will be the Connection Monitor node, in the ble_device_car_node.py file. Then, save the python file.

  • Make sure that all the launchpads are powered, have been flashed with correct FW, and that the correct Com Ports are being used in the Python script.

  • To run the demo, in the shell terminal window, with the python venv activated, navigate to the YOUR_SDK\tools\ble\ble_agent\examples folder, and run the following command: python .\examples\ble_device_car_node.py. This will kickoff the process shown in the information flow for the connection monitor.