OAD Application

OAD State Machine

The OAD service implements an ‘OAD State Machine’ for performing the OAD. The following state machine depicts the OAD service state transitions and its interactions with the OAD communication profile messages for both on-chip and off-chip OAD.

../_images/oad_state_machine.png

Figure 211. OAD Types Overview

The states and state transitions are encapsulated inside the OAD service, but some of the critical states are described below to aide in understanding.

Note these sections refer to internal state handling and transitions local to the target device. For a summary of the over the air sequence see Sequence diagram for OAD process and for a breakdown of the different types of profile messages and how to interpret them over the air please see BLE-Stack OAD Profile.

Image Validation

After establishing a new connection, updating the connection interval for a faster OAD and enabling notifications of OAD Image Identify and OAD Image Block characteristics on the OAD target, the OAD distributor shall write to the Image Identify characteristic of the OAD target. The message data will be the header retrieved from the OAD Image available for OAD.

On receiving the Image Identify message, the OAD target will get ready for OAD process.

Image Block Transfers

Once the OAD target is ready for receiving image, it will switch to the configuration state. There it will get the block size and set image count. When the OAD distributor sends the Start OAD Command to the Control Characteristic (for more details see OAD Control Characteristic Supported Commands.), the OAD target will respond with a Control characteristic notification requesting the first block. The OAD distributor will then send the first block to the OAD target.

This process continues with the OAD target notifying the OAD distributor of the next block it needs and the OAD distributor sending the requested image block until all blocks have been transferred.

Completion of the OAD Process

After receiving the complete image, OAD application will transit to OAD_COMPLETE state and then trigger a reset. After reset the secure bootloader will start the new image validation.