CC2340R5 to CC2340R53 Porting Guide¶
This section will describe, in general terms, how to migrate a project developed for the CC2340R5 device to a CC2340R53 device running the SimpleLink Low Power F3 SDK. However, it is important to first assess the differences between both devices to make sure that the project migration is possible (See Platform Devices Comparison).
The primary difference between CC2340R5 and CC2340R53 is the SRAM size, as specified in their respective datasheets. CC2340R5 has 36 kB SRAM, and CC2340R53 has 64 kB SRAM.
Migration Guide¶
The recommended migration path is to start with a CC2340R5 based example project from the SimpleLink Low Power F3 SDK and follow the next steps:
Import the project into Code Composer Studio or you IDE of preference.
Open SysConfig, go to
Device Viewand click onSWITCH.
Figure 270. SysConfig - Switch Device.¶
Once the
Switch Board or Devicewindow is opened, select the CC2340R53 board, or 64 kB device and click onCONFIRM. Make sure to save the project changes so that the migration takes place.
Figure 271. SysConfig - Select CC2340R53 device.¶
Warning
If a new linker command file is generated after migration (named cc23x0r53.cmd in the project files)
please make sure to exclude it from build (or eliminated it from the project files) so that the original
lpf3_app_freertos.cmd file is used during build time.
Build and flash the project.
Additional Steps for Off-Chip OAD and MCUBoot examples¶
For the MCUBoot project, additionaly to the device migration, modify the MCUBoot configuration inside SysConfig.
Enable Overwrite-only code path.
Enable External Flash configuration.
Modify the Base Address and Image Size depending on your application.
Figure 272. SysConfig - MCUBoot.¶
Build both projects.