.. _sec-mcuboot-oad-process:

OAD Application
===============

OAD State Machine
-----------------

The OAD service implements an 'OAD State Machine' for performing the OAD. The
following state machine depicts the OAD service state transitions and its
interactions with the OAD communication profile messages for both on-chip and
off-chip OAD.

.. _fig-mcuboot-oad-state-machine:
.. figure:: resources/oad_state_machine.png
    :align: center

    OAD Types Overview

The states and state transitions are encapsulated inside the OAD service, but
some of the critical states are described below to aide in understanding.

Note these sections refer to internal state handling and transitions local to
the target device. For a summary of the over the air sequence see
:ref:`fig-mcuboot-oad-sequence-diagram` and for a breakdown of the different types of
profile messages and how to interpret them over the air please see
:ref:`sect-mcuboot-oad-profile`.

Image Validation
""""""""""""""""

After establishing a new connection, updating the connection interval
for a faster OAD and enabling notifications of OAD Image Identify and
OAD Image Block characteristics on the OAD target, the
OAD distributor shall write to the Image Identify characteristic of the
OAD target. The message data will be the header retrieved from the OAD
Image available for OAD.

On receiving the `Image Identify` message, the OAD target will get ready
for OAD process.

Image Block Transfers
"""""""""""""""""""""

Once the OAD target is ready for receiving image, it will switch to
the configuration state. There it will get the block size and set image count.
When the OAD distributor sends the Start OAD Command to the Control
Characteristic (for more details see
:ref:`tbl-mcuboot-oad-control-supported-commands`), the OAD target will respond
with a Control characteristic notification requesting the first block. The OAD
distributor will then send the first block to the OAD target.

This process continues with the OAD target notifying the OAD distributor
of the next block it needs and the OAD distributor sending the requested
image block until all blocks have been transferred.

Completion of the OAD Process
"""""""""""""""""""""""""""""

After receiving the complete image, OAD application will transit to
*OAD_COMPLETE* state and then trigger a reset. After reset the secure
bootloader will start the new image validation.