.. _sec-l2cap:

Logical Link Control and Adaptation Layer Protocol (L2CAP)
----------------------------------------------------------

The L2CAP layer sits on top of the HCI layer on the host side and
transfers data between the upper layers of the host (GAP, GATT, SM,
application) and the link layer. This layer is
responsible for protocol multiplexing capability, segmentation, and
reassembly operation for data exchanged between the host and the
protocol stack. All data from the host or application goes through and is
encapsulated in an L2CAP packet. L2CAP permits higher-level protocols
(such as GATT and SM) and applications to transmit and receive upper layer data
packets (L2CAP service data units, SDU) up to 64KB long. See
:numref:`l2cap-architectural-blocks` for more information.

.. note::
    The actual L2CAP payload size is limited by the amount of memory
    available on the specific device being implemented. L2CAP also permits
    per-channel flow control and retransmission.

.. _l2cap-architectural-blocks:
.. figure:: resources/l2cap-architectural-blocks.jpg
    :align: center

    L2CAP Architectural blocks.

General L2CAP Terminology
^^^^^^^^^^^^^^^^^^^^^^^^^

.. _general-l2cap-terminology:
.. table:: General L2CAP Terminology

   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Term                                          |     Description                                                      |
   +=================================================+======================================================================+
   |   L2CAP channel                                 |     The logical connection between two endpoints in peer devices,    |
   |                                                 |     characterized by their Channel Identifiers (CIDs)                |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   SDU or L2CAP SDU                              |     Service Data Unit: a packet of data that L2CAP exchanges with    |
   |                                                 |     the upper layer and transports transparently over an L2CAP       |
   |                                                 |     channel using the procedures specified in this document.         |
   |                                                 |     This is the raw payload from the host/app, and does not include  |
   |                                                 |     L2CAP headers.                                                   |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   PDU or L2CAP PDU                              |     Protocol Data Unit: a packet of data containing L2CAP protocol   |
   |                                                 |     information fields, control information, and/or upper layer      |
   |                                                 |     information data. This packet includes L2CAP headers.            |
   |                                                 |     A single SDU may be split across multiple PDUs.                  |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Maximum Transmission Unit (MTU)               |     The maximum size of payload data, in octets, that the upper      |
   |                                                 |     layer entity can accept (that is, the MTU corresponds to the     |
   |                                                 |     maximum SDU size). Note: This is different than ATT\_MTU.        |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Maximum PDU Payload Size (MPS)                |     The maximum size of payload data in octets that the L2CAP        |
   |                                                 |     layer entity can accept (that is, the MPS corresponds to the     |
   |                                                 |     maximum PDU payload size).                                       |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Credit                                        |     The number of LE-frames that the device can receive.             |
   |                                                 |     Credits may range between 1 and 65535, and are used as a flow    |
   |                                                 |     control mechanism between devices.                               |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   L2CAP Basic Header                            |     L2CAP protocol information that is prepended to each PDU.        |
   |                                                 |     This includes CID and  length                                    |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Protocol/Service Multiplexer (PSM)            |     A two octet field that is used to define the interpretation of   |
   |                                                 |     L2CAP channel data. There are both dynamic and fixed PSMs.       |
   |                                                 |     Fixed PSMs are assigned by the SIG, while dynamic PSMs may       |
   |                                                 |     be discovered by GATT.                                           |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Fragmentation/Recombination                   |     Fragmentation is the process of breaking down L2CAP PDUs into    |
   |                                                 |     smaller pieces for the controller to send out.                   |
   |                                                 |     Recombination is the process of the controller reassembling      |
   |                                                 |     fragments into complete L2CAP PDUs.                              |
   |                                                 |     Fragmentation/Recombination is performed by the controller       |
   |                                                 |     and is based on the LE Data Length Extension feature.            |
   |                                                 |     Fragmentation/Recombination operations are transparent to L2CAP. |
   +-------------------------------------------------+----------------------------------------------------------------------+
   |   Segmentation/Reassembly                       |     Segmentation is the process of breaking a single L2CAP SDU up    |
   |                                                 |     multiple L2CAP packets called SDU segments. Reassembly in the    |
   |                                                 |     inverse of this operation on the receive side. Each segment is   |
   |                                                 |     encapsulated in a proper L2CAP header. Both segmentation and     |
   |                                                 |     reassembly is handled by the L2CAP layer and transparent to      |
   |                                                 |     lower and higher layers.                                         |
   +-------------------------------------------------+----------------------------------------------------------------------+

.. important::

    The max SDU size supported by the stack is ``L2CAP_SDU_SIZE``.


L2CAP Modes of Operation
^^^^^^^^^^^^^^^^^^^^^^^^

The |STACK| supports two different modes of operation of the L2CAP layer.

 * Basic L2CAP Mode
 * LE Credit Based Flow Control Mode

Note that the L2CAP section is shared for BR/EDR, BR/EDR/LE (dual mode), and
LE only controller implementations. The |STACK| controller implementation is
LE only, thus only the modes above are relevant.

.. _l2cap-channels:

L2CAP Channels
^^^^^^^^^^^^^^

There are three types of channels in L2CAP:

 * Connection-oriented
 * Connectionless data
 * L2CAP signaling

Each endpoint of an L2CAP channel is referred to by a channel identifier (CID).
See the Channel Identifiers section ([Vol 3], Part A, Section 2.1) of
the |CORESPEC| for more details on L2CAP Channel Identifiers. Connectionless
channels are not supported over the LE-U controller, and thus are not used by
the |STACK|.

Channels can be divided into fixed and dynamic channels.

Fixed Channels
~~~~~~~~~~~~~~

Fixed channels perform a specific L2CAP function, and use CIDs
between 0x0001 and 0x003F. The characteristics of each fixed channel (such as
MTU) are defined on a per channel basis.

.. tip::

    Higher level protocols such as ATT may enforce their own MTU, which is
    different than the L2CAP MTU.

The relevant CIDs that are available for use by the stack or application are
listed below.

.. _l2cap-cids:
.. table:: L2CAP CIDs

    +---------------+---------------------------------+--------------------------------------+
    | CID           | Description                     | Usage                                |
    +---------------+---------------------------------+--------------------------------------+
    | 0x0004        | Attribute Protocol (ATT)        | Sending ATT information              |
    +---------------+---------------------------------+--------------------------------------+
    | 0x0005        | LE Signaling Channel            | Sending L2CAP commands               |
    +---------------+---------------------------------+--------------------------------------+
    | 0x0006        | Security Manager Protocol (SMP) | Sending pairing/security information |
    +---------------+---------------------------------+--------------------------------------+
    | 0x0040-0x007F | Dynamically Allocated           | LE Credit Based Flow control packets |
    +---------------+---------------------------------+--------------------------------------+

For example, data exchanged over the GATT protocol uses channel 0x0004, SMP
(pairing and security) uses 0x0006, and the LE signaling channel uses 0x0005.
The ATT, SMP, and signaling channels are not directly accessible via the
application as they are used by their associated Host layers. Put another way,
when calling a GATT related API, it handles the necessary encapsulation into
an L2CAP packet. The signaling channel is used for L2CAP connection parameter
update procedure, establishing LE credit based connections on the
dynamic channels, and exchanging credits.


Dynamically Allocated Channels
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

A dynamically allocated CID is allocated to identify the logical link and the
local endpoint. The local endpoint must be in the range from 0x0040 to 0xFFFF.
This endpoint is used in the connection-orientated L2CAP channels described in
the following section. Credit Based Flow Control mode is used by the L2CAP
layer for Connection-Oriented Channels. These dynamically assigned channels
are accessible and managed directly at the application layer. This means that
the application is responsible for defining its own protocol on top of L2CAP
CoC. L2CAP channels are bidirectional and are analogous to sockets.

When a channel is dynamically allocated, it must have the following parameters
set:

 * PSM
 * MTU
 * CID

Fixed PSMs are defined by the Bluetooth SIG, these range between 0x0001 and
0x007F. Dynamic PSMs range between 0x0080 and 0x00FF. PSMs may be fixed on
GATT server devices, while GATT clients shall obtain PSMs from the GATT
service.


L2CAP Frame types
^^^^^^^^^^^^^^^^^

There are two frame types that are used by the |STACK|. These are the Basic
frame which is used by the fixed channels in basic mode, and the LE information
frame which is used by the dynamic channels in LE credit based flow control
mode. L2CAP handles framing of the SDU data from the host or application, but
it is important to keep the protocol overhead of each frame in mind as it will
affect how much application data ends up in a PDU.

The contents of the L2CAP frames are defined in Vol 3, Part A. The LE
information frame is defined in section 3.4 and the basic frame is defined in
section 3.1. The headers sizes are summarized here for reference.

.. _l2cap-frames:
.. table:: L2CAP Frames and Overhead

    +----------------------+----------------------+----------------------+
    | L2CAP Frame Type     | Header Size (octets) | Header contents      |
    +----------------------+----------------------+----------------------+
    | Basic frame          | 4                    | Length: 2 octets     |
    |                      |                      | CID: 2 octets        |
    +----------------------+----------------------+----------------------+
    | LE Information Frame | 6                    | Length: 2 octets     |
    |                      |                      | CID: 2 octets        |
    |                      |                      | SDU length: 2 octets |
    +----------------------+----------------------+----------------------+

.. _l2cap-fragmentation:

Fragmentation/Recombination
^^^^^^^^^^^^^^^^^^^^^^^^^^^

From an L2CAP perspective, all packets are delivered to and received from
the controller as complete packets. This means that fragmentation/recombination
(if enabled by LE Data Length Extension) is performed by the controller
and not visible to L2CAP. See :ref:`le_data_length_extension` for more
information.

When fragmentation is used, larger packets are split
into multiple link layer packets and reassembled by the link layer
of the peer device. The picture below shows this
relationship.


.. ditaa::
   :--no-separation:
   :--no-shadows:

                               +------------------------------------------+
       Application             |                   SDU cAAA               |
                               +------------------------------------------+
                                                     |
            -----------------------------------------|----------------------------------------
                                                     |
        L2CAP                                        v

               +------------------------------+               +------------------------------+
               |           PDU_1  cC00        |               |           PDU_n  cC00        |
               +------------+-----------------+               +------------+-----------------+
               |Header c156 | SDU_1 cAAA      | ............. |Header c156 | SDU_n cAAA      |
               +------------+-----------------+               +------------+-----------------+
                                                     

                        If SDU + L2CAP header is smaller or equals to the MAX_PDU_SIZE,
                        then in the L2CAP layer there will only be one packet which is
                        L2CAP header + SDU.

                                                     |
            -----------------------------------------|----------------------------------------
                                                     |
                                                     v
          
        Host                                 HCI_sendDataPkt

                                                     |
            -----------------------------------------|----------------------------------------
                                                     |
                                                     v

        Link Layer    Depends on the DLE PDU size to decide whether fragmentation is needed,
                      and then send packets over the air.                                        


.. note::
  The **DLE PDU** is negotiated by ``LL_LEN_REQ`` and ``LL_LEN_RSP``. DLE PDU is *NOT* the same 
  as L2CAP PDU. For more information regarding how to change the DLE PDU, see 
  :ref:`le_data_length_extension`.


.. _l2cap-segmentation:

Segmentation/Reassembly
^^^^^^^^^^^^^^^^^^^^^^^

When operating in Basic Mode, L2CAP will not perform any segmentation or
reassembly. However, when operating in LE Credit Based Flow Control mode on a
dynamic channel (CoC) segmentation and reassembly at the L2CAP layer may occur.


.. _l2cap-config:

Configuring L2CAP
^^^^^^^^^^^^^^^^^

.. _l2cap-enable-config:

Build Configuration
~~~~~~~~~~~~~~~~~~~

The L2CAP CoC dynamic channels by default is not enabled in the projects.
It can be enabled by the following methods:

.. ifconfig:: device != 'cc2640'
   
   **SysConfig tool**: For projects that support SysConfig tool, you can enable
   L2CAP CoC dynamic channels by checking ``L2CAP Connection Oriented Channels`` box.
   Please refer to :numref:`fig-ble5-stack-feature` for |STACK| feature overview.

-  **build_config.opt**: For projects that do not support SysConfig tool, you 
   can enable L2CAP CoC dynamic channels by adding ``-DV41_FEATURES=L2CAP_COC_CFG``
   to ``build_config.opt`` file.


Runtime Configuration
~~~~~~~~~~~~~~~~~~~~~

.. tip::
    This is a bit of a misnomer because generally these parameters are set
    via ``#define`` but they are in fact initialized dynamically at the time
    of the stack boot. In this case, runtime means that they not fixed by the
    protocol stack library and may be changed by the user.

.. ifconfig:: doctarget == 'ble3'

   These L2CAP parameters are passed into the |STACK| at initialization via the
   BLE user config structure (``ble_user_config.h``). These include:

.. ifconfig:: doctarget == 'ble5'

   These L2CAP parameters are passed into the |STACK| at initialization via the
   ``.opt`` file. These include:   

* ``L2CAP_NUM_PSM`` : Number of Protocol/Service multiplexers
* ``L2CAP_NUM_CO_CHANNELS`` : Number of allowed dynamic CoCs.
* ``MAX_PDU_SIZE``: Max PDU buffer size that the controller accepts
* ``MAX_NUM_PDU``: Number of L2CAP TX PDU buffers in the controller


   For more information for how to change the above parameters, please
   see :ref:`stack_features_configuration`


.. _l2cap-mtu:

L2CAP MTU
^^^^^^^^^

As mentioned in :ref:`general-l2cap-terminology`, the L2CAP MTU is the maximum
payload that can be processed by the L2CAP layer. The MTU size is the largest
SDU that L2CAP will accept.

However, the MTU used by L2CAP will vary depending on the mode and channel type

 * Signaling channel will use the ``L2CAP_SIG_MTU_SIZE``
 * Fixed channel packets are limited by ``MAX_PDU_SIZE - L2CAP_HDR_SIZE``
 * CoC packets depend on the PSM's MTU and are limited by ``L2CAP_SDU_SIZE``

For fixed channel MTU is defined by a higher level protocol such as ATT.
On dynamic connection oriented channels, the MTU is bound by the minimum of
``L2CAP_SDU_SIZE`` and the peer's supported MTU.

.. _l2cap-ram:

RAM Considerations
~~~~~~~~~~~~~~~~~~

Care must be taken with respect to RAM when enabling these features as they
will consume heap memory. Additionally, since L2CAP is responsible for
encapsulating packets from higher layers, the higher level protocols may have
requirements on how L2CAP is configured.


.. table:: L2CAP RAM Usage

    +---------------------------+---------------------------------------------------------------------+----------------------+
    | L2CAP Frame Type          | Heap Allocation                                                     | Alloc time           |
    +---------------------------+---------------------------------------------------------------------+----------------------+
    | ``L2CAP_NUM_PSM``         | sizeof(l2capPsm_t)*L2CAP_NUM_PSM                                    | L2CAP init           |
    |                           |                                                                     |                      |
    +---------------------------+---------------------------------------------------------------------+----------------------+
    | ``L2CAP_NUM_CO_CHANNELS`` | sizeof(l2capChannel_t)* (MAX_NUM_BLE_CONNS + L2CAP_NUM_CO_CHANNELS) | L2CAP Init           |
    +---------------------------+---------------------------------------------------------------------+----------------------+
    | ``L2CAP_NUM_CO_CHANNELS`` | sizeof( l2capCoChannel_t )                                          | Channel creation     |
    +---------------------------+---------------------------------------------------------------------+----------------------+
    | ``MAX_PDU_SIZE``          | Depends on application usage, can be up to MAX_PDU_SIZE*MAX_NUM_PDU | Runtime              |
    |                           | in TX case. In the RX case it depends on RX throughput              |                      |
    +---------------------------+---------------------------------------------------------------------+----------------------+
    | ``MAX_NUM_PDU``           | See above                                                           | Runtime              |
    +---------------------------+---------------------------------------------------------------------+----------------------+

The two parameters are only used by dynamic connection oriented channels,
and do not need to be considered if the feature is not used. ``MAX_PDU_SIZE``
and ``MAX_NUM_PDU`` as they do affect both the fixed channels used by ATT and
SM as well as the dynamic connection oriented channels.

When using connection oriented channels, L2CAP will allocate space for each TX
segment of the SDU before passing to the controller. The size is based on the
max packet size that is negotiated by the controller.

On RX, L2CAP will allocate the size of the entire SDU on receiving the first
packet based on the length field in the header.

For signaling commands on the fixed channels, L2CAP will allocate the memory
for the packet itself, based on ``L2CAP_SIG_MTU_SIZE`` which is the MTU of the
signaling channel.

.. tip::
    For data packet payloads, the higher level protocol (ATT, SM, Application)
    is responsible for allocating using ``L2CAP_bm_alloc(...)``. In the case
    of ATT and SM, this is done transparent to the user. For CoC SDUs, the user
    owns the memory associated with the payload.


.. _l2cap-flow-ctrl:

Controller to Host Flow Control
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

As mentioned above, ``MAX_NUM_PDU`` defines the max number of TX packets that
can be queued up to the controller at a time. Attempting to send more packets
will result in a failure code being returned by the high level API and the
packet not being queued up by the controller.

The application may not know how many packets are queued up at a given time
so it is best to always check return codes. Additionally, the application
can increase the efficiency at which is queues packets up by registering
for flow control notifications from the L2CAP layer.

This can be done with :ble_api:`L2CAP_RegisterFlowCtrlTask`. When enabled,
the API will notify the application with ``L2CAP_NUM_CTRL_DATA_PKT_EVT`` with
the number of data packets that are available for sending. This event is
triggered each time a new buffer becomes available.

Connection Oriented Channels Example
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

.. ifconfig:: device != 'cc23xx'

  The |STACK| provides APIs to create L2CAP CoC channels to transfer
  bidirectional data between two Bluetooth Low Energy devices supporting this
  feature. Following are the steps and generic code example which are needed
  to create L2CAP CoC channels communication using TI |STACK|.
  
  #. **Enable L2CAP CoC Feature**, please refer to :ref:`l2cap-enable-config`
  
  #. **Register Simplified Protocol/Service Multiplexer (SPSM)**. 
     :term:`SPSM` registration is needed for both central and peripheral devices.
      
      .. code-block:: c
       :caption: Register SPSM
       :linenos:
  
       #define App_SPSM      0x0080
          
       static void application_openL2CAPChanCoc(void)
       {
          
         l2capPsm_t psm;
         l2capPsmInfo_t psmInfo;
          
         if (L2CAP_PsmInfo(App_SPSM, &psmInfo) == INVALIDPARAMETER)
         {
           // Prepare the PSM parameters
           psm.initPeerCredits = 0xFFFF;
           psm.maxNumChannels = MAX_NUM_BLE_CONNS;
           psm.mtu = MAX_PDU_SIZE;
           psm.peerCreditThreshold = 0;
           psm.pfnVerifySecCB = NULL;
           psm.psm = App_SPSM;
           psm.taskId = ICall_getLocalMsgEntityId(ICALL_SERVICE_CLASS_BLE_MSG, selfEntity);
          
           // Register SPSM with L2CAP task
           L2CAP_RegisterPsm(&psm);        
         }
         else
         {
           // print L2CAP setup failed
         }
          
       }
  
      .. tip::
        This function might be called at the end of the
        ``GAP_DEVICE_INIT_DONE_EVENT``.
  
  #. Central or peripheral device sends **L2CAP LE Credit Based Connection Request**.
  
      .. code-block:: c
       :caption: Sends out L2CAP LE Credit Based Connection Request
       :linenos:
       
  
       // Send out L2CAP_LE_CREDIT_BASED_CONNECTION_REQ
       L2CAP_ConnectReq(connHandle, App_SPSM, App_SPSM);
  
      .. note::
          Both central and peripheral device can request to establish L2CAP CoC channels.
          As long as one of the device requests, the link establishment request will be sent.
          There is no need to add this part of the code for both devices.
  
      .. tip::
        This function might be called at the end of the
        ``GAP_LINK_ESTABLISHED_EVENT``.
  
  #. Once the L2CAP credit based connection establishment is successful, the |STACK| will 
     send ``L2CAP_SIGNAL_EVENT`` to the application with opcode 
     ``L2CAP_CHANNEL_ESTABLISHED_EVT`` for both central and peripheral devices.
     Therefore, we will **implement a function to handle L2CAP messages**
     under application process stack message function.
  
      .. code-block:: c
       :caption: Process L2CAP event 
       :linenos:
  
       static uint8_t Application_processStackMsg(ICall_Hdr *pMsg)
       {
       
         switch (pMsg->event)
         {
       
           case L2CAP_SIGNAL_EVENT:
             Application_processL2CAPSignalEvent((l2capSignalEvent_t *)pMsg);
             break;
  
             ...
             ...
  
  
      .. code-block:: c
       :caption: Process L2CAP events 
       :linenos:
  
       // Connected device information.
       // If this structure already exists, it is sufficient to add the cocCID.
       typedef struct
       {
         uint16_t connHandle;        // Connection Handle
         uint16_t charHandle;        // Characteristic Handle
         uint8_t  addr[B_ADDR_LEN];  // Peer Device Address
         Clock_Struct *pRssiClock;   // pointer to clock struct
         uint16_t cocCID;            // CID for the L2CAP channel
       } connRec_t;  
       
       /******************************************************************************
       * @fn          Application_processL2CAPSignalEvent
       *
       * @brief       This function is used to handle all the L2CAP signal events.
       *
       * @param       pMsg - pointer to the signal that was received
       *
       * @return      None.
       */
       static void Application_processL2CAPSignalEvent(l2capSignalEvent_t *pMsg)
       {
         // Sanity check
         if (!pMsg)
         {
           return;
         }
       
         switch (pMsg->opcode)
         {
           case L2CAP_CHANNEL_ESTABLISHED_EVT:
           {
             l2capChannelEstEvt_t *pEstEvt = &(pMsg->cmd.channelEstEvt); 
             
             if (pMsg->connHandle != LINKDB_CONNHANDLE_INVALID && pMsg->connHandle < MAX_NUM_BLE_CONNS)
             {
               // Successfully establish link over L2CAP
               // Extract the CID and store in the application layer
               // This will be useful when sending data over L2CAP channels
               connList[pMsg->connHandle].cocCID = pEstEvt->CID;
             }
             else
             {
               // Could not establish an L2CAP link
             }
           }
           break;
       
           case L2CAP_SEND_SDU_DONE_EVT:
           {
             if (pMsg->hdr.status == SUCCESS)
             {
              // Successfully sending data over L2CAP
             }
             else
             {
             }
           }
           break;
       
           case L2CAP_CHANNEL_TERMINATED_EVT:
           {
           }
           break;
         }
       }
  
  #. Both peripheral and central devices need to **exchange L2CAP Credits**.
     After the link is established, devices can distribute credit using the
     following code snippet.
  
      .. code-block:: c
       :caption: Exchange credits 
       :linenos:
  
       l2capChannelEstEvt_t *pEstEvt = &(pMsg->cmd.channelEstEvt);
          
       // Give max credits to the other side
       L2CAP_FlowCtrlCredit(pEstEvt->CID, 0xFFFF);
          
  
      .. tip::
        This code can be placed when application receives successful 
        ``L2CAP_CHANNEL_ESTABLISHED_EVT``.
  
  #. **Send data using L2CAP CoC channel**. In order to send data over L2CAP,
     :ble_api:`L2CAP_SendSDU` is needed. After successfully sending data over
     the air, the |STACK| will send ``L2CAP_SIGNAL_EVENT`` to application with 
     opcode ``L2CAP_SEND_SDU_DONE_EVT``.
  
      .. code-block:: c
       :caption: Sending data over L2CAP
       :linenos:
  
       static bStatus_t Application_sendL2capData(void)
       {
         l2capPacket_t pkt;
         bStatus_t status = SUCCESS;
         uint8_t appData[] = "Example Data!";
       
         // Tell L2CAP the desired Channel ID
         pkt.CID = connList[connIndex].cocCID;
       
         // Allocate space for payload
         pkt.pPayload = L2CAP_bm_alloc(sizeof(appData));
         
         // Copy payload data
         memcpy(pkt.pPayload, appData, sizeof(appData));
         
         if (pkt.pPayload != NULL)
         {
  
           pkt.len = (sizeof(appData));
           status = L2CAP_SendSDU(&pkt);
         
           // Check that the packet was sent
           if (SUCCESS != status)
           {
             // If SDU wasn't sent, free
             BM_free(pkt.pPayload);
           }
         }
         else
         {
           status = bleMemAllocError;
         }
     
         return (status);
       }
  
  #. **Process received data over L2CAP**. When device receives data from L2CAP,
     the |STACK| will send ``L2CAP_DATA_EVENT`` to the application. Therefore, we will
     handle this under application process stack message function.
  
      .. code-block:: c
       :caption: Received data over L2CAP
       :linenos:
  
       static uint8_t Application_processStackMsg(ICall_Hdr *pMsg)
       {
        
          switch (pMsg->event)
          {
            case L2CAP_DATA_EVENT:
              Application_processL2CAPDataEvent((l2capDataEvent_t *)pMsg);
              break;   
  
              ...
              ...
  
  
      .. code-block:: c
       :caption: Extract data received over L2CAP
       :linenos:            
  
       /******************************************************************************
       * @fn          Application_processL2CAPDataEvent
       *
       * @brief       This function is used to handle the L2CAP data extraction.
       *
       * @param       pMsg - pointer to the signal that was received
       *
       * @return      None.
       */
       static void Application_processL2CAPDataEvent(l2capDataEvent_t *pMsg)
       {
           if (!pMsg)
           {
             // Caller needs to figure out by himself that pMsg is NULL
             return;
           }
  
           // The data locates under pMsg->pkt.pPayload
           // Extract the data and do what you want to do
           // For example:
           //Display_printf(dispHandle, 19, 0, "L2CAP data Rx: %s", pMsg->pkt.pPayload);
  
           // Free the payload (must use BM_free here)
           BM_free(pMsg->pkt.pPayload);
       }

.. ifconfig:: device == 'cc23xx'

  The |STACK| provides APIs to create L2CAP CoC channels to transfer
  bidirectional data between two Bluetooth Low Energy devices supporting this
  feature. Following are the steps and generic code example which are needed
  to create L2CAP CoC channels communication using **basic_ble** framework.
  
  #. **Enable L2CAP CoC Feature**, please refer to :ref:`l2cap-enable-config`
    
  #. **Create file app_l2cap.c and add it to the project --> app folder**. This
     file will contain most of the changes needed for using L2CAP CoC Channels.
     Therefore, create a new file app_l2cap.c inside the **app** folder of the
     **basic_ble** project.
    
  #. **Includes**. The new created file should contain the following includes.
    
     .. code-block:: c
       :caption: Includes of app\_l2cap.c
       :linenos:
       
       //*****************************************************************************
       //! Includes
       //*****************************************************************************
       #include <stdio.h>
       #include <string.h>
       #include "ti_ble_config.h"
       #include <ti/bleapp/ble_app_util/inc/bleapputil_api.h>
       #include <ti/bleapp/menu_module/menu_module.h>
       #include <app_main.h>
    
  #. **Define APP_L2CAP_SPSM**. Since this constant needs to get accessed from
     several files, this definition should be placed in app_main.h.
     
     .. code-block:: c
       :caption: Define of APP_L2CAP_SPSM in app_main.h.
       :linenos:
       
       //The valid range for SPSM is 0x0080 ~ 0x00FF, 0x0080 is used as an example.
       #define APP_L2CAP_SPSM      0x0080
       
     
  #. **Event Handlers**. The L2CAP CoC implementation requires the setup and
     registration of two event handlers with its corresponding masks, one for
     L2CAP signals and one for L2CAP data.
     
     .. code-block:: c
       :caption: Event Handlers of app\_l2cap.c
       :linenos:
       
       //*****************************************************************************
       //! Globals
       //*****************************************************************************
       
       static void L2CAP_SIGNAL_EventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData);
       static void L2CAP_DATA_EventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData);
       
       // Events handlers struct, contains the handlers and event masks
       // of the application data module
       BLEAppUtil_EventHandler_t data_L2CACAP_SIGNAL_Handler =
       {
           .handlerType    = BLEAPPUTIL_L2CAP_SIGNAL_TYPE,
           .pEventHandler  = L2CAP_SIGNAL_EventHandler,
           .eventMask      = BLEAPPUTIL_L2CAP_CHANNEL_ESTABLISHED_EVT |
                             BLEAPPUTIL_L2CAP_CHANNEL_TERMINATED_EVT |
                             BLEAPPUTIL_L2CAP_SEND_SDU_DONE_EVT
       };
       
       BLEAppUtil_EventHandler_t data_L2CACAP_DATA_Handler =
       {
           .handlerType    = BLEAPPUTIL_L2CAP_DATA_TYPE,
           .pEventHandler  = L2CAP_DATA_EventHandler
       };
       
       ...
       
       // Holds the connection ID
       static uint16_t cocCID;
       
       bStatus_t Application_sendL2capData(void);
     
     The registration of the event handlers will be done as part of the L2CAP
     initialization function.
     
     .. code-block:: c
       :caption: L2cap\_start function of app\_l2cap.c
       :linenos:
       :emphasize-lines: 19, 20
       
       //*****************************************************************************
       //! Functions
       //*****************************************************************************
       
       /*********************************************************************
        * @fn      L2cap_start
        *
        * @brief   This function is called after stack initialization,
        *          the purpose of this function is to initialize and
        *          register the L2CAP CoC functionality.
        *
        * @return  SUCCESS, errorInfo
        */
       bStatus_t L2cap_start( void )
       {
           bStatus_t status = SUCCESS;
       
           // Register the handlers
           status = BLEAppUtil_registerEventHandler( &data_L2CACAP_SIGNAL_Handler );
           status = BLEAppUtil_registerEventHandler( &data_L2CACAP_DATA_Handler );
       
           // ...
       }
       
     
  #. **L2CAP Initialization**. As briefly mentioned earlier in this chapter,
     the L2CAP CoC initialization is done with function L2cap_start. This
     function also setting up and registering the SPSM (Simplified
     Protocol/Service Multiplexer).
     
     .. code-block:: c
       :caption: Initialize L2CAP in app\_l2cap.c
       :linenos:
       :emphasize-lines: 21
       
       bStatus_t L2cap_start( void )
       {
           // ...
       
           // Setup SPSM
           l2capPsm_t psm;
           l2capPsmInfo_t psmInfo;
       
           if (L2CAP_PsmInfo(APP_L2CAP_SPSM, &psmInfo) == INVALIDPARAMETER)
           {
             // Prepare the PSM parameters
             psm.initPeerCredits = 0xFFFF; //give peer maximum credit
             psm.maxNumChannels = MAX_NUM_BLE_CONNS;
             psm.mtu = MAX_PDU_SIZE;
             psm.peerCreditThreshold = 0;
             psm.pfnVerifySecCB = NULL;
             psm.psm = APP_L2CAP_SPSM;
             psm.taskId = ICall_getLocalMsgEntityId(ICALL_SERVICE_CLASS_BLE_MSG, BLEAppUtil_getSelfEntity());
       
             // Register SPSM with L2CAP task
             status = L2CAP_RegisterPsm(&psm);
           }
           else
           {
             // L2CAP setup failed
             status = FAILURE;
           }
           
           // Return status value
           return( status );
       }
     
     Call **L2cap_start** from the ``App_StackInitDoneHandler`` in file
     app_main.c.
     
     .. code-block:: c
       :caption: L2cap\_start in app\_main.c
       :linenos:
       :emphasize-lines: 5
       
       void App_StackInitDoneHandler(gapDeviceInitDoneEvent_t *deviceInitDoneData)
       {
           ...
           
           status =  L2cap_start();
           if(status != SUCCESS)
           {
               // Call Error Handler
           }
           
  
  #. Central or peripheral device sends **L2CAP LE Credit Based Connection
     Request**. This request can be done at the end of the
     BLEAPPUTIL_LINK_ESTABLISHED_EVENT in app_connection.c.
     
     .. code-block:: c
       :caption: **app\_connection.c** Sends out L2CAP LE Credit Based Connection Request
       :linenos:
       :emphasize-lines: 10
       
       void Connection_ConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
       {
           ...
           
           case BLEAPPUTIL_LINK_ESTABLISHED_EVENT:
           {
               ...
               
               // Send out L2CAP_LE_CREDIT_BASED_CONNECTION_REQ, only one side needs to do this
               L2CAP_ConnectReq(gapEstMsg->connectionHandle, APP_L2CAP_SPSM, APP_L2CAP_SPSM);
            
               break;
           }
     
     .. note::
       Both central and peripheral device can request to establish L2CAP CoC
       channels. As long as one of the device requests, the link establishment
       request will be sent. There is no need to add this part of the code for
       both devices. In this example the code is added for the central device
       only.
     
     Once the L2CAP credit based connection establishment is successful, the
     |STACK| will send ``BLEAPPUTIL_L2CAP_SIGNAL_TYPE`` through the application
     data module with opcode ``BLEAPPUTIL_L2CAP_CHANNEL_ESTABLISHED_EVT`` for
     both central and peripheral devices.
     Therefore, we will implement a event handler function to handle L2CAP
     messages in app_l2cap.c.
     
     .. code-block:: c
       :caption: **app\_l2cap.c** Process L2CAP signal event 
       :linenos:
       
       //*****************************************************************************
       //! Functions
       //*****************************************************************************
       
       ...
       
       /*********************************************************************
        * @fn      L2CAP_SIGNAL_EventHandler
        *
        * @brief   The purpose of this function is to handle L2CAP signal
        *          events which were registered in
        *          @ref BLEAppUtil_registerEventHandler
        *
        * @param   event - message event.
        * @param   pMsgData - pointer to message data.
        *
        * @return  none
        */
       static void L2CAP_SIGNAL_EventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
       {
         l2capSignalEvent_t *l2capMsg = ( l2capSignalEvent_t * )pMsgData;
       
         switch (event)
         {
           case BLEAPPUTIL_L2CAP_CHANNEL_ESTABLISHED_EVT:
             {
                 l2capChannelEstEvt_t *pEstEvt = &(l2capMsg->cmd.channelEstEvt);
       
                 if (l2capMsg->connHandle != LINKDB_CONNHANDLE_INVALID && l2capMsg->connHandle < MAX_NUM_BLE_CONNS)
                 {
                   // Successfully establish link over L2CAP
                   // Extract the CID and store in the application layer
                   // This will be useful when sending data over L2CAP channels
                   cocCID = pEstEvt->CID;
                 }
                 else
                 {
                   // Could not establish an L2CAP link
                 }
       
                 // Give max credits to the other side
                 L2CAP_FlowCtrlCredit(pEstEvt->CID, 0xFFFF);
       
                 // Send test data
                 Application_sendL2capData();
             }
             break;
       
           case BLEAPPUTIL_L2CAP_SEND_SDU_DONE_EVT:
             {
                 if (l2capMsg->hdr.status == SUCCESS)
                 {
                     // Successfully sending data over L2CAP
                 }
             }
             break;
       
           case BLEAPPUTIL_L2CAP_CHANNEL_TERMINATED_EVT:
             {
                 // L2CAP channel has been terminated
                 MenuModule_printf(13, 0, "L2CAP terminated");
             }
             break;
       
           default:
             break;
         }
       }
      
     .. note::
       Both peripheral and central devices need to **exchange L2CAP Credits**.
       After the link is established, devices can distribute credit using
       ``L2CAP_FlowCtrlCredit`` as shown in the listing above.
  
  #. **Send data using L2CAP CoC channel**. In order to send data over L2CAP,
     :ble_api:`L2CAP_SendSDU` is needed. Therefore, we will implement a
     function `Application_sendL2capData` in app_l2cap.c and executed it for
     the ``BLEAPPUTIL_L2CAP_CHANNEL_ESTABLISHED_EVT``. After successfully
     sending data over the air, the |STACK| will send
     ``BLEAPPUTIL_L2CAP_SIGNAL_TYPE`` through the application data module with
     opcode ``BLEAPPUTIL_L2CAP_SEND_SDU_DONE_EVT``.
     
     .. code-block:: c
       :caption: Sending data over L2CAP in app\_l2cap.c
       :linenos:
       :emphasize-lines: 31
       
       //*****************************************************************************
       //! Functions
       //*****************************************************************************
       
       ...
       
       uint8_t appData[] = "Test Data!";
       
       bStatus_t Application_sendL2capData(void)
       {
         l2capPacket_t pkt;
         bStatus_t status = SUCCESS;
       
         // Tell L2CAP the desired Channel ID
         pkt.CID = cocCID;
       
         // Allocate space for payload
         pkt.pPayload = L2CAP_bm_alloc(sizeof(appData));
       
         /* Copy payload data */
         memcpy(pkt.pPayload, appData, sizeof(appData));
       
         if (pkt.pPayload != NULL)
         {
           pkt.len = (sizeof(appData));
       
           // Print transmit data to serial terminal, expected data is /0 terminated
           MenuModule_printf(11, 0, "L2CAP Data TX - %s", pkt.pPayload);
       
           // Send packet
           status = L2CAP_SendSDU(&pkt);
       
           // Check that the packet was sent
           if (SUCCESS != status)
           {
             // If SDU wasn't sent, free
             BM_free(pkt.pPayload);
           }
         }
         else
         {
           status = bleMemAllocError;
         }
       
         return (status);
       }
     
     When the device receives data from L2CAP, the |STACK| will send
     ``BLEAPPUTIL_L2CAP_DATA_TYPE`` to the application data module. Therefore,
     we will implement a function to handle L2CAP data in app_l2cap.c.
     
     .. code-block:: c
       :caption: Received data over L2CAP
       :linenos:
       
       //*****************************************************************************
       //! Functions
       //*****************************************************************************
       
       ...
       
       /*********************************************************************
        * @fn      L2CAP_DATA_EventHandler
        *
        * @brief   The purpose of this function is to handle L2CAP data
        *          events that rise from the GAP and were registered in
        *          @ref BLEAppUtil_RegisterGAPEvent
        *
        * @param   event - message event.
        * @param   pMsgData - pointer to message data.
        *
        * @return  none
        */
       static void L2CAP_DATA_EventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
       {
         if (!pMsgData)
         {
           // Caller needs to figure out by himself that pMsg is NULL
           return;
         }
       
         l2capDataEvent_t *l2capDataEventData = ( l2capDataEvent_t * )pMsgData;
       
         // Print received data to serial terminal, expected data is /0 terminated
         MenuModule_printf(12, 0, "L2CAP Data RX - %s", l2capDataEventData->pkt.pPayload);
       }
      
  
  #. **Close L2CAP CoC channel**. If no longer needed, you can disconnect a
     L2CAP CoC channel with the following function call, for example after data
     was sent successfully in function ``Application_sendL2capData``.
     
     .. code-block:: c
       :caption: Close the L2CAP CoC channel in app\_l2cap.c
       :linenos:
       :emphasize-lines: 16
       
       bStatus_t Application_sendL2capData(void)
       {
          // ...
          
          // Send packet
          status = L2CAP_SendSDU(&pkt);
          
          // Check that the packet was sent
          if (SUCCESS != status)
          {
              // If SDU wasn't sent, free
              BM_free(pkt.pPayload);
          }
          else
          {
               status = L2CAP_DisconnectReq(cocCID);
          }
          
          // ...
     
     The disconnect will then trigger the
     ``BLEAPPUTIL_L2CAP_CHANNEL_TERMINATED_EVT`` in the
     ``L2CAP_SIGNAL_EventHandler``. Here you could also deregister the SPSM by
     calling the function ``L2CAP_DeregisterPsm``.

The :numref:`sample-connection-central-peripheral` shows a sample connection
and data exchange process between central and peripheral device using a L2CAP
connection-oriented channel in LE Credit Based Flow Control Mode.

.. _sample-connection-central-peripheral:
.. uml::
  :caption: L2CAP Connection Oriented Channels Example
  :align: center

   @startuml
    participant Central
    participant Peripheral

    rnote over Central
    Resgister PSM
    end note

    rnote over Peripheral
    Register PSM
    end note

    == Connection Established  ==

    Central --> Peripheral : L2CAP_ConnectReq()
    Central -> Central : L2CAP_SIGNAL_EVENT\nL2CAP_CHANNEL_ESTABLISHED_EVT
    Peripheral -> Peripheral : L2CAP_SIGNAL_EVENT\nL2CAP_CHANNEL_ESTABLISHED_EVT

    Central <--> Peripheral : L2CAP_FlowCtrlCredit()

    group Central device sends data to peripheral device
      Central --> Peripheral : L2CAP_SendSDU()
      Central -> Central: L2CAP_SIGNAL_EVENT\nL2CAP_SEND_SDU_DONE_EVT
      Peripheral-> Peripheral: L2CAP_DATA_EVENT
      rnote over Peripheral
        App task process data
      end note
    end

    group Peripheral device sends data to central device    
      Peripheral --> Central : L2CAP_SendSDU()
      Peripheral -> Peripheral: L2CAP_SIGNAL_EVENT\nL2CAP_SEND_SDU_DONE_EVT
      Central-> Central: L2CAP_DATA_EVENT
      rnote over Central
        App task process data
      end note
    end

    Central --> Peripheral : L2CAP_DisconnectReq()
    Central -> Central : L2CAP_SIGNAL_EVENT\nL2CAP_CHANNEL_TERMINATED_EVT
    Peripheral -> Peripheral : L2CAP_SIGNAL_EVENT\nL2CAP_CHANNEL_TERMINATED_EVT

    Central <-> Peripheral : L2CAP_DeregisterPsm()
  @enduml