RF Testing using BTool
----------------------

.. note:: For a step by step explanation about how to execute a sequence of
          commands for testing, please refer to the Application Note on
          |HowtoDoRFTestBTOOL|. Please consider that this guide has been
          specially developed for CC26xx devices but is still applicable
          for CC23xx devices considering differences in commands (such
          for CC23xx & CC27xx devices considering differences in commands (such
          as the ones used for setting TX Power). Information related to 
          Packet Error Rate (PER) and RSSI measurements can be found there.

Tool Configuration
^^^^^^^^^^^^^^^^^^

1. In order to set the device to perform RF tests, we need an image capable
   of receive and executing HCI commands.

    * Flash the device with the respective ``host_test example``, which
      can be found inside the SDK folder
      ``<SDK>/examples/rtos/LP_EM_CC23xx/ble/host_test``.
      It is also possible to use projects that have Production Test Mode
      ``<SDK>/examples/rtos/DEVICE/ble/host_test``.
      Specifically for CC23xx, It is also possible to use projects that have Production Test Mode
      (PTM) enabled functionalities such as the example found in
      ``<SDK>/examples/rtos/LP_EM_CC2340R5/ble/basic_ble_ptm``.
      You can import the project in CCS or IAR and tune it to fit your own
      design (e.g. change the UART mapping).
    * If your design allows it (or if you are running the tests on a TI
      LaunchPad), you can directly flash the pre-built hexfile on the device.
      To do so, use UniFlash_ and use the following image 
      ``<SDK>/examples/rtos/DEVICE/ble/prebuilt_hexfiles/host_test_app.hex``.
      ``<SDK>/examples/rtos/DEVICE/ble/prebuilt_hexfiles/host_test_app.hex``.
    * Finally, it is recommended to power cycle the device after flashing it.

2. BTool can be found within the SDK. Execute the file
   ``<SDK>/tools/ble/btool/btool.exe`` to open the tool.

3. When opening BTool, you are prompted to select the COM interface used
   by your device. Make sure to choose the interface ``COMXX - XDS110
   Class Application/User UART``.

.. figure:: resources/btool_step3.PNG
    :align: center 

    Btool Prompt.

4. At start BTool automatically sends a few commands to the device.
   These commands are not relevant for this use case, so just wait
   for the commands to be executed, then right click on the log and
   click ``Clear Log``.

5. Move to the panel ``Advanced Commands``. From this panel you can
   send commands to the device. For this use case, the commands within
   ``HCI Extended`` and ``HCI`` should be the most useful.

6. Send a reset command ``HCI_Reset``. A UART command is sent to 
   the device (displayed in green) and the device resets and sends
   back an answer.

.. _btool_screen:
.. figure:: resources/Btool.png
    :align: center
    
    BTool interface - Advanced Commands

Assuming you have reached this point, it means the device is properly
flashed, the UART commands are properly sent and executed by the device.
Now we can look at sending more test commands to the device.

7. The HCI commands are specified by the Bluetooth Specifications.
   In order to offer more testing possibilities, these commands are
   completed by HCI Extended commands. Documentation for all these
   commands can be found in the
   commands for both CC23xx and CC27xx can be found in the
   `API references section of the user's guide <../ble-stack-5.x-guide/api-reference-cc23xx.html>`_.

8. Only a subset of the commands will be used for testing (see below).
   Commands in bold are the ones commonly used:

    Continuous Wave (Non-signaling)
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | **Command**                            | **Parameters**                       | **Comments**                             |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_Reset                              | none                                 | To reset the device                      |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_EndModemTestCmd                 | none                                 | To terminate a modem test                |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_ModemTestTxCmd                  | Modulation, Channel                  | For the 1M PHY only                      |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_ModemTestRxCmd                  | Channel                              | For the 1M PHY only                      |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_EnhancedModemTestTxCmd          | Modulation, PHY, Channel             |                                          |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_EnhancedModemTestRxCmd          | PHY, Channel                         |                                          |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_ReadRssi                           | none                                 | To read RSSI                             |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_SetTxPowerDbmCmd                | dBm, fraction (not used)             | To set TxPower for modem tests           |
      +----------------------------------------+--------------------------------------+------------------------------------------+
     
    Direct Test Mode - DTM (Signaling)
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | **Command**                            | **Parameters**                       | **Comments**                             |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_Reset                              | none                                 | To reset the device                      |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_LE_TestEnd                         | none                                 | To terminate a DTM test                  |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_LE_TransmitterTest                 | Channel, Data Length, Data           | For the 1M PHY only                      |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_LE_ReceiverTest                    | Channel                              | For the 1M PHY only                      |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_LE_EnhancedTransmitterTest         | Channel, Data Length, Payload, PHY   | Payload to be selected from DTM standard |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_LE_EnhancedReceiverTest            | Channel, PHY, modulationIndex        |                                          |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCI_ReadRssi                           | none                                 | To read RSSI                             |
      +----------------------------------------+--------------------------------------+------------------------------------------+
      | HCIExt_SetMaxDtmTxPowerDbmCmd          | dBm, fraction (not used)             | To set TxPower for DTM tests             |
      +----------------------------------------+--------------------------------------+------------------------------------------+
     

Hands-on Examples
^^^^^^^^^^^^^^^^^
Let's try some of them! You will be able to see the log that is produced in
BTool. Highlighted in yellow are the commands to send and the parameters you
should make sure to set. Highlighted in blue are the events received from the
device (a non-SUCCESS answer means there has been an issue).
Always remember to end the previous test before starting a new one.
   
- **Example 1:** Set the device to transmit at 8dBm a Continuous Wave with
  2M PHY on channel 1.

.. figure:: resources/btool_example_1.PNG
    :align: center
    
    Display of command execution using Btool.

- **Example 2:** Set the device to transmit at 8dBm a Continuous Wave with
  2M PHY on channel 4.
  1M PHY on channel 4.

.. figure:: resources/btool_example_2.PNG
    :align: center
    
    Display of command execution using Btool.

- **Example 3:** Set the device to transmit DTM packets at 5 dBm with 1M PHY
  on channel 36 with 37-byte payload of PRBS9.

.. figure:: resources/btool_example_3.PNG
    :align: center
    
    Display of command execution using Btool.

- **Example 4:** Set the device to transmit DTM packets at 5 dBm with 1M
  PHY on channel 36 with 37-byte payload of 0b11110000.

.. figure:: resources/btool_example_4.PNG
    :align: center
    
    Display of command execution using Btool.

- **Example 5:** Set the device to receive a Continuous Wave before ending it.

.. figure:: resources/btool_example_5.PNG
    :align: center 
    
    Display of command execution using Btool.

.. warning:: Command parameters (such as channel number, payload, TX power, etc) 
             cannot be changed while a test is running. To perform such changes, 
             you need to stop the current test by issuing the proper end commands.


Direct Test Mode (DTM) & Continuous Wave (CW) testing with basic_ble example
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

Now, let's try to do both DTM and CW testing using the basic_ble example.
First, make sure that the device is in peripheral mode from the SysConfig.

.. figure:: resources/basicBLE_SysConfig.PNG
    :align: center 

    Sysconfig Page of Basic BLE Example.

Direct Test Mode 
^^^^^^^^^^^^^^^^

1. From ``app_peripheral.c :: Peripheral_start()``, comment out the code which initializes and starts the advertising.

.. code-block:: c

  //Do not start advertising when entering DTM
    // status = BLEAppUtil_initAdvSet(&peripheralAdvHandle_1, &advSetInitParamsSet_1);
    // if(status != SUCCESS)
    // {
    //     // Return status value
    //     return(status);
    // }


    //    status = BLEAppUtil_advStart(peripheralAdvHandle_1, &advSetStartParamsSet_1);
    //    if(status != SUCCESS)
    //    {
    //        // Return status value
    //        return(status);
    //    }

2. Add the HCI DTM commands to start DTM. For this example, random values were used.

.. code-block:: c

  //DTM
    //Set the number of packets
    uint16_t txPktCnt = 1400;
    HCI_EXT_SetDtmTxPktCntCmd(txPktCnt);

    //Define the starting TX power
    int8 txPowerDbm = -8;
    uint8 fraction = 0;
    HCI_EXT_SetMaxDtmTxPowerDbmCmd(txPowerDbm, fraction);
    HCI_EXT_SetTxPowerDbmCmd(txPowerDbm, fraction);

    //Start DTM
    uint8 txChan = 11;
    uint8 payloadLen = 15;
    uint8 payloadType = HCI_DIRECT_TEST_PAYLOAD_0x0F;
    uint8 txPhy = HCI_PHY_1_MBPS;
    HCI_LE_EnhancedTxTestCmd(txChan,payloadLen, payloadType, txPhy);

3. Add a simple delay then end the test.

.. code-block:: c

  //Easy example of delay then end DTM
  //The delay is necessary to give the device enough time to execute the commands
  int i = 0;
  int j = 0;
  while(i < 300000){
      i++;
      if(i == 299999){
          j++;
          i = 0;
      }
      if (j == 20) {
          HCI_LE_TestEndCmd();
          i=300000;
      }
  }

4. Re-enable BLE advertising. Do not forget to initialize the advertisement set parameters.

.. code-block:: c

  //Initialize the BLE advertisement set again
    status = BLEAppUtil_initAdvSet(&peripheralAdvHandle_1, &advSetInitParamsSet_1);
    if(status != SUCCESS)
    {
        // Return status value
        return(status);
    }

    //Start the BLE advertisement
    status = BLEAppUtil_advStart(peripheralAdvHandle_1, &advSetStartParamsSet_1);
    if(status != SUCCESS)
    {
        // Return status value
        return(status);
    }

Continuous Wave Testing
^^^^^^^^^^^^^^^^^^^^^^^

If desired, add the CW testing code immediately after step 3 of the DTM test setup.

1. Comment out the code which initializes and starts the advertising. 

.. code-block:: c

  //Do not start advertising when entering DTM
    // status = BLEAppUtil_initAdvSet(&peripheralAdvHandle_1, &advSetInitParamsSet_1);
    // if(status != SUCCESS)
    // {
    //     // Return status value
    //     return(status);
    // }


    //    status = BLEAppUtil_advStart(peripheralAdvHandle_1, &advSetStartParamsSet_1);
    //    if(status != SUCCESS)
    //    {
    //        // Return status value
    //        return(status);
    //    }

2. Add the HCI CW commands to start the CW test.

.. code-block:: c

  //CW
  //Setup parameters for CW test
    int cwMode = 0;
    txChan = 15;

    //Easy example of short delay before starting the CW test
    //The delay is only needed if you have done the DTM test before
    //The delay gives the device enough time to execute the HCI_LE_TEST_CMD
    i = 0;
    j = 0;
    while(i < 50000){
        i++;
        if(i == 49999){
            j++;
            i = 0;
        }
        if (j == 20) {
            HCI_EXT_ModemTestTxCmd(cwMode, txChan);
            i=5000000;
        }
    }

3. Add delay before ending the CW test. The command executed to end the test is different from DTM.

.. code-block:: c

  //Easy example of short delay before ending the CW test
  //The delay is necessary to give the device enough time to execute the test
    i = 0;
    j = 0;
    while(i < 5000000){
        i++;
        if(i == 4999999){
            j++;
            i = 0;
        }
        if (j == 20) {
            HCI_EXT_EndModemTestCmd();
            i=5000000;
        }
    }

4. Re-enable BLE advertising.

.. code-block:: c

  //Correct the desired power level for the advertisement events
    txPowerDbm = 0;
    fraction = 0;
    HCI_EXT_SetMaxDtmTxPowerDbmCmd(txPowerDbm, fraction);
    HCI_EXT_SetTxPowerDbmCmd(txPowerDbm, fraction);

    //Initialize the BLE advertisement set again
    status = BLEAppUtil_initAdvSet(&peripheralAdvHandle_1, &advSetInitParamsSet_1);
    if(status != SUCCESS)
    {
        // Return status value
        return(status);
    }

    //Start the BLE advertisement
    status = BLEAppUtil_advStart(peripheralAdvHandle_1, &advSetStartParamsSet_1);
    if(status != SUCCESS)
    {
        // Return status value
        return(status);
    }