.. _sec-using-production-test-mode:

==========================================
Production and Direct Test Mode (PTM, DTM)
==========================================


This page will describe Production Test Mode (PTM) which allows a
|DEVICE| BLE application in a "single-chip" configuration to
temporarily expose the host control interface (HCI) test commands over the
serial interface when triggered externally to do so (e.g. holding a GPIO pin
low during power up). This test mode allows the device to be connected to a
Bluetooth RF Tester in order to run Direct Test Mode (DTM) commands on a
production line using the final release firmware, while leaving the UART GPIO
pins available for the application to use at all other times. Note that this
page only considers UART, and not SPI, as the transport protocol since it uses
the least amount of GPIO's and throughput is not a factor for DTM.


.. note::

  Note: DTM defines two interface methods for controlling the LE PHY: HCI and
  2-wire UART. The TI Bluetooth Low Energy protocol stack only supports the HCI
  method for DTM and PTM.


Direct Test Mode (DTM)
^^^^^^^^^^^^^^^^^^^^^^

DTM is a standard method for testing BLE devices using the DTM HCI commands. A
number of wireless test equipment manufactures, including Anritsu (MT8852B),
Keysight and Rhode and Schwarz, make BLE Testers that use this mode. It is very
useful to use these testers during development or on the production line in
order to verify the RF performance of a BLE system. Complementary to these
testers, it is also possible to create your own PC application that sends
these DTM commands over the serial link. DTM is very well described in the
|CORESPEC| Volume 6 Part F. All DTM commands as well as
TI Vendor Specific modem test commands are accessible in embedded
(single-device) application via API calls as well as over HCI in the
Host_Test sample application. Refer to the `TI Vendor Specific HCI Guide`_ in
the documents folder of the |SDK|.

Production Test Mode (PTM)
^^^^^^^^^^^^^^^^^^^^^^^^^^

One problem with DTM is that it relies on a certain stack configuration
(network processor with HCI exposed over UART) in order to work with the
testers, though many end-applications don't use this configuration.
This would require the customer, during production, to flash the wireless
MCU with a network processor image (e.g., ``host_test``) before testing, and
then re-flash with the final product image. To circumvent this, the TI
BLE-Stack has implemented a feature called Production Test Mode (PTM), which
allows for an embedded software application to support direct test mode without
exposing the HCI to the UART pins under normal operation.
Note that the pins used for PTM can also be used for an application UART
interface. In this case, it is necessary to ensure that the other device that
is connected to the UART interface does not run at the same time that DTM is
being exercised. If the device powers up and goes into PTM mode (by a GPIO
being held high or low or some other stimulus), the UART will then be used for
DTM commands. If the device powers up normally and does not go into PTM mode,
then the UART can be initialized by the application and used to communicate
with the other device.
DTM commands can also be called by the embedded BLE application.

.. ifconfig:: device == 'cc23xx'

  To add PTM to the ``ble_basic`` project follow the steps below:

  #. Open the SysConfig file (double-click on the ble_basic.syscfg 
     file)

  #. Open the BLE tab and enter Advanced Settings

  #. Check the PTM box

  This is the only configuration required to enable PTM as checking the PTM box
  automatically increases the Max Number of ICall Enabled tasks to 4.
  If you want to enable the NPI packet flow control, this can be done in the
  NPI panel. The default settings when enabling PTM is shown in the figure 
  below. 

   .. figure:: resources/ptm_sysconfig_setup.png
       :align: center

       Default settings when enabling PTM. 

.. ifconfig:: device == 'cc2640'

  Those wishing to use PTM in their application, should reference the ``_PTM_``
  configuration of the ``simple_peripheral`` project. Diffing this build
  configuration to the default build configuration should show the steps needed
  to enable PTM mode.

.. ifconfig:: device == 'cc13xx_cc26xx'

  To add PTM to the ``simple_peripheral`` project follow the steps below:

  #. Open the SysConfig file (double-click on the simple_peripheral.sysconfig 
     file)

  #. Open the BLE tab and enter Advanced Settings

  #. Check the PTM box

  This is the only configuration required to enable PTM as checking the PTM box
  automatically increases the Max Number of ICall Enabled tasks to 4.
  If you want to enable the NPI packet flow control, this can be done in the
  NPI panel. The default settings when enabling PTM is shown in the figure 
  below. 

   .. _fig_ptm_sysconfig_setup.png:
   .. figure:: resources/ptm_sysconfig_setup.png
       :align: center

       Default settings when enabling PTM. 

.. tip::

  When adding PTM mode to the application, it is recommended to change the
  NPI task to use ``Task_create(...)`` as opposed to construct. In this way,
  the RAM needed by the NPI runtime task stack is consuming RAM that is
  not used in the application's default behavior.

In order to determine if a command is accessible via PTM mode, users should
refer to the translation tables created in ``icall_hci_tl.c`` under the define
``PTM_MODE``.

.. ifconfig:: device == 'cc2640'

  Note: Out of box PTM builds does not support enabling gapbondmgr due to the
  limited flash space.