.. _sec-hci:

Host Controller Interface (HCI)
-------------------------------

The host controller interface (HCI) layer is a thin layer which
transports commands and events between the host and controller
elements of the Bluetooth protocol stack. In a pure network
processor application (that is, the host\_test project), the HCI
layer is implemented through a transport protocol such as SPI or
UART.

In embedded wireless MCU projects such as basic\_ble\_ptm project, the
HCI layer is implemented through function calls and callbacks within the
wireless MCU. All of the commands and events discussed that communicate with
the controller, such as ATT, GAP, etc, will eventually call an HCI API to
pass from the upper layers of the protocol stack through the HCI layer to
the controller. Likewise, the controller sends received data and
events to the host and upper layers through HCI.

As well as standard Bluetooth LE HCI commands, a number of HCI
extension vendor-specific commands are available which extend some
of the functionality of the controller for use by the application.
See :ref:`ble_api_reference` for a description of available HCI
and HCI extension commands callable in the embedded application.

The |STACK| supports a network processor configuration
(host\_test) that allows an application to running on an external
MCU to interface to the |STACK|. The network processor can
accept all LE HCI commands over a external transport protocol (UART, SPI, etc);
however, because the Bluetooth LE host and controller both reside on the
wireless MCU, some HCI commands will
have their corresponding events consumed by the TI BLE host. Thus,
it is not possible to interface an external, off-chip Bluetooth host
to the |DEVICE| wireless MCU using standard HCI LE commands. Network
processor configurations should use both HCI and TI vendor-specific
HCI commands to implement an external Bluetooth application.

Similar to a network processor configuration (host\_test), the |STACK|
can be configured to be pass a subset HCI commands from a transport
protocol (UART, SPI, etc) to the controller with the ability to switch
to an intact embedded application. This configuration is known as Production
Test Mode (PTM). The subset of HCI commands available are those to
perform Bluetooth RF certification. For information on how to
enable PTM on your embedded application
see :ref:`sec-using-production-test-mode`.

PTM should be considered for use for Direct Test Mode (DTM)
in place of a full network processor configuration (host\_test)
when the following is required:

    * Device is only Flashed Once during the production line

        If product flashing is only done once or production firmware
        is flashed prior to testing Bluetooth RF Functionality, and firmware
        images can no longer be changed.

    * Flash Availability for HCI Transport Layer

        PTM requires flash along side the application, thus reducing
        application flash.

.. note::

    Direct Test Mode (DTM) is also supported by the |STACK|.
    DTM is described in detail in the Direct Test Mode section ([Vol 6], Part F)
    of the |CORESPEC|. Host\_test supports all DTM
    commands as well as Vendor Specific modem test commands.

    See `Configuring Bluetooth LE devices for Direct Test Mode (SWRA720) <https://www.ti.com/lit/swra720>`_
    for information on how to set up host\_test application binary
    designed to work with a custom product and chip package types.

Using HCI and HCI Vendor-Specific Commands in the Application
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

The following examples will be modifying ``app_peripheral.c`` in the 
``basic_ble``. However, these modifications will work in any of the 
framework's projects.

Follow these steps to use these commands and receive their
respective events in the application:

1. **BLEAppUtil_EventHandler_t** structure is used to create different
   event handlers. You can find all of the different handler types in 
   **bleapputil_api.h :: BLEAppUtil_eventHandlerType_e**.  

    .. code-block:: c
     :linenos:

     BLEAppUtil_EventHandler_t peripheralHCIHandler =
     {
         .handlerType = BLEAPPUTIL_HCI_GAP_TYPE, // Handler type.
         .pEventHandler = Peripheral_HCIEventHandler, // Function to handle events.
         .eventMask = BLEAPPUTIL_HCI_COMMAND_COMPLETE_EVENT_CODE // HCI events to subscribe to.
                      | BLEAPPUTIL_HCI_VE_EVENT_CODE,
     };

2. Create a handler function. The handler code below is the general structure
   of a handler in the BLEAppUtil framework.

    .. code-block:: c
     :linenos:

     void Peripheral_HCIEventHandler( uint32_t event, BLEAppUtil_msgHdr_t *pMsgData)
     {
         switch (event)
         {
             case BLEAPPUTIL_HCI_COMMAND_COMPLETE_EVENT_CODE:
             {
                 Display_printf(dispHandle, dispIndex, 0,
                                "#%5d    HCI_COMMAND_COMPLETE_CODE",
                                dispIndex); dispIndex++;
                 break; 
             }

             case BLEAPPUTIL_HCI_VE_EVENT_CODE:
             {
                 Display_printf(dispHandle, dispIndex, 0,
                                "#%5d    HCI_VE_EVENT_CODE",
                                dispIndex); dispIndex++;
                 break; 
             }
             default: break;
         }
     }

3. Register the new event handler with **BLEAppUtil_registerEventHandler()**.
   This can be done in the **Peripheral_start()** function. 

  .. code-block:: c
    :linenos:

    // Note that the structure is used to register the event handler.
    status = BLEAppUtil_registerEventHandler(&peripheralHCIHandler);
    if(status != SUCCESS)
        return(status);

4. Call any standard HCI or HCI vendor-specific command that is able to be 
   called from the application. See the :ble_api:`HCI_Function_Maps` for a 
   table of which commands can be sent.

The following sections consider receiving standard HCI events and HCI
vendor-specific events.

Standard LE HCI Commands and Events
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

These commands are documented in the HCI Commands and Events chapter
(Volume 4, Part E, Section 7) of the |CORESPEC|. The mechanism to use these
commands is the same for any command in this section of the |CORESPEC|,
including HCI LE commands. 

.. note:: 
   The example below demonstrates how to use the |CORESPEC| to implement an HCI
   command in the application. The command considered is Read RSSI Command.
   This command is not yet supported on |DEVICE| devices.

Sending an HCI Command
""""""""""""""""""""""

1. Find the command in the |CORESPEC|:

.. figure:: resources/hci_ble_core_rssi_snippet.jpg
    :align: center
    :width: 75%

    RSSI Command from the |CORESPEC|.

2. Find mapping to BLE stack command. Using the :ref:`ble_api_reference` (HCI
   section --> HCI Function Maps), shows that this command maps to :ble_api:`HCI_ReadRssiCmd`.

3. Using the API from Step 1, fill in the parameters and call the
   command from somewhere in the application. This specific command
   should be called after a connection is formed. There is only
   command parameter here: a 2-byte connection handle. 

  .. code-block:: c
    :linenos:

    HCI_ReadRssiCmd( connHandle );

Receiving HCI Events
""""""""""""""""""""

1. Look at the |CORESPEC| to see the format of the returned event:

    .. figure:: resources/hci_ble_core_rssi_rtnparams.jpg
        :align: center
        :width: 75%

        RSSI Return information with Event from the |CORESPEC|.

2. This command returns a Command Complete event (:ble_api:`hciEvt_CmdComplete_t`) as stated
   in the "Corresponding Events" section of the doxygen API (:ble_api:`HCI_ReadRssiCmd`).

  .. code-block:: c
     :linenos:

     void Peripheral_HCIEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
     {
         // Process HCI message
         switch(event)
         {
             // Process HCI Command Complete Event case.
             case BLEAPPUTIL_HCI_COMMAND_COMPLETE_EVENT_CODE:
             {
               Display_printf(dispHandle, dispIndex, 0,
                           "#%5d    HCI_COMMAND_COMPLETE_CODE",
                           dispIndex); dispIndex++;

               // Parse Command Complete Event for opcode and status.
               hciEvt_CmdComplete_t* command_complete = (hciEvt_CmdComplete_t*) pMsgData;
               uint8_t status = command_complete->pReturnParam[0];

               // Find which command this command complete is for
               switch (command_complete->cmdOpcode)
               {
                  case HCI_READ_RSSI:
                  {
                     if (status == SUCCESS)
                     {
                        uint16_t handle = BUILD_UINT16( command_complete->pReturnParam[1], command_complete->pReturnParam[2] );

                        // Check handle.
                        if (handle == 0x00)
                        {
                           uint8_t rssi = command_complete->pReturnParam[3];
                           Display_printf(dispHandle, dispIndex, 0,
                                           "#%5d    HCI_READ_RSSI: %d",
                                           dispIndex, rssi); dispIndex++;

First, the stack message is checked to see what type
of HCI event it is. In this case, it is an
:ble_api:`HCI_COMMAND_COMPLETE_EVENT_CODE`. Then the event returned
from the stack as a message (pMsgData) is cast to an 
:ble_api:`hciEvt_CmdComplete_t`, which is defined as:

  .. code-block:: c
     :linenos:

     // Command Complete Event typedef struct.
     {
         osal_event_hdr_t hdr;
         uint8 numHciCmdPkt;
         uint16 cmdOpcode;
         uint8* pReturnParam;
     } hciEvt_CmdComplete_t;

Next, the cmdOpcode is checked and it is found that it matches
:ble_api:`HCI_READ_RSSI`. Then the status of the event is checked.
Now that the event is known, the pReturnParmam can be parsed using the 
information from the |CORESPEC|. The |CORESPEC| API from above states 
that the first byte of the return parameters is the Status.

The |CORESPEC| API states that the second and third bytes of the return
parameters are the Handle.  The RSSI is then checked to
see if it corresponds to the desired connection handle.

Continuing parsing using the |CORESPEC| API, the RSSI value can be found by reading the fourth byte
of the return paramters. Finally, the RSSI value is stored.

HCI Vendor-Specific Commands
^^^^^^^^^^^^^^^^^^^^^^^^^^^^

These commands are documented in the `TI Vendor Specific HCI Guide`_. The
mechanism to use these commands is the same for all vendor-specific commands.
The example below demonstrates how to use the `TI Vendor Specific HCI Guide`_
to implement an HCI command in the application. The command considered is
HCI Extension Packet Error Rate.

Sending HCI Vendor-Specific Command
"""""""""""""""""""""""""""""""""""

1. Find the :ble_api:`HCI_EXT_PacketErrorRateCmd` in the `TI Vendor Specific HCI Guide`_.

2. Use the HCI section in :ref:`ble_api_reference` to find the BLE Stack
   function that implements this command : :ble_api:`HCI_EXT_PacketErrorRateCmd`.

3. Using the API from Step 1, fill in the parameters and call the
   command from the application.  In this specific case, this command should be
   called after a connection has been formed. The first parameter is
   a 2-byte connHandle, which is 0x0000 for this example. The second
   parameter is a 1-byte command ( :ble_api:`HCI_EXT_PER_READ` ) to read the
   counters. Therefore, use:

  .. code-block:: c
    :linenos:

    HCI_EXT_PacketErrorRateCmd( 0, HCI_EXT_PER_READ );

Receiving HCI Vendor-Specific Events
""""""""""""""""""""""""""""""""""""

1. Find the corresponding :ble_api:`HCI_EXT_PER` event in the `TI Vendor Specific HCI Guide`_.

2. As stated in the "Corresponding Events" section of the command API, this
   command returns a Vendor Specific Command Complete Event ( :ble_api:`hciEvt_VSCmdComplete_t` )
   This is further detailed below.

  .. code-block:: c
     :linenos:

     void Peripheral_HCIEventHandler( uint32_t event, BLEAppUtil_msgHdr_t *pMsgData )
     {
         // Process HCI message.
         switch (event)
         {
             // Process HCI Vendor Specific Command Complete Event.
             case BLEAPPUTIL_HCI_VE_EVENT_CODE:
             {
                 Display_printf(dispHandle, dispIndex, 0,
                                "%5d    HCI_VE_EVENT_CODE",
                                dispIndex); dispIndex++;

                 // Parse Command Complete Event for opcode and status.
                 hciEvt_VSCmdComplete_t *command_complete = (hciEvt_VSCmdComplete_t *)pMsgData;

                 // Find which command this command complete is for.
                 case HCI_EXT_PER:
                 {
                     uint8_t status = command_complete->pEventParam[2];
                     if (status == SUCCESS)
                     {
                         Display_printf(dispHandle, dispIndex, 0,
                                       "%5d    HCI_EXT_PER",
                                       dispIndex); dispIndex++;
                         uint8_t cmdVal = command_complete->pEventParam[3];
                         if (cmdVal == 1)
                         {
                             uint16_t numPkts = BUILD_UINT16(command_complete->pEventParam[4], command_complete->pEventParam[5]);
                             uint16_t numCrcErr = BUILD_UINT16(command_complete->pEventParam[6], command_complete->pEventParam[7]);
                             uint16_t numEvents = BUILD_UINT16(command_complete->pEventParam[8], command_complete->pEventParam[9]);
                             uint16_t numMissedEvents = BUILD_UINT16(command_complete->pEventParam[10], command_complete->pEventParam[11]);

First, the status of the stack message is checked to see what type
of HCI event it is. In this case, it is an :ble_api:`HCI_VE_EVENT_CODE`.

Next, the event returned from the stack as a message (pMsg) is cast
to an :ble_api:`hciEvt_VSCmdComplete_t`, which is defined as:

.. code-block:: c
 :linenos:

 typedef struct
 {
    osal_event_hdr_t hdr; uint8 length;
    uint16 cmdOpcode; uint8* pEventParam;
 } hciEvt_VSCmdComplete_t;

The opcode is checked by reading command\_complete->cmdOpcode, and
found that it matches :ble_api:`HCI_EXT_PER`.

Next, the \*pEventParam is parsed to extract the parameters defined
in the event API. The first two bytes (shown in red in :numref:`per_memory_map`)
are the event opcode (0x1404). The third byte is the Status. This is
the case for all vendor-specific events.

From the fourth byte of pEventParam on, the event API from the TI
BLE Vendor-Specific Guide is used for parsing, starting at the third
parameter. This is the case for all vendor-specific events. For this
example, the fourth byte of pEventParam corresponds to the cmdVal
parameter. This is shown in memory and explained further below.

.. _per_memory_map:

.. figure:: resources/hci_vendor_per_memory.jpg
     :align: center
     :width: 75%

     RSSI Commend from the |CORESPEC|.

The status is checked by reading the third byte of the event
parameters (command\_complete->pEventParam[2]). This is shown in
yellow in :numref:`per_memory_map`.

Starting from the fourth byte of the event parameters
(command\_complete->pEventParam[3]), the event API states that the
next parameter is a one-byte cmdVal. This is checked to verify that
this event corresponds to a read of the PER counters. This is shown
in pink.

Continuing parsing using the event API, the next parameter is a
two-byte numPkts. This is found by building a uint16\_t out of the
fifth and sixth bytes of the event parameters. This is shown in
blue. In a similar fashion, numCrcErr is found from the seventh and
eight bytes of the event parameters (shown in green).

Next, numEvents is found from the ninth and tenth bytes of the event
parameters (shown in orange). Finally, numMissedEvents is found from
the eleventh and twelfth bytes of the event parameters (shown in
purple).


Disabling Controller Features using HCI 
"""""""""""""""""""""""""""""""""""""""
Disabling the CSA #2 feature will be used as an example to disable controller 
features. The process below will work for disabling all controller features 
listed in ``ll_common.h``. The code snippet below contains all of the various
controller features that may be disabled.

  .. code-block:: c
     :linenos:

     // Byte 0
     #define LL_FEATURE_ENCRYPTION                          0x01
     #define LL_FEATURE_CONN_PARAMS_REQ                     0x02
     #define LL_FEATURE_REJECT_EXT_IND                      0x04
     #define LL_FEATURE_SLV_FEATURES_EXCHANGE               0x08
     #define LL_FEATURE_PING                                0x10
     #define LL_FEATURE_DATA_PACKET_LENGTH_EXTENSION        0x20
     #define LL_FEATURE_PRIVACY                             0x40
     #define LL_FEATURE_EXTENDED_SCANNER_FILTER_POLICIES    0x80

     // Byte 1
     #define LL_FEATURE_2M_PHY                              0x01
     #define LL_FEATURE_STABLE_MODULATION_INDEX_TX          0x02
     #define LL_FEATURE_STABLE_MODULATION_INDEX_RX          0x04
     #define LL_FEATURE_CODED_PHY                           0x08
     #define LL_FEATURE_EXTENDED_ADVERTISING                0x10
     #define LL_FEATURE_PERIODIC_ADVERTISING                0x20
     #define LL_FEATURE_CHAN_ALGO_2                         0x40
     #define LL_FEATURE_LE_POWER_CLASS_1                    0x80

     // Byte 2
     #define LL_FEATURE_MINIMUM_NUMBER_OF_USED_CHANNELS     0x01
     #define LL_FEATURE_CONNECTION_CTE_REQUEST              0x02  // support CTE request procedure as initiator
     #define LL_FEATURE_CONNECTION_CTE_RESPONSE             0x04  // support CTE request procedure as responder
     #define LL_FEATURE_CONNECTIONLESS_CTE_TRANSMITTER      0x08
     #define LL_FEATURE_CONNECTIONLESS_CTE_RECEIVER         0x10
     #define LL_FEATURE_ANTENNA_SWITCHING_DURING_CTE_TX     0x20  // support LL_FEATURE_RECEIVING_CTE and switching antennas for AoD
     #define LL_FEATURE_ANTENNA_SWITCHING_DURING_CTE_RX     0x40  // support LL_FEATURE_RECEIVING_CTE and switching antennas for AoA
     #define LL_FEATURE_RECEIVING_CTE                       0x80  // support receiving CTE in data PDUs and IQ sampling

     // Byte 3
     #define LL_FEATURE_PERIODIC_ADV_SYNC_TRANSFER_SEND     0x01
     #define LL_FEATURE_PERIODIC_ADV_SYNC_TRANSFER_RECV     0x02
     #define LL_FEATURE_SLEEP_CLOCK_ACCURACY_UPDATES        0x04
     #define LL_FEATURE_REMOTE_PUBLIC_KEY_VALIDATION        0x08


To disable controller features, first call the 
:ble_api:`HCI_ReadLocalSupportedFeaturesCmd` to grab the current feature list.
The pReturnParmam can be parsed using the information from the |CORESPEC|. 
The |CORESPEC| API from above states that bytes 1-9 of the return 
parameters is the feature set. Once the feature set is received, modify the bit 
at the correct byte and call :ble_api:`HCI_SetLocalSupportedFeaturesCmd` to set 
the new feature set. Typically, this is done after the stack has been 
initialized, and there are no stack operations (advertising, scanning, etc.) 
running.

  .. code-block:: c
     :linenos:

     void Peripheral_HCIEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
     {
         // Process HCI message
         switch(event)
         {
             // Process HCI Command Complete Event case.
             case BLEAPPUTIL_HCI_COMMAND_COMPLETE_EVENT_CODE:
             {

               // Parse Command Complete Event for opcode and status.
               hciEvt_CmdComplete_t* command_complete = (hciEvt_CmdComplete_t*) pMsgData;
               uint8_t status = command_complete->pReturnParam[0];

               // Find which command this command complete is for
               switch (command_complete->cmdOpcode)
               {
                  case HCI_READ_LOCAL_SUPPORTED_FEATURES:
                  {
                     if (status == SUCCESS)
                     {
                              uint8_t featSet[8];
                              // Get current feature set from received event (bytes 1-9
                              // of the returned data
                              memcpy( featSet, &pMsg->pReturnParam[1], 8 );
                              
                              // Clear bit 7 of byte 1 of feature set to disable LL
                              // the Channel Selection Algorithm 2 feature
                              CLR_FEATURE_FLAG( featSet[1], LL_FEATURE_CHANN_ALGO_2 );
                              
                              // Update controller with modified features
                              HCI_EXT_SetLocalSupportedFeaturesCmd( featSet );