.. _cc2340r5-cc2340r21-migration-guide:

CC2340R5 to CC2340R21 Porting Guide
***********************************

This section will describe, in general terms, how to migrate
a project developed for the |DEVICE_LOW_PLUS| device to a
|DEVICE_LOW| device running the |SDK|. However, it is important to first
assess the differences between both devices to make sure that the
project migration is possible (See `Platform Devices Comparison <../../ble-stack-5.x/overview-cc23xx.html>`_).

Evaluate the |DEVICE_LOW| device when only having |DEVICE_LOW_PLUS| devices
===========================================================================

To evaluate the |DEVICE_LOW| when only having a |DEVICE_LOW_PLUS|, you can modify
the Flash and RAM size as described below.

 * Open the Linker command file ``.cmd`` and modify the Flash size
   to |FLASH_SIZE_LOW|.

    .. code-block:: c
        :caption: lpf3_app_freertos.cmd - Replace ``FLASH_SIZE`` and ``RAM_SIZE``values.
        :linenos:

        #define FLASH_SIZE   0x40000
        #define RAM_SIZE     0x7000

.. note::
    The two devices are API compatible, a project for |DEVICE_LOW| developed on
    |DEVICE_LOW_PLUS| can be migrated (via the migration guide below) 
    with very few modifications to be built and flashed on |DEVICE_LOW|.

Migration Guide
===============

The recommended migration path is to start with a |DEVICE_LOW_PLUS| 
based example project from the |SDK| and follow the next steps:

1. Import the project into Code Composer Studio or you IDE of preference.

2. Open SysConfig, go to ``Device View`` and click on ``SWITCH``.

.. _deviceview_switch_configurationR21_1:
.. figure:: resources/DeviceView_Switch.png
    :align: center

    SysConfig - Switch Device.

3. Once the ``Switch Board or Device`` window is opened, select the
   |DEVICE_LOW| board, or |DEVICE_LOW| device and click on ``CONFIRM``.
   Make sure to save the project changes so that the migration takes place.

.. _deviceview_switch_configurationR21_2:
.. figure:: resources/Select_R2device.png
    :align: center

    SysConfig - Select |DEVICE_LOW| device.

.. warning:: If a new linker command file is generated after migration (named ``cc23x0r2.cmd`` in the project files)
             please make sure to exclude it from build (or eliminated it from the project files) so that the original
             ``lpf3_app_freertos.cmd`` file is used during build time.

4. Open SysConfig and reduce the heap size, under FreeRTOS |rarr| ``Stack and Heap Sizing``.
   For an out-of-the-box implementation of the examples, consider the following heap sizes as a starting point:

        - basic_ble / basic_ble_profiles: 0x00003F50
        - host_test / data_stream: 0x00003000
        - Off-Chip OAD: 0x0003400

.. _deviceview_switch_configurationR21_4:
.. figure:: resources/change_heap_size.png
    :align: center

    SysConfig - Modify Heap Size.

.. warning::
    Depending on the RAM size consumed by your application, this new value may 
    require a modification.

5. Open SysConfig and reduce the internal NVS size, under NVS |rarr| ``Internal Flash``.
   For an out-of-the-box implementation of the examples, consider using 0x3C000 as the
   region base value.

.. _deviceview_switch_configurationR21_5:
.. figure:: resources/change_NVS_basic_ble.png
    :align: center

    SysConfig - Modify NVS base region.

6. For project examples that require reallocation of pins due to differences 
   in package size between |DEVICE_LOW_PLUS| and |DEVICE_LOW| devices. Open 
   SysConfig and modify the GPIO information with the available pins you have 
   depending on your application. You can see below how this is done for the 
   case of the host_test project example.

.. _deviceview_switch_configurationR21_6:
.. figure:: resources/host_test_GPIOchange.png
    :align: center

    SysConfig - Modify GPIOs.

7. Build the project.

Additional Steps for Off-Chip OAD and MCUBoot examples
======================================================

.. note::
   The |DEVICE_LOW| device does not support On-Chip and Dual Image OAD due
   to reduced Flash size.

1. Inside the Off-Chip OAD project, open SysConfig and update NVS External 
   Configuration as seen below:

.. _deviceview_switch_configurationR21_7:
.. figure:: resources/offchip_externalNVS_config1.png
    :align: center

    SysConfig - Modify size of NVS External Flash to match the size of the External Flash available on the board.

.. _deviceview_switch_configurationR21_8:
.. figure:: resources/offchip_externalNVS_config2.png
    :align: center

    SysConfig - Modify SPI pins.

2. Right click on the project file and select Properties.
   Modify the post build steps so that the slot sizes match the ones of the
   |DEVICE_LOW| device.

.. _deviceview_switch_configurationR21_9:
.. figure:: resources/modify_post_build_offchip.png
    :align: center

    Project Properties - Modify post build steps.

3. For the MCUBoot project, additionaly to the device migration, modify the MCUBoot configuration inside SysConfig.

    - Enable Overwrite-only code path.
    - Enable External Flash configuration.
    - Modify the Base Address and Image Size depending on your application.

.. _deviceview_switch_configurationR21_10:
.. figure:: resources/flash_backend_size.png
    :align: center

    SysConfig - MCUBoot.
    
4. Build both projects.