.. The below versions should only be modified after verification that the steps
   in the guide hold true.

.. |CHAMELEON_VER| replace:: CC2640R2 SDK 5.30
.. |AGAMA_VER| replace:: CC13xx/CC26xx SDK 6.10

.. _blestack_to_ble5stack:

Porting BLE-Stack to BLE5-Stack
*******************************

This section will describe how to port from a BLEStack project to a BLE5Stack
project.

.. note::
    This example is specifically for |CHAMELEON_VER| to |AGAMA_VER| but the
    steps are similar for all cases. Individual differences can be found in the
    relevant migration and/or porting guides.



This guide will describe a way to port a project from |CHAMELEON_VER| to a
|AGAMA_VER| project. If your project uses the BLE-Stack, please note that this
guide won't show how to add BLE5 features. However porting your project will
allow the use of BLE5 features that are contained in |AGAMA_VER|.

See the following tables for API replacements:

* :ref:`sec-porting-translation-tables`

    * :ref:`tbl_ble5_porting_gaprole_changes_cc2640r2_to_cc26x2`

    * :ref:`tbl_ble5_porting_gapbondmgr_changes_cc2640r2_to_cc26x2`

    * :ref:`tbl_ble5_porting_gapgattserver_changes_cc2640r2_to_cc26x2`

    * :ref:`tbl_ble5_porting_linkdb_changes_cc2640r2_to_cc26x2`

    * :ref:`tbl_ble5_porting_sample_app_changes`

Porting Steps
=============

To minimize project configuration differences, start with an example project in
the |AGAMA_VER|. For example, if your base project was ``simple_peripheral`` in
the |CHAMELEON_VER|, use ``simple_peripheral`` in the |AGAMA_VER| as the project
base to implement application-level modifications on. In other words, no
modifications will be made to the original project. All application specific
code should be inserted into the |AGAMA_VER| project.

Some of these application-level modifications are due to various API changes.
To aid in this, the guide provides an API translation table:
:ref:`tbl_ble5_porting_gaprole_changes_cc2640r2_to_cc26x2`.

Be sure to utilize the IDE and Tools recommended by the SDK's release notes.
For API Descriptions see :ref:`ble_api_reference`.

#. **Choose a** |AGAMA_VER| **example Bluetooth LE project and open it in the
   preferred supported IDE**

   We're going to use ``simple_peripheral`` as the starting |AGAMA_VER|
   sample project to provide context.

#. **Modify the SysConfig file in the project folder. Use the SysConfig tool to
   transfer your project settings from the original project.**
   
   This includes:

   - Any modification to the example project's original predefined symbols
   - Any stack modification done through predefined symbols
   - Desired Radio settings
   - TI Drivers initializations/settings
   - Board file configuration

   For more information, see :ref:`sysconfig-sysconfig` and
   :ref:`sysconfig-ble5`.

#. **Transfer any additional app specific predefined symbols into the example
   project**

#. **Transfer modified application files into the example project**

   Modify ``main.c`` in the |AGAMA_VER| example to create or rename any
   tasks that were added or modified in the original project.

   In this example, the following files from the original project were moved
   into the target ``simple_peripheral`` example:

   - ``two_btn_menu.c`` and ``two_btn_menu.h``
   - ``simple_peripheral.c`` and ``simple_peripheral.h``
   - ``simple_peripheral_menu.c`` and ``simple_peripheral_menu.h``
   - ``simple_gatt_profile.c`` and ``simple_gatt_profile.h``

#. **Adjust the Application for the GAP Role Removal**

    .. note::
       ``GAPRole_createTask()`` should **not** be brought over to ``main.c``.
       See :ref:`gap-role-removal` for more information.

    All GAP Roles source and header files (``peripheral.c``, ``peripheral.h``,
    ``central.c``, ``central.h``, etc.) have been removed in |AGAMA_VER|.
    These files will produce build errors and should not be included in your app.
    This change will introduce a structure change in the application.

    The functionality of the roles have been broken into distinct GAP functions:
    Scanner, Advertiser, and Initiator.

    These functions of GAP can be independently controlled to allow the device
    to function as a desired GAP Role such as peripheral or central. For
    additional information about using these roles, it is suggested to refer to
    the :ref:`gap_roles` section of the User Guide. If you formerly used the
    BLE-Stack, this section provides information about the legacy features that
    exist in your current application.

    Utilize the :ref:`tbl_ble5_porting_gaprole_changes_cc2640r2_to_cc26x2` table
    to port application GAP functionality. For example, in this table you'll
    find information such as ``TGAP_LIM_DISC_ADV_INT_MIN`` is now replaced with
    ``GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN``, ``GAPROLE_ADVERT_ENABLED`` is
    now done with ``GapAdv_enable()`` or that ``GAPRole_StartDevice()`` is
    replaced by ``GAP_DeviceInit()`` to start the GAP module.

    It is suggested to look at an existing example in the SDK.
    ``simple_peripheral`` or ``simple_central`` may need to be used to assist in
    the porting process of the application. For example, the initialization of
    GAP Advertiser can be found in ``simple_peripheral``.

    After using the :ref:`tbl_ble5_porting_gaprole_changes_cc2640r2_to_cc26x2`
    table and using a relevant |AGAMA_VER| example project as a guide, such as
    ``simple_peripheral``, the structure and changes will become clearer.

    In the context of ``simple_peripheral`` and using the rest of the guide,
    the following table provides an example of changes to understand and
    implement when porting:
    :ref:`tbl_ble5_porting_sample_app_changes`.

#. **Adjust the Application for the GAP Bond Manager Changes**

    See :ref:`tbl_ble5_porting_gapbondmgr_changes_cc2640r2_to_cc26x2` for
    additional changes.

    * Include ``icall_ble_api.h`` if Stack/ICall APIs are used. Add the
      following #include **AFTER** all other includes for source files using
      Stack/ICall APIs.

       In this example, add::

       #include "icall_ble_api.h"

       into the following files **AFTER** all other includes. In for the
       ``simple_peripheral`` port, add this into these files:

       * ``simple_peripheral.c``
       * ``simple_gatt_profile.c``

       For more information regarding ``icall_ble_api.h`` see
       :ref:`sec-the-application-icall-lite`.

       .. warning::
          All Stack/ICall APIs are listed in ``icall_ble_api.h``. If any APIs
          are used without ``icall_ble_api.h``, build and or link errors may
          occur with erratic runtime behaviors!

#. **Replace GAP Event processing**

    In addition to the GAP Role changes, GAP events are being handled
    differently. This used to be received by GAP Role
    (ie. **SimpleBLEPeripheral_processStateChangeEvt**), which would then call
    GAPBondMgr, and then translate the event to GAPRole specific events and
    pass it to the application through a callback
    (ie. **SimpleBLEPeripheral_gapRoleCBs**).

    GAP events are now returned to the application directly as RTOS events.
    If the GAPBondMgr is present, they will first be received by the GAPBondMgr
    to do some processing but it will still be received the same in the
    application. This is now configured with ``GAP_DeviceInit``. GAP
    events are received by the application (when the bond manager exists) as
    stack messages of type ``GAP_MSG_EVENT``.

    See the example for ``simple_peripheral`` from |AGAMA_VER|
    in the snippets below:

    .. code-block:: c
        :caption: Register to receive GAP events

        // Entity ID globally used to check for source and/or destination of messages
        static ICall_EntityID selfEntity;
        //...

        // Event globally used to post local events and pend on system and
        // local events.
        static ICall_SyncHandle syncEvent;
        //...

        // Address mode
        static GAP_Addr_Modes_t addrMode = DEFAULT_ADDRESS_MODE;
        //...

        static void SimplePeripheral_init(void)
        {
         BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- init ", SP_TASK_PRIORITY);
         // Create the menu
         SimplePeripheral_buildMenu();

         // ******************************************************************
         // N0 STACK API CALLS CAN OCCUR BEFORE THIS CALL TO ICall_registerApp
         // ******************************************************************
         // Register the current thread as an ICall dispatcher application
         // so that the application can send and receive messages.
         ICall_registerApp(&selfEntity, &syncEvent);

         //...
         BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- call GAP_DeviceInit", GAP_PROFILE_PERIPHERAL);
         //Initialize GAP layer for Peripheral role and register to receive GAP events
         GAP_DeviceInit(GAP_PROFILE_PERIPHERAL, selfEntity, addrMode, &pRandomAddress);
        }

    .. code-block:: c
        :caption: Receiving GAP Events
        :emphasize-lines: 1, 10-12, 18

        static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg); // function definition to handle GAP messages

        static uint8_t SimplePeripheral_processStackMsg(ICall_Hdr *pMsg)
        {
          // Always dealloc pMsg unless set otherwise
          uint8_t safeToDealloc = TRUE;

          switch (pMsg->event)
          {
            case GAP_MSG_EVENT:
              SimplePeripheral_processGapMessage((gapEventHdr_t*) pMsg);
              break;
            //...
          }
        }

        //...
        static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg)
        {
            switch(pMsg->opcode)
            {
                case GAP_DEVICE_INIT_DONE_EVENT:
                {
                //... etc.

#. **Adjust the Application for the GATT Profile Changes**

    Due to changes in LinkDB defines (``linkdb.h``), custom GATT profiles
    may need to be modified in order to account for the new definitions.


    Prepend ``LINKDB_`` to all constants starting with ``CONNHANDLE_``, for example in ``simple_gatt_profile.c``:

        .. code-block:: c

            // Initialize Client Characteristic Configuration attributes
            GATTServApp_InitCharCfg( LINKDB_CONNHANDLE_INVALID, simpleProfileChar4Config );


    See :ref:`tbl_ble5_porting_gapgattserver_changes_cc2640r2_to_cc26x2` and
    :ref:`tbl_ble5_porting_linkdb_changes_cc2640r2_to_cc26x2` for additional changes as required.

#. Note that additional return parameters have been added to ``HCI_EXT_ConnEventNoticeCmd()``:

    .. code-block:: c

        /**
         * Report describing connection event Returned via a @ref pfnGapConnEvtCB_t.
         */
        typedef struct
        {
          GAP_ConnEvtStat_t     status;   //!< status of connection event
          uint16_t              handle;   //!< connection handle
          uint8_t               channel;  //!< BLE RF channel index (0-39)
          GAP_ConnEvtPhy_t      phy;      //!< PHY of connection event
          int8_t                lastRssi; //!< RSSI of last packet received
          /// Number of packets received for this connection event
          uint16_t              packets;
          /// Total number of CRC errors for the entire connection
          uint16_t              errors;
          /// Type of next BLE task
          GAP_ConnEvtTaskType_t nextTaskType;
          /// Time to next BLE task (in us). 0xFFFFFFFF if there is no next task.
          uint32_t              nextTaskTime;
        } Gap_ConnEventRpt_t;

        /** @} End GAP_Structs */

#. Note that additional parameter (signalIdentifier) has been added to ``GAP_UpdateLinkParamReq``:

    .. code-block:: c

        /**
         * Establish Link Request parameters
         *
         * This is used by @ref GAP_UpdateLinkParamReq
         */
        typedef struct
        {
          uint16_t connectionHandle; //!< Connection handle of the update
          uint16_t intervalMin;      //!< Minimum Connection Interval
          uint16_t intervalMax;      //!< Maximum Connection Interval
          uint16_t connLatency;      //!< Connection Latency
          uint16_t connTimeout;      //!< Connection Timeout
          uint8_t  signalIdentifier; //!< L2CAP Signal Identifier. Must be 0 for LL Update
        } gapUpdateLinkParamReq_t;

#. ``HCI_EXT_ConnEventNoticeCmd()`` has been replaced with :ble_api:`Gap_RegisterConnEventCb`.

.. _sec-porting-translation-tables:

API Translation Tables
======================

These tables describe BLE5Stack API replacements for BLEStack API's.

.. _tbl_ble5_porting_gaprole_changes_cc2640r2_to_cc26x2:
.. table:: GAP Changes

    +---------------------------------------------------------+------------------------------------------------------------------------------------------------------------+
    | Previous Implementation                                 | New/Current implementation                                                                                 |
    +============+============================================+============================================================================================================+
    |    Type    |   Name                                     | Description / API / Parameter                                                                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP EVENT | GAP_ADV_DATA_UPDATE_DONE_EVENT             | Check return status of :ble_api:`GapAdv_loadByHandle` or :ble_api:`GapAdv_loadByBuffer`                    |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP EVENT | GAP_DEVICE_DISCOVERY_EVENT                 | This depends on how the scanner is configured but one or more of the following events will be received:    |
    |            |                                            |                                                                                                            |
    |            |                                            |     :ble_api:`GAP_EVT_SCAN_DISABLED`                                                                       |
    |            |                                            |     :ble_api:`GAP_EVT_SCAN_PRD_ENDED`                                                                      |
    |            |                                            |     :ble_api:`GAP_EVT_SCAN_REQ_RECEIVED`                                                                   |
    |            |                                            |     :ble_api:`GAP_EVT_SCAN_INT_ENDED`                                                                      |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP EVENT | GAP_DEVICE_INFO_EVENT                      | :ble_api:`GAP_EVT_ADV_REPORT` or :ble_api:`GAP_EVT_ADV_REPORT_FULL`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP EVENT | GAP_END_DISCOVERABLE_DONE_EVENT            | Check return status of :ble_api:`GapAdv_disable` to see that advertising is successfully being cancelled.  |
    |            |                                            | The :ble_api:`GAP_EVT_ADV_END_AFTER_DISABLE` will be sent after the last advertisement ends.               |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP EVENT | GAP_MAKE_DISCOVERABLE_DONE_EVENT           | Check return status of :ble_api:`GapAdv_enable` to see that advertising is successfully being started.     |
    |            |                                            | The :ble_api:`GAP_EVT_ADV_START_AFTER_ENABLE` will be sent after the first advertisement starts.           |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP EVENT | GAP_RANDOM_ADDR_CHANGED_EVENT              | Obsolete - Address Resolution is done controller                                                           |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_ADV_MIN                      | Configured by durationOrMaxEvents parameter of :ble_api:`GapAdv_enable`                                    |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_ADV_TIMEOUT                       | Configured by durationOrMaxEvents parameter of :ble_api:`GapAdv_enable`                                    |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_SCAN                         | Configured by parameters of :ble_api:`GapScan_enable`                                                      |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_SCAN                         | Configured by parameters of :ble_api:`GapScan_enable`                                                      |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_SCAN_INT                     | Configured by interval parameter of :ble_api:`GapScan_setPhyParams`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_SCAN_WIND                    | Configured by window parameter of :ble_api:`GapScan_setPhyParams`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_SCAN_INT                     | Configured by interval parameter of :ble_api:`GapScan_setPhyParams`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_SCAN_WIND                    | Configured by window parameter of :ble_api:`GapScan_setPhyParams`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_ADV_TIMEOUT                  | Configured by durationOrMaxEvents parameter of :ble_api:`GapAdv_enable`                                    |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_PARAM_TIMEOUT                    | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_CONN_PARAM_TIMEOUT`                                  |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_ADV_INT_MIN                  | :ble_api:`GapAdv_setParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN`                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_ADV_INT_MAX                  | :ble_api:`GapAdv_setParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX`                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_ADV_INT_MIN                  | :ble_api:`GapAdv_setParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN`                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_ADV_INT_MAX                  | :ble_api:`GapAdv_setParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX`                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_ADV_INT_MIN                      | :ble_api:`GapAdv_setParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN`                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_ADV_INT_MAX                      | :ble_api:`GapAdv_setParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX`                              |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_SCAN_INT                         | Configured by interval parameter of :ble_api:`GapScan_setPhyParams`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_SCAN_WIND                        | Configured by window parameter of :ble_api:`GapScan_setPhyParams`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_HIGH_SCAN_INT                    | Configured by interval parameter of :ble_api:`GapScan_setPhyParams`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_HIGH_SCAN_WIND                   | Configured by window parameter of :ble_api:`GapScan_setPhyParams`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_SCAN_INT                     | Configured by interval parameter of :ble_api:`GapScan_setPhyParams`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GEN_DISC_SCAN_WIND                    | Configured by window parameter of :ble_api:`GapScan_setPhyParams`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_SCAN_INT                     | Configured by interval parameter of :ble_api:`GapScan_setPhyParams`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_LIM_DISC_SCAN_WIND                    | Configured by window parameter of :ble_api:`GapScan_setPhyParams`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_INT_MIN                      | :ble_api:`GapInit_setPhyParam` with :ble_api:`INIT_PHYPARAM_CONN_INT_MIN`                                  |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_INT_MAX                      | :ble_api:`GapInit_setPhyParam` with :ble_api:`INIT_PHYPARAM_CONN_INT_MAX`                                  |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_SCAN_INT                     | :ble_api:`GapInit_setPhyParam` with :ble_api:`INIT_PHYPARAM_SCAN_INTERVAL`                                 |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_SCAN_WIND                    | :ble_api:`GapInit_setPhyParam` with :ble_api:`INIT_PHYPARAM_SCAN_WINDOW`                                   |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_SUPERV_TIMEOUT               | :ble_api:`GapInit_setPhyParam` with :ble_api:`INIT_PHYPARAM_SUP_TIMEOUT`                                   |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_LATENCY                      | :ble_api:`GapInit_setPhyParam` with :ble_api:`INIT_PHYPARAM_CONN_LATENCY`                                  |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_MIN_CE_LEN                   | Obsolete - Not Used by Controller                                                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_EST_MAX_CE_LEN                   | Obsolete - Not Used by Controller                                                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_PRIVATE_ADDR_INT                      | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_PRIVATE_ADDR_INT`                                    |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_PAUSE_CENTRAL                    | Obsolete - Not Used by Controller                                                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_CONN_PAUSE_PERIPHERAL                 | :ble_api:`GAP_UpdateLinkParamReq`                                                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_SM_TIMEOUT                            | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_SM_TIMEOUT`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_SM_MIN_KEY_LEN                        | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_SM_MIN_KEY_LEN`                                      |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_SM_MAX_KEY_LEN                        | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_SM_MAX_KEY_LEN`                                      |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_FILTER_ADV_REPORTS                    | Obsolete - Duplicate Filtering done in Controller                                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_SCAN_RSP_RSSI_MIN                     | :ble_api:`GapScan_setParam` with :ble_api:`SCAN_PARAM_FLT_MIN_RSSI`                                        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_REJECT_CONN_PARAMS                    | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_LINK_UPDATE_DECISION`                                |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_AUTH_TASK_ID                          | :ble_api:`GAP_SetParamValue` with ``GAP_PARAM_AUTH_TASK_ID``                                               |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_VERIFY_CAR                            | DEPRECATED                                                                                                 |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | TGAP_GGS_PARAMS                            | :ble_api:`GAP_SetParamValue` with ``GAP_PARAM_GGS_PARAMS``                                                 |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_IRK,                               | :ble_api:`GapConfig_SetParameter` with :ble_api:`GAP_CONFIG_PARAM_IRK`                                     |
    |            | GAPCENTRALROLE_IRK                         |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_SRK,                               | :ble_api:`GapConfig_SetParameter` with :ble_api:`GAP_CONFIG_PARAM_SRK`                                     |
    |            | GAPCENTRALROLE_SRK                         |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_BD_ADDR,                           | :ble_api:`HCI_ReadBDADDRCmd`                                                                               |
    |            | GAPCENTRALROLE_BD_ADDR                     |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADVERT_ENABLED,                    | :ble_api:`GapAdv_enable` and :ble_api:`GapAdv_disable`                                                     |
    |            | GAPROLE_ADV_NONCONN_ENABLED                |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADVERT_OFF_TIME                    | Configured by durationOrMaxEvents parameter of :ble_api:`GapAdv_enable`                                    |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADVERT_DATA                        | Various API:                                                                                               |
    |            |                                            |                                                                                                            |
    |            |                                            |    :ble_api:`GapAdv_loadByBuffer`                                                                          |
    |            |                                            |    :ble_api:`GapAdv_loadByHandle`                                                                          |
    |            |                                            |    :ble_api:`GapAdv_prepareLoadByBuffer`                                                                   |
    |            |                                            |    :ble_api:`GapAdv_prepareLoadByHandle`                                                                   |
    |            |                                            |    :ble_api:`GapAdv_getBuffer`                                                                             |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_SCAN_RSP_DATA                      | Various API:                                                                                               |
    |            |                                            |                                                                                                            |
    |            |                                            |    :ble_api:`GapAdv_loadByBuffer`                                                                          |
    |            |                                            |    :ble_api:`GapAdv_loadByHandle`                                                                          |
    |            |                                            |    :ble_api:`GapAdv_prepareLoadByBuffer`                                                                   |
    |            |                                            |    :ble_api:`GapAdv_prepareLoadByHandle`                                                                   |
    |            |                                            |    :ble_api:`GapAdv_getBuffer`                                                                             |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADV_EVENT_TYPE                     | :ble_api:`GapAdv_setParam` or :ble_api:`GapAdv_getParam` with :ble_api:`GAP_ADV_PARAM_PROPS`               |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADV_DIRECT_TYPE                    | :ble_api:`GapAdv_setParam` or :ble_api:`GapAdv_getParam` with :ble_api:`GAP_ADV_PARAM_PEER_ADDRESS_TYPE`   |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADV_DIRECT_ADDR                    | :ble_api:`GapAdv_setParam` or :ble_api:`GapAdv_getParam` with :ble_api:`GAP_ADV_PARAM_PEER_ADDRESS`        |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADV_CHANNEL_MAP                    | :ble_api:`GapAdv_setParam` or :ble_api:`GapAdv_getParam` with :ble_api:`GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP` |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_ADV_FILTER_POLICY                  | :ble_api:`GapAdv_setParam` or :ble_api:`GapAdv_getParam` with :ble_api:`GAP_ADV_PARAM_FILTER_POLICY`       |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_CONNHANDLE                         | Returned for each GAP event                                                                                |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_RSSI_READ_RATE                     | RSSI can be received by :ble_api:`HCI_ReadRssiCmd`                                                         |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_PARAM_UPDATE_ENABLE                | :ble_api:`GAP_UpdateLinkParamReq` can be called as desired                                                 |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_MIN_CONN_INTERVAL                  | pParams.intervalMin parameter of :ble_api:`GAP_UpdateLinkParamReq`                                         |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_MAX_CONN_INTERVAL                  | pParams.intervalMax parameter of :ble_api:`GAP_UpdateLinkParamReq`                                         |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_SLAVE_LATENCY                      | pParams.connLatency parameter of :ble_api:`GAP_UpdateLinkParamReq`                                         |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_TIMEOUT_MULTIPLIER                 | pParams.connTimeout parameter of :ble_api:`GAP_UpdateLinkParamReq`                                         |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_STATE                              | Obsolete - GAP changes remove the need for this                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_CONN_BD_ADDR,                      | Returned in :ble_api:`GAP_LINK_ESTABLISHED_EVENT`,                                                         |
    |            | GAPROLE_BD_ADDR_TYPE                       | contained in stack message, :ble_api:`gapEstLinkReqEvent_t` when the link is established                   |
    |            |                                            |                                                                                                            |
    |            |                                            | Or use :ble_api:`linkDB_GetInfo` at any time during the connection                                         |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_CONN_INTERVAL                      | Returned from :ble_api:`linkDB_GetInfo`, as linkDBInfo_t.connInterval                                      |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_CONN_LATENCY                       | Returned from :ble_api:`linkDB_GetInfo`, as linkDBInfo_t.connLatency                                       |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPROLE_CONN_TIMEOUT                       | Returned from :ble_api:`linkDB_GetInfo`, as linkDBInfo_t.connTimeout                                       |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPCENTRALROLE_MAX_SCAN_RES                | Configured by maxNumReport parameter of :ble_api:`GapScan_enable`                                          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP PARAM | GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY | :ble_api:`GAP_SetParamValue` with :ble_api:`GAP_PARAM_LINK_UPDATE_DECISION`                                |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_DeviceInit,                            | Declaration Change -  Use :ble_api:`GAP_DeviceInit` with parameter for roles desired                       |
    |            | GAPRole_StartDevice,                       |                                                                                                            |
    |            | GAPCentralRole_StartDevice                 |     See :ble_api:`GAP_PROFILE_BROADCASTER`                                                                 |
    |            |                                            |         :ble_api:`GAP_PROFILE_OBSERVER`                                                                    |
    |            |                                            |         :ble_api:`GAP_PROFILE_PERIPHERAL`                                                                  |
    |            |                                            |         :ble_api:`GAP_PROFILE_CENTRAL`                                                                     |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAPRole_RegisterAppCBs                     | Obsolete - Functionality moved to :ble_api:`GAPBondMgr_Register`                                           |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_SetAdvToken                            | Obsolete - Advertisement Sets are Used                                                                     |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_GetAdvToken                            | Obsolete - Advertisement Sets are Used                                                                     |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_RemoveAdvToken                         | Obsolete - Advertisement Sets are Used                                                                     |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_UpdateAdvTokens                        | Obsolete - Advertisement Sets are Used                                                                     |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAPRole_SendUpdateParam,                   | :ble_api:`GAP_UpdateLinkParamReq`                                                                          |
    |            | GAPCentralRole_UpdateLink                  |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_MakeDiscoverable                       | :ble_api:`GapAdv_enable`                                                                                   |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_UpdateAdvertisingData                  | Various API:                                                                                               |
    |            |                                            |                                                                                                            |
    |            |                                            |    :ble_api:`GapAdv_loadByBuffer`                                                                          |
    |            |                                            |    :ble_api:`GapAdv_loadByHandle`                                                                          |
    |            |                                            |    :ble_api:`GapAdv_prepareLoadByBuffer`                                                                   |
    |            |                                            |    :ble_api:`GapAdv_prepareLoadByHandle`                                                                   |
    |            |                                            |    :ble_api:`GapAdv_getBuffer`                                                                             |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_EndDiscoverable                        | :ble_api:`GapAdv_disable`                                                                                  |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_DeviceDiscoveryRequest,                | :ble_api:`GapScan_enable`                                                                                  |
    |            | GAPCentralRole_StartDiscovery              |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_DeviceDiscoveryCancel,                 | :ble_api:`GapScan_disable`                                                                                 |
    |            | GAPCentralRole_CancelDiscovery             |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_ResolvePrivateAddr                     | Obsolete - Address Resolution is done controller                                                           |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_EstablishLinkReq,                      | :ble_api:`GapInit_connect`, or :ble_api:`GapInit_connectWl` to use Filter Accept List                      |
    |            | GAPCentralRole_EstablishLink               |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_TerminateLinkReq,                      | :ble_api:`GapInit_cancelConnect` for connection request, :ble_api:`GAP_TerminateLinkReq` otherwise         |
    |            | GAPRole_TerminateConnection,               |                                                                                                            |
    |            | GAPCentralRole_TerminateLink               |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP API   | GAP_ConfigDeviceAddr                       | Obsolete - Only way to configure the device address is as parameters in :ble_api:`GAP_DeviceInit`          |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP CB    | gapRolesParamUpdateCB_t,                   | These are handled through :ble_api:`GAP_UPDATE_LINK_PARAM_REQ_EVENT`,                                      |
    |            | paramUpdateAppDecision_t,                  | applies to the L2CAP Parameter Update Procedure as well.                                                   |
    |            | passThroughToApp_t                         |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+
    |  GAP CB    | gapRolesStateNotify_t,                     | Moved into GAP Bond Manager callbacks, :ble_api:`gapBondCBs_t`                                             |
    |            | pfnGapCentralRoleEventCB_t                 |                                                                                                            |
    +------------+--------------------------------------------+------------------------------------------------------------------------------------------------------------+

.. _tbl_ble5_porting_gapbondmgr_changes_cc2640r2_to_cc26x2:
.. table:: GAP Bond Manager Changes

    +--------------------------------------------------+----------------------------------------------+
    | Previous Implementation                          | New/Current implementation                   |
    +================+=================================+==============================================+
    |    Type        |   Name                          | Description / API / Parameter                |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND PARAM | GAPBOND_DEFAULT_PASSCODE        | Use :ble_api:`pfnPasscodeCB_t`,              |
    |                |                                 | shared default passcode defined in bcomdef.h |
    |                |                                 | :ble_api:`B_APP_DEFAULT_PASSCODE`            |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND PARAM | GAPBOND_REMOTE_OOB_SC_ENABLED   | Obsolete                                     |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND PARAM | GAPBOND_REMOTE_OOB_SC_DATA      | Obsolete                                     |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND PARAM | GAPBOND_LOCAL_OOB_SC_ENABLED    | Obsolete                                     |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND PARAM | GAPBOND_LOCAL_OOB_SC_DATA       | Obsolete                                     |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND STATE | GAPBOND_PAIRING_STATE_BONDED    | :ble_api:`GAPBOND_PAIRING_STATE_ENCRYPTED`   |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND DEF   | GBM_QUEUE_PAIRINGS              | Removed, is now default behavior             |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND DEF   | GBM_GATT_NO_CLIENT              | Configured by ``GATT_NO_CLIENT``             |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND DEF   | SNP_SECURITY                    | Configured by ``GAPBONDMGR_NO_SIGNING``      |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_LinkEst              | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_LinkTerm             | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_SlaveReqSecurity     | :ble_api:`GAPBondMgr_Pair`, allowing both    |
    |                |                                 | Centrals and Peripherals to request pairing  |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_UpdateCharCfg        | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_ReadGattChar         | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_SupportsEnhancedPriv | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_CheckNVLen           | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+
    |  GAPBOND API   | GAPBondMgr_syncResolvingList    | Removed Application Access to API            |
    |                |                                 | Handled Internally                           |
    +----------------+---------------------------------+----------------------------------------------+

.. _tbl_ble5_porting_gapgattserver_changes_cc2640r2_to_cc26x2:
.. table:: GAP GATT Server Changes

    +-------------------------------------------------+-----------------------------------+
    | Previous Implementation                         | New/Current implementation        |
    +============+====================================+===================================+
    |    Type    |   Name                             | Description / API / Parameter     |
    +------------+------------------------------------+-----------------------------------+
    |  GGS PARAM | GGS_PERI_PRIVACY_FLAG_ATT          | Obsolete                          |
    +------------+------------------------------------+-----------------------------------+
    |  GGS PARAM | GGS_RECONNCT_ADDR_ATT              | Obsolete                          |
    +------------+------------------------------------+-----------------------------------+
    |  GGS PARAM | GGS_PERI_PRIVACY_FLAG_PROPS        | Obsolete                          |
    +------------+------------------------------------+-----------------------------------+
    |  GGS PARAM | GGS_W_PERMIT_PRIVACY_FLAG_ATT      | Obsolete                          |
    +------------+------------------------------------+-----------------------------------+
    |  GGS PARAM | GGS_TESTMODE_W_PERMIT_PRIVACY_FLAG | Obsolete                          |
    +------------+------------------------------------+-----------------------------------+

.. _tbl_ble5_porting_linkdb_changes_cc2640r2_to_cc26x2:
.. table:: Link Database Changes

    +--------------------------------------------+-----------------------------------+
    | Previous Implementation                    | New/Current implementation        |
    +============+===============================+===================================+
    |    Type    |   Name                        | Description / API / Parameter     |
    +------------+-------------------------------+-----------------------------------+
    | LinkDB API | linkDB_Remove                 | API now accepts                   |
    |            |                               | :ble_api:`linkDBInfo_t` in        |
    |            |                               | addition to connection handle     |
    +------------+-------------------------------+-----------------------------------+

.. _tbl_ble5_porting_sample_app_changes:
.. table:: Sample Simple Peripheral App Changes

    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | **Previous Implementation**                            | **BLE5-Stack 1.02.00 Implementation**                                           |
    +========================================================+=================================================================================+
    | SimpleBLEPeripheral_processStateChangeEvt              | See ``SimplePeripheral_processGapMessage``                                      |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | SimpleBLEPeripheral_processAppMsg                      | Different events are now being handled. See ``SimplePeripheral_processAppMsg``  |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | SimpleBLEPeripheral_processStackMsg                    | See the guide’s step to ``Replace GAP Event processing``                        |
    |                                                        |                                                                                 |                                                                                                        
    |                                                        |  This is modified to process :ble_api:`GAP_MSG_EVENT`                           |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | SimpleBLEPeripheral_stateChangeCB                      | See the guide’s step to ``Replace GAP Event processing``                        |
    | gapRolesCBs_t SimpleBLEPeripheral_gapRoleCBs           |                                                                                 |  
    |                                                        |  This is no longer used. GAP events are now returned to the application         |
    |                                                        |  directly as the RTOS event, :ble_api:`GAP_MSG_EVENT`                           |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAP_SetParamValue(TGAP_CONN_PAUSE_PERIPHERAL,          | :ble_api:`GAP_UpdateLinkParamReq`                                               |
    | DEFAULT_CONN_PAUSE_PERIPHERAL)                         |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED,           | In ``SimplePeripheral_processGapMessage`` by :ble_api:`GapAdv_enable`           |
    | sizeof(uint8_t),&initialAdvertEnable)                  |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_ADVERT_OFF_TIME,          | In ``SimplePeripheral_processGapMessage`` by :ble_api:`GapAdv_enable`.          |
    | sizeof(uint16_t),&advertOffTime)                       | Configured by the third parameter ``durationOrMaxEvents``                       |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_SCAN_RSP_DATA,            | In ``SimplePeripheral_processGapMessage`` by :ble_api:`GapAdv_loadByHandle`.    |
    | sizeof(scanRspData),scanRspData)                       | with :ble_api:`GAP_ADV_DATA_TYPE_SCAN_RSP` set as the data type                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_ADVERT_DATA,              | In ``SimplePeripheral_processGapMessage`` by :ble_api:`GapAdv_loadByHandle`     |
    | sizeof(advertData), advertData)                        | with :ble_api:`GAP_ADV_DATA_TYPE_ADV` set as the data type                      |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE,      | In ``SimplePeripheral_processGapMessage``,                                      |
    | sizeof(uint8_t), &enableUpdateRequest)                 | parameter updates from a central device are                                     |
    |                                                        | handled in :ble_api:`GAP_UPDATE_LINK_PARAM_REQ_EVENT` and                       |
    |                                                        | uses :ble_api:`GAP_UpdateLinkParamReqReply`                                     |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_MIN_CONN_INTERVAL,        | In ``SimplePeripheral_processParamUpdate``,                                     |
    | sizeof(uint16_t), &desiredMinInterval)                 | set as ``DEFAULT_DESIRED_MIN_CONN_INTERVAL``                                    |
    |                                                        | and applied with :ble_api:`GAP_UpdateLinkParamReq`                              |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_MAX_CONN_INTERVAL,        | In ``SimplePeripheral_processParamUpdate``,                                     |
    | sizeof(uint16_t), &desiredMaxInterval)                 | set as ``DEFAULT_DESIRED_MAX_CONN_INTERVAL``                                    |
    |                                                        | and applied with :ble_api:`GAP_UpdateLinkParamReq`                              |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_SLAVE_LATENCY,            | In ``SimplePeripheral_processParamUpdate``,                                     |
    | sizeof(uint16_t), &desiredSlaveLatency)                | set as ``DEFAULT_DESIRED_SLAVE_LATENCY``                                        |
    |                                                        | and applied with :ble_api:`GAP_UpdateLinkParamReq`                              |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPRole_SetParameter(GAPROLE_TIMEOUT_MULTIPLIER,       | In ``SimplePeripheral_processParamUpdate``,                                     |
    | sizeof(uint16_t), &desiredConnTimeout)                 | set as ``DEFAULT_DESIRED_CONN_TIMEOUT``                                         |
    |                                                        | and applied with :ble_api:`GAP_UpdateLinkParamReq`                              |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MIN,           | :ble_api:`GapAdv_setParam`                                                      |
    | advInt)                                                | with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN`                              |
    | GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MIN,           |                                                                                 |
    | advInt)                                                |                                                                                 |
    |                                                        |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MAX,           | :ble_api:`GapAdv_setParam`                                                      |
    | advInt)                                                | with :ble_api:`GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX`                              |
    | GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MAX,           |                                                                                 |
    | advInt)                                                |                                                                                 |
    |                                                        |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    |  GAPBondMgr_SetParameter(GAPBOND_DEFAULT_PASSCODE,     |                                                                                 |
    |  sizeof(uint32_t), &passkey)                           | Use :ble_api:`pfnPasscodeCB_t`,                                                 |
    |                                                        | shared default passcode defined in bcomdef.h                                    |
    |                                                        | :ble_api:`B_APP_DEFAULT_PASSCODE`                                               |
    |                                                        |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPROLE_STATE                                          | Obsolete - GAP changes remove the need for this                                 |
    |                                                        |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+
    | GAPROLE_CONNHANDLE                                     | Returned for each GAP event                                                     |
    |                                                        |                                                                                 |
    +--------------------------------------------------------+---------------------------------------------------------------------------------+