API Documentation  9.14.00
Data Fields
PDMCC26XX_HWAttrs Struct Reference

PDMCC26XX Hardware attributes. More...

Data Fields

uint32_t micPower
 
int taskPriority
 

Detailed Description

PDMCC26XX Hardware attributes.

These fields are used by the PDM driver

Field Documentation

§ micPower

uint32_t PDMCC26XX_HWAttrs::micPower

Microphone power pin

§ taskPriority

int PDMCC26XX_HWAttrs::taskPriority

PDM task priority pin


The documentation for this struct was generated from the following file: