API Documentation  9.14.00
Data Fields
I2CCC26XX_I2CPinCfg Struct Reference

I2CCC26XX Pin Configuration. More...

Data Fields

uint8_t pinSCL
 
uint8_t pinSDA
 

Detailed Description

I2CCC26XX Pin Configuration.

Pin configuration that holds non-default pins. The default pin configuration is typically defined in I2CCC26XX_HWAttrsV1 placed in the board file. The pin configuration structure is used by setting the custom void pointer in the I2C_Params to point to this struct. If the custom void pointer is NULL, the I2CCC26XX_HWAttrsV1 pin mapping will be used.

I2C_Handle handle;
I2C_Params i2cParams;
I2C_Params_init(&i2cParams); // sets custom to NULL
pinCfg.pinSDA = CONFIG_I2C0_SDA1;
pinCfg.pinSCL = CONFIG_I2C0_SCL1;
i2cParams.custom = &pinCfg;
handle = I2C_open(CONFIG_I2C, &i2cParams);

The documentation for this struct was generated from the following file: