API Documentation  9.14.00
Data Fields
Display_Params Struct Reference

Display Parameters. More...

Data Fields

Display_LineClearMode lineClearMode
 

Detailed Description

Display Parameters.

Display parameters are used with the Display_open() call. Default values for these parameters are set using Display_Params_init().

See also
Display_Params_init()

The documentation for this struct was generated from the following file: