|
API Documentation
9.14.00
|
The definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation. More...
Data Fields | |
| ADC_CloseFxn | closeFxn |
| ADC_ControlFxn | controlFxn |
| ADC_ConvertChainFxn | convertChainFxn |
| ADC_ConvertFxn | convertFxn |
| ADC_ConvertToMicroVoltsFxn | convertToMicroVolts |
| ADC_InitFxn | initFxn |
| ADC_OpenFxn | openFxn |
The definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation.
| ADC_CloseFxn ADC_FxnTable::closeFxn |
Function to close the specified peripheral
| ADC_ControlFxn ADC_FxnTable::controlFxn |
Function to perform implementation specific features
| ADC_ConvertChainFxn ADC_FxnTable::convertChainFxn |
Function to initiate an ADC multi-channel conversion
| ADC_ConvertFxn ADC_FxnTable::convertFxn |
Function to initiate an ADC single channel conversion
| ADC_ConvertToMicroVoltsFxn ADC_FxnTable::convertToMicroVolts |
Function to convert ADC result to microvolts
| ADC_InitFxn ADC_FxnTable::initFxn |
Function to initialize the given data object
| ADC_OpenFxn ADC_FxnTable::openFxn |
Function to open the specified peripheral
1.8.12