|
API Documentation
9.14.00
|
Watchdog driver interface. More...
Go to the source code of this file.
Data Structures | |
| struct | Watchdog_Config_ |
| Watchdog Global configuration. More... | |
| struct | Watchdog_FxnTable |
| The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation. More... | |
| struct | Watchdog_Params |
| Watchdog Parameters. More... | |
Macros | |
| #define | Watchdog_CMD_RESERVED (32) |
| #define | Watchdog_STATUS_ERROR (-1) |
| Generic error status code returned by Watchdog_control(). More... | |
| #define | Watchdog_STATUS_RESERVED (-32) |
| #define | Watchdog_STATUS_SUCCESS (0) |
| Successful status code returned by Watchdog_control(). More... | |
| #define | Watchdog_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by Watchdog_control() for undefined command codes. More... | |
| #define | Watchdog_STATUS_UNSUPPORTED (-3) |
| An error status code returned by Watchdog_setReload() for drivers which do not support the aforementioned API. More... | |
Typedefs | |
| typedef void(* | Watchdog_Callback) (uintptr_t handle) |
| Watchdog callback pointer. More... | |
| typedef void(* | Watchdog_ClearFxn) (Watchdog_Handle handle) |
| A function pointer to a driver specific implementation of Watchdog_clear(). | |
| typedef void(* | Watchdog_CloseFxn) (Watchdog_Handle handle) |
| A function pointer to a driver specific implementation of Watchdog_close(). | |
| typedef struct Watchdog_Config_ | Watchdog_Config |
| Watchdog Global configuration. More... | |
| typedef int_fast16_t(* | Watchdog_ControlFxn) (Watchdog_Handle handle, uint_fast16_t cmd, void *arg) |
| A function pointer to a driver specific implementation of Watchdog_control(). | |
| typedef uint32_t(* | Watchdog_ConvertMsToTicksFxn) (Watchdog_Handle handle, uint32_t milliseconds) |
| A function pointer to a driver specific implementation of Watchdog_ConvertMsToTicksFxn(). | |
| typedef struct Watchdog_Config_ * | Watchdog_Handle |
| Watchdog Handle. | |
| typedef void(* | Watchdog_InitFxn) (Watchdog_Handle handle) |
| A function pointer to a driver specific implementation of Watchdog_init(). | |
| typedef Watchdog_Handle(* | Watchdog_OpenFxn) (Watchdog_Handle handle, Watchdog_Params *params) |
| A function pointer to a driver specific implementation of Watchdog_open(). | |
| typedef int_fast16_t(* | Watchdog_SetReloadFxn) (Watchdog_Handle handle, uint32_t ticks) |
| A function pointer to a driver specific implementation of Watchdog_setReload(). | |
Enumerations | |
| enum | Watchdog_DebugMode { Watchdog_DEBUG_STALL_ON, Watchdog_DEBUG_STALL_OFF } |
| Watchdog debug stall settings. More... | |
| enum | Watchdog_ResetMode { Watchdog_RESET_OFF, Watchdog_RESET_ON } |
| Watchdog reset mode settings. More... | |
Functions | |
| void | Watchdog_clear (Watchdog_Handle handle) |
| Clears the Watchdog. More... | |
| void | Watchdog_close (Watchdog_Handle handle) |
| Function to close a Watchdog peripheral specified by the Watchdog handle. It stops (holds) the Watchdog counting on applicable platforms. More... | |
| int_fast16_t | Watchdog_control (Watchdog_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs implementation specific features on a given Watchdog_Handle. More... | |
| uint32_t | Watchdog_convertMsToTicks (Watchdog_Handle handle, uint32_t milliseconds) |
| Converts milliseconds to Watchdog clock ticks. More... | |
| void | Watchdog_init (void) |
| Initializes the Watchdog module. More... | |
| Watchdog_Handle | Watchdog_open (uint_least8_t index, Watchdog_Params *params) |
| Opens a Watchdog. More... | |
| void | Watchdog_Params_init (Watchdog_Params *params) |
| Function to initialize the Watchdog_Params structure to its defaults. More... | |
| int_fast16_t | Watchdog_setReload (Watchdog_Handle handle, uint32_t ticks) |
| Sets the Watchdog reload value. More... | |
Watchdog driver interface.
A watchdog timer can be used to generate a reset signal if a system has become unresponsive. The Watchdog driver simplifies configuring and starting the watchdog peripherals. The watchdog peripheral can be configured with resets either on or off and a user-specified timeout period.
When the watchdog peripheral is configured not to generate a reset, it can be used to cause a hardware interrupt at a programmable interval. The driver provides the ability to specify a user-provided callback function that is called when the watchdog causes an interrupt.
The Watchdog driver simplifies configuring and starting the Watchdog peripherals. The Watchdog can be set up to produce a reset signal after a timeout, or simply cause a hardware interrupt at a programmable interval. The driver provides the ability to specify a callback function that is called when the Watchdog causes an interrupt.
When resets are turned on, it is the user application's responsibility to call Watchdog_clear() in order to clear the Watchdog and prevent a reset. Watchdog_clear() can be called at any time.
This section will cover driver usage.
Open the driver with default settings:
The Watchdog driver must be initialized by calling Watchdog_init(), before any other Watchdog APIs can be called. Once the watchdog is initialized, a Watchdog object can be created through the following steps:
To have a user-defined function run at the hardware interrupt caused by a watchdog timer timeout, define a function of the following type:
Then pass the function to Watchdog_open() through the Watchdog_Params structure.
An example of the Watchdog creation process that uses a callback function:
If no Watchdog_Params structure is passed to Watchdog_open(), the default values are used. By default, the Watchdog driver has resets turned on, no callback function specified, and stalls the timer at breakpoints during debugging. For CC35XX devices, debug stalling is not supported.
Options for the resetMode parameter are Watchdog_RESET_ON and Watchdog_RESET_OFF. The latter allows the watchdog to be used like another timer interrupt. When resetMode is Watchdog_RESET_ON, it is up to the application to call Watchdog_clear() to clear the Watchdog interrupt flag to prevent a reset. Watchdog_clear() can be called at any time.
Refer to the Driver's Configuration section for more information.
| typedef void(* Watchdog_Callback) (uintptr_t handle) |
Watchdog callback pointer.
This is the typedef for the function pointer that will allow a callback function to be specified in the Watchdog_Params structure. The function will take a Watchdog_Handle of the Watchdog causing the interrupt (cast as a uintptr_t) as an argument.
| typedef struct Watchdog_Config_ Watchdog_Config |
Watchdog Global configuration.
The Watchdog_Config structure contains a set of pointers used to characterize the Watchdog driver implementation.
This structure needs to be defined before calling Watchdog_init() and it must not be changed thereafter.
| enum Watchdog_DebugMode |
Watchdog debug stall settings.
This enumeration defines the debug stall modes for the Watchdog. On some targets, the Watchdog timer will continue to count down while a debugging session is halted. To avoid unwanted resets, the Watchdog can be set to stall while the processor is stopped by the debugger.
| Enumerator | |
|---|---|
| Watchdog_DEBUG_STALL_ON | Watchdog will be stalled at breakpoints |
| Watchdog_DEBUG_STALL_OFF | Watchdog will keep running at breakpoints |
| enum Watchdog_ResetMode |
Watchdog reset mode settings.
This enumeration defines the reset modes for the Watchdog. The Watchdog can be configured to either generate a reset upon timeout or simply produce a periodic interrupt.
| Enumerator | |
|---|---|
| Watchdog_RESET_OFF | Timeouts generate interrupts only |
| Watchdog_RESET_ON | Generates reset after timeout |
| void Watchdog_clear | ( | Watchdog_Handle | handle | ) |
Clears the Watchdog.
Clears the Watchdog to to prevent a reset signal from being generated if the module is in Watchdog_RESET_ON reset mode.
| handle | A Watchdog_Handle |
| void Watchdog_close | ( | Watchdog_Handle | handle | ) |
Function to close a Watchdog peripheral specified by the Watchdog handle. It stops (holds) the Watchdog counting on applicable platforms.
| handle | A Watchdog_Handle returned from Watchdog_open() |
| int_fast16_t Watchdog_control | ( | Watchdog_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs implementation specific features on a given Watchdog_Handle.
Commands for Watchdog_control can originate from Watchdog.h or from implementation specific Watchdog*.h files. While commands from Watchdog.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific Watchdog*.h files add unique driver capabilities but are not API portable across all Watchdog driver implementations.
Commands supported by Watchdog.h follow a Watchdog_CMD_<cmd> naming convention.
Commands supported by Watchdog*.h follow a Watchdog*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See Watchdog_control command codes for command codes.
See Watchdog_control return status codes for status codes.
| handle | A Watchdog_Handle returned from Watchdog_open() |
| cmd | Watchdog.h or Watchdog*.h commands. |
| arg | An optional R/W (read/write) command argument accompanied with cmd |
| uint32_t Watchdog_convertMsToTicks | ( | Watchdog_Handle | handle, |
| uint32_t | milliseconds | ||
| ) |
Converts milliseconds to Watchdog clock ticks.
Converts the input value into number of Watchdog clock ticks as close as possible. If the converted value exceeds 32 bits, a zero (0) will be returned to indicate overflow. For WFF3, a zero (0) indicates that the value exceeds the maximum allowed value or falls bellow the minimum possible value. The converted value can be used as the function parameter 'ticks' in Watchdog_setReload().
This API is not applicable for all platforms. See the page for your specific driver implementation for details.
| handle | A Watchdog_Handle |
| milliseconds | Value to be converted |
| void Watchdog_init | ( | void | ) |
Initializes the Watchdog module.
The application-provided Watchdog_config must be present before the Watchdog_init() function is called. The Watchdog_config must be persistent and not changed after Watchdog_init is called. This function must be called before any of the other Watchdog driver APIs.
| Watchdog_Handle Watchdog_open | ( | uint_least8_t | index, |
| Watchdog_Params * | params | ||
| ) |
Opens a Watchdog.
Opens a Watchdog object with the index and parameters specified, and returns a Watchdog_Handle.
| index | Logical peripheral number for the Watchdog indexed into the Watchdog_config table |
| params | Pointer to a Watchdog_Params, if NULL it will use default values. All the fields in this structure are RO (read-only). |
| void Watchdog_Params_init | ( | Watchdog_Params * | params | ) |
Function to initialize the Watchdog_Params structure to its defaults.
| params | A pointer to Watchdog_Params structure for initialization |
Default parameters: callbackFxn = NULL resetMode = Watchdog_RESET_ON debugStallMode = Watchdog_DEBUG_STALL_ON
| int_fast16_t Watchdog_setReload | ( | Watchdog_Handle | handle, |
| uint32_t | ticks | ||
| ) |
Sets the Watchdog reload value.
Sets the value from which the Watchdog will countdown after it reaches zero or Watchdog_clear() is called. This is how the reload value can be changed after the Watchdog has already been opened. The new reload value will be loaded into the Watchdog timer when this function is called. Watchdog_setReload is not reentrant. For CC13XX/CC26XX, if the parameter 'ticks' is set to zero (0), a Watchdog interrupt is immediately generated.
This API is not applicable for all platforms. See the page for your specific driver implementation for details.
| handle | A Watchdog_Handle |
| ticks | Value to be loaded into Watchdog timer Unit is in Watchdog clock ticks |
1.8.12