347 #ifndef ti_drivers_Power__include 348 #define ti_drivers_Power__include 355 #include <ti/drivers/utils/List.h> 356 #include <ti/devices/DeviceFamily.h> 367 #define Power_TOTAL (1U) 368 #define Power_RESUME (2U) 374 #define Power_NOTIFYDONE (0) 375 #define Power_NOTIFYERROR (-1) 381 #define Power_SOK (0) 382 #define Power_EFAIL (-1) 383 #define Power_EINVALIDINPUT (-2) 384 #define Power_EINVALIDPOINTER (-3) 385 #define Power_ECHANGE_NOT_ALLOWED (-4) 386 #define Power_EBUSY (-5) 392 #define Power_ACTIVE (1U) 393 #define Power_ENTERING_SLEEP (2U) 394 #define Power_EXITING_SLEEP (3U) 395 #define Power_ENTERING_SHUTDOWN (4U) 401 typedef void (*Power_PolicyInitFxn)(void); 429 typedef int_fast16_t (*
Power_NotifyFxn)(uint_fast16_t eventType, uintptr_t eventArg, uintptr_t clientArg);
696 uint_fast16_t eventTypes,
698 uintptr_t clientArg);
893 int_fast16_t
Power_shutdown(uint_fast16_t shutdownState, uint_fast32_t shutdownTime);
918 int_fast16_t
Power_sleep(uint_fast16_t sleepState);
939 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X0_CC26X0 || \ 940 DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X1_CC26X1 || \ 941 DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2 || \ 942 DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 944 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC23X0) 945 #include <ti/drivers/power/PowerCC23X0.h> 946 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) 947 #include <ti/drivers/power/PowerCC27XX.h> 948 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC35XX) 949 #include <ti/drivers/power/PowerWFF3.h> uint_fast32_t Power_getTransitionLatency(uint_fast16_t sleepState, uint_fast16_t type)
Get the hardware transition latency for a sleep state.
int_fast16_t Power_sleep(uint_fast16_t sleepState)
Transition the device into a sleep state.
int_fast16_t Power_init(void)
Power initialization function.
Power_NotifyFxn notifyFxn
Definition: Power.h:445
Power manager interface for CC26XX/CC13XX.
int_fast16_t(* Power_NotifyFxn)(uint_fast16_t eventType, uintptr_t eventArg, uintptr_t clientArg)
Power notify callback function used with the Power_registerNotify()
Definition: Power.h:429
int_fast16_t Power_setDependency(Power_Resource resourceId)
Declare a dependency upon a resource.
int_fast16_t Power_setConstraint(uint_fast16_t constraintId)
Declare an operational constraint.
int_fast16_t Power_registerNotify(Power_NotifyObj *pNotifyObj, uint_fast16_t eventTypes, Power_NotifyFxn notifyFxn, uintptr_t clientArg)
Register a function to be called upon a specific power event.
void(* Power_PolicyFxn)(void)
Power policy function pointer.
Definition: Power.h:406
bool Power_disablePolicy(void)
Disable the configured power policy from running when the CPU is idle.
uintptr_t clientArg
Definition: Power.h:446
int_fast16_t Power_shutdown(uint_fast16_t shutdownState, uint_fast32_t shutdownTime)
Put the device into a shutdown state.
int_fast16_t Power_getDependencyCount(Power_Resource resourceId)
Get the current dependency count for a resource.
uint_fast16_t eventTypes
Definition: Power.h:444
int_fast16_t Power_releaseDependency(Power_Resource resourceId)
Release a previously declared dependency.
void Power_setPolicy(Power_PolicyFxn policy)
Set a new Power policy.
uint32_t Power_Resource
Power resource identifier.
Definition: Power.h:452
Power notify object structure.
Definition: Power.h:441
void Power_unregisterNotify(Power_NotifyObj *pNotifyObj)
Unregister previously registered notifications.
void Power_reset(void)
Resets the system and causes it to reboot.
uint_fast32_t Power_getConstraintMask(void)
Get the constraints that have been declared with Power.
uint_fast16_t Power_getTransitionState(void)
Get the current transition state of the Power Manager.
List_Elem link
Definition: Power.h:443
int_fast16_t Power_releaseConstraint(uint_fast16_t constraintId)
Release a previously declared constraint.
void Power_enablePolicy(void)
Enable the configured power policy to run when the CPU is idle.
int_fast16_t Power_getConstraintCount(uint_fast16_t constraintId)
Get the current constraint count for an operational transition.
void Power_idleFunc(void)
Power function to be added to the application idle loop.