128 #ifndef ti_display_DisplayUart2__include 129 #define ti_display_DisplayUart2__include 131 #include <ti/drivers/dpl/SemaphoreP.h> 137 #define DisplayUart2_SCROLLING 0xFF 173 SemaphoreP_Handle mutex;
186 void DisplayUart2Min_clearLines(
Display_Handle handle, uint8_t fromLine, uint8_t toLine);
187 void DisplayUart2Ansi_clearLines(
Display_Handle handle, uint8_t fromLine, uint8_t toLine);
189 void DisplayUart2Min_vprintf(
Display_Handle handle, uint8_t line, uint8_t column,
const char *fmt, va_list va);
190 void DisplayUart2Ansi_vprintf(
Display_Handle handle, uint8_t line, uint8_t column,
const char *fmt, va_list va);
195 int DisplayUart2Min_control(
Display_Handle handle,
unsigned int cmd,
void *arg);
196 int DisplayUart2Ansi_control(
Display_Handle handle,
unsigned int cmd,
void *arg);
198 unsigned int DisplayUart2Min_getType(
void);
199 unsigned int DisplayUart2Ansi_getType(
void);
UART2 Global configuration.
Definition: UART2.h:721
PRELIMINARY UART driver interface
unsigned int uartIdx
Definition: DisplayUart2.h:154
Display Parameters.
Definition: Display.h:485
char * strBuf
Definition: DisplayUart2.h:160
DisplayUart2 Object.
Definition: DisplayUart2.h:170
Generic interface for text output.
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:535
uint16_t strBufLen
Definition: DisplayUart2.h:162
unsigned int baudRate
Definition: DisplayUart2.h:156
Display Global configuration.
Definition: Display.h:558
unsigned int mutexTimeout
Definition: DisplayUart2.h:158
DisplayUart2 Attributes.
Definition: DisplayUart2.h:151