|
API Documentation
9.14.00
|
Extention of Display to access GrLib functionality in capable displays. More...
Go to the source code of this file.
Data Structures | |
| struct | DisplayGrLib_Object |
Macros | |
| #define | DisplayExt_getGraphicsContext(handle) DisplayExt_doGetGraphicsContext(handle) |
Typedefs | |
| typedef struct DisplayGrLib_Object * | DisplayGrLib_Handle |
| typedef struct DisplayGrLib_Object | DisplayGrLib_Object |
Functions | |
| Graphics_Context * | DisplayExt_doGetGraphicsContext (Display_Handle handle) |
| Get the Graphics_Context object of the first available and open Display that uses GrLib for output. More... | |
Extention of Display to access GrLib functionality in capable displays.
============================================================================
The display header file should be included in an application as follows:
This extension depends on an already opened Display interface, and accesses the global Display_config object.
First, the regular Display interface must be opened, and after that, APIs in this extension become usable.
This interface expects that all Display implementations that report type Display_Type_GRLIB will also 'inherit' the DisplayGrLib_Object so that the implementation specific instance object can be cast to the type DisplayGrLib_Object.
In practice this means that the Graphics_Context object used to control GrLib by the display implementation must be the first member of the Object structure used by that implementation.
For example, Display_SharpObject can be cast to DisplayGrLib_Object to access the Graphics_Context object, without this interface having prior knowledge about the Sharp display implementation.
The Display interface produces log statements if instrumentation is enabled.
| Diagnostics Mask | Log details |
|---|---|
| Diags_USER1 | basic operations performed |
| Diags_USER2 | detailed operations performed |
| #define DisplayExt_getGraphicsContext | ( | handle | ) | DisplayExt_doGetGraphicsContext(handle) |
Get Graphics_Context of first opened Display that uses GrLib
| Graphics_Context* DisplayExt_doGetGraphicsContext | ( | Display_Handle | handle | ) |
Get the Graphics_Context object of the first available and open Display that uses GrLib for output.
Useful for drawing graphics if you know that the display is GrLib capable.
1.8.12