|
TI OAD API Documentation
9.14.00
|
Functions | |
| psa_status_t | psa_export_key (psa_key_id_t key, uint8_t *data, size_t data_size, size_t *data_length) |
| Export a key in binary format. More... | |
| psa_status_t | psa_export_public_key (psa_key_id_t key, uint8_t *data, size_t data_size, size_t *data_length) |
| Export a public key or the public part of a key pair in binary format. More... | |
| psa_status_t | psa_import_key (const psa_key_attributes_t *attributes, const uint8_t *data, size_t data_length, psa_key_id_t *key) |
| Import a key in binary format. More... | |
| psa_status_t psa_export_key | ( | psa_key_id_t | key, |
| uint8_t * | data, | ||
| size_t | data_size, | ||
| size_t * | data_length | ||
| ) |
Export a key in binary format.
The output of this function can be passed to psa_import_key() to create an equivalent object.
If the implementation of psa_import_key() supports other formats beyond the format specified here, the output from psa_export_key() must use the representation specified here, not the original representation.
For standard key types, the output format is as follows:
RSAPrivateKey, version 0. ceiling(m/8)-byte string where m is the bit size associated with the curve, i.e. the bit size of the order of the curve's coordinate field. This byte string is in little-endian order for Montgomery curves (curve types PSA_ECC_FAMILY_CURVEXXX), and in big-endian order for Weierstrass curves (curve types PSA_ECC_FAMILY_SECTXXX, PSA_ECC_FAMILY_SECPXXX and PSA_ECC_FAMILY_BRAINPOOL_PXXX). For Weierstrass curves, this is the content of the privateKey field of the ECPrivateKey format defined by RFC 5915. For Montgomery curves, the format is defined by RFC 7748, and output is masked according to s5. For twisted Edwards curves, the private key is as defined by RFC 8032 (a 32-byte string for Edwards25519, a 57-byte string for Edwards448).x as a big-endian byte string. The length of the byte string is the private key size in bytes (leading zeroes are not stripped).The policy on the key must have the usage flag #PSA_KEY_USAGE_EXPORT set.
| key | Identifier of the key to export. It must allow the usage #PSA_KEY_USAGE_EXPORT, unless it is a public key. | |
| [out] | data | Buffer where the key data is to be written. |
| data_size | Size of the data buffer in bytes. | |
| [out] | data_length | On success, the number of bytes that make up the key data. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_NOT_PERMITTED | The key does not have the #PSA_KEY_USAGE_EXPORT flag. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_BUFFER_TOO_SMALL | The size of the data buffer is too small. You can determine a sufficient buffer size by calling #PSA_EXPORT_KEY_OUTPUT_SIZE(type, bits) where type is the key type and bits is the key size in bits. |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_export_public_key | ( | psa_key_id_t | key, |
| uint8_t * | data, | ||
| size_t | data_size, | ||
| size_t * | data_length | ||
| ) |
Export a public key or the public part of a key pair in binary format.
The output of this function can be passed to psa_import_key() to create an object that is equivalent to the public key.
This specification supports a single format for each key type. Implementations may support other formats as long as the standard format is supported. Implementations that support other formats should ensure that the formats are clearly unambiguous so as to minimize the risk that an invalid input is accidentally interpreted according to a different format.
For standard key types, the output format is as follows:
RSAPublicKey. m be the bit size associated with the curve, i.e. the bit size of q for a curve over F_q. The representation consists of:x_P as a ceiling(m/8)-byte string, big-endian;y_P as a ceiling(m/8)-byte string, big-endian.y = g^x mod p as a big-endian byte string. The length of the byte string is the length of the base prime p in bytes.Exporting a public key object or the public part of a key pair is always permitted, regardless of the key's usage flags.
| key | Identifier of the key to export. | |
| [out] | data | Buffer where the key data is to be written. |
| data_size | Size of the data buffer in bytes. | |
| [out] | data_length | On success, the number of bytes that make up the key data. |
| #PSA_SUCCESS | |
| #PSA_ERROR_INVALID_HANDLE | |
| #PSA_ERROR_INVALID_ARGUMENT | The key is neither a public key nor a key pair. |
| #PSA_ERROR_NOT_SUPPORTED | |
| #PSA_ERROR_BUFFER_TOO_SMALL | The size of the data buffer is too small. You can determine a sufficient buffer size by calling #PSA_EXPORT_KEY_OUTPUT_SIZE(#PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR(type), bits) where type is the key type and bits is the key size in bits. |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_import_key | ( | const psa_key_attributes_t * | attributes, |
| const uint8_t * | data, | ||
| size_t | data_length, | ||
| psa_key_id_t * | key | ||
| ) |
Import a key in binary format.
This function supports any output from psa_export_key(). Refer to the documentation of psa_export_public_key() for the format of public keys and to the documentation of psa_export_key() for the format for other key types.
The key data determines the key size. The attributes may optionally specify a key size; in this case it must match the size determined from the key data. A key size of 0 in attributes indicates that the key size is solely determined by the key data.
Implementations must reject an attempt to import a key of size 0.
This specification supports a single format for each key type. Implementations may support other formats as long as the standard format is supported. Implementations that support other formats should ensure that the formats are clearly unambiguous so as to minimize the risk that an invalid input is accidentally interpreted according to a different format.
| [in] | attributes | The attributes for the new key. The key size is always determined from the data buffer. If the key size in attributes is nonzero, it must be equal to the size from data. |
| [out] | key | On success, an identifier to the newly created key. For persistent keys, this is the key identifier defined in attributes. 0 on failure. |
| [in] | data | Buffer containing the key data. The content of this buffer is interpreted according to the type declared in attributes. All implementations must support at least the format described in the documentation of psa_export_key() or psa_export_public_key() for the chosen type. Implementations may allow other formats, but should be conservative: implementations should err on the side of rejecting content if it may be erroneous (e.g. wrong type or truncated data). |
| data_length | Size of the data buffer in bytes. |
| #PSA_SUCCESS | Success. If the key is persistent, the key material and the key's metadata have been saved to persistent storage. |
| #PSA_ERROR_ALREADY_EXISTS | This is an attempt to create a persistent key, and there is already a persistent key with the given identifier. |
| #PSA_ERROR_NOT_SUPPORTED | The key type or key size is not supported, either by the implementation in general or in this particular persistent location. |
| #PSA_ERROR_INVALID_ARGUMENT | The key attributes, as a whole, are invalid, or the key data is not correctly formatted, or the size in attributes is nonzero and does not match the size of the key data. |
| #PSA_ERROR_INSUFFICIENT_MEMORY | |
| #PSA_ERROR_INSUFFICIENT_STORAGE | |
| #PSA_ERROR_COMMUNICATION_FAILURE | |
| #PSA_ERROR_DATA_CORRUPT | |
| #PSA_ERROR_DATA_INVALID | |
| #PSA_ERROR_STORAGE_FAILURE | |
| #PSA_ERROR_HARDWARE_FAILURE | |
| #PSA_ERROR_CORRUPTION_DETECTED | |
| #PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
1.8.12