Here is a list of all documented files with brief descriptions:
| crypto.h | Platform Security Architecture cryptography module |
| ext_flash_layout.h | Contains common structures and defines related to external flash layout as it for the OAD usecase |
| flash_interface.h | An interface that abstracts flash operations for OAD this allows on-chip and off-chip OAD to use the same flash APIs |
| HSMBareMetal.h | Interface to The HSM IP in a BareMetal-based implementation |
| oad_image_header.h | Structure definition for image header and segments, these are prepended to the over the air images |