![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
Information pertaining to the linklinkDB info. More...
Data Fields | |
| uint8 | addr [B_ADDR_LEN] |
| Other Device's address. More... | |
| uint8 | addrPriv [B_ADDR_LEN] |
| Other Device's Private address. More... | |
| uint8 | addrType |
| Address type of connected device. More... | |
| uint16 | connInterval |
| The connection's interval (n * 1.23 ms) More... | |
| uint16 | connLatency |
| current connection latency More... | |
| uint8 | connRole |
| Connection formed as Central or Peripheral. More... | |
| uint16 | connTimeout |
| current connection timeout More... | |
| uint16 | MTU |
| The connection's MTU size. More... | |
| uint8 | stateFlags |
| LinkDB Connection State Flags More... | |
Information pertaining to the linklinkDB info.
| uint8 addr[B_ADDR_LEN] |
Other Device's address.
| uint8 addrPriv[B_ADDR_LEN] |
Other Device's Private address.
| uint8 addrType |
Address type of connected device.
| uint16 connInterval |
The connection's interval (n * 1.23 ms)
| uint16 connLatency |
current connection latency
| uint8 connRole |
Connection formed as Central or Peripheral.
| uint16 connTimeout |
current connection timeout
| uint16 MTU |
The connection's MTU size.
| uint8 stateFlags |