TI BLE5-Stack API Documentation  9.14.00
Data Fields
l2capSendSduDoneEvt_t Struct Reference

L2CAP_SEND_SDU_DONE_EVT message format. More...

Data Fields

uint16 CID
 Local channel id. More...
 
uint16 credits
 Local credits. More...
 
uint16 peerCID
 Peer channel id. More...
 
uint16 peerCredits
 Peer credits. More...
 
uint16 totalLen
 Total length of SDU being transmitted. More...
 
uint16 txLen
 Total number of octets transmitted. More...
 

Detailed Description

L2CAP_SEND_SDU_DONE_EVT message format.

This message is sent to the app when an SDU transmission is completed or aborted.

Field Documentation

§ CID

uint16 CID

Local channel id.

§ credits

uint16 credits

Local credits.

§ peerCID

uint16 peerCID

Peer channel id.

§ peerCredits

uint16 peerCredits

Peer credits.

§ totalLen

uint16 totalLen

Total length of SDU being transmitted.

§ txLen

uint16 txLen

Total number of octets transmitted.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale