![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
Connection Response format. More...
Data Fields | |
| uint16 | dstCID |
| Represents CID on device receiving request and sending response. More... | |
| uint16 | initCredits |
| Indicates number of LE-frames that peer device can send. More... | |
| uint16 | mps |
| uint16 | mtu |
| uint16 | result |
| Indicates outcome of connection request: L2CAP Connection Response Result Values. More... | |
Connection Response format.
| uint16 dstCID |
Represents CID on device receiving request and sending response.
| uint16 initCredits |
Indicates number of LE-frames that peer device can send.
| uint16 mps |
Specifies Maximum PDU Payload Size (MPS) that can be received on this channel (Maximum Transmission Unit (MTU) for an outgoing/incoming L2CAP PDU.)
| uint16 mtu |
Specifies maximum SDU (service data unit) size that can be received on this channel (Maximum Transmission Unit for an unsegmented outgoing/incoming L2CAP SDU)
| uint16 result |
Indicates outcome of connection request: L2CAP Connection Response Result Values.