![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
Data Fields | |
| uint16_t | connectionHandle |
| Connection handle of the update. More... | |
| uint16_t | connInterval |
| Requested connection interval. More... | |
| uint16_t | connLatency |
| Requested connection latency. More... | |
| uint16_t | connTimeout |
| Requested connection timeout. More... | |
| osal_event_hdr_t | hdr |
| GAP_MSG_EVENT and status More... | |
| uint8_t | opcode |
| GAP_LINK_PARAM_UPDATE_EVENT More... | |
| uint8_t | status |
| status from link layer, defined in ll.h More... | |
GAP_LINK_PARAM_UPDATE_EVENT message format.
This message is sent to the app when the connection parameters update request is complete.
| uint16_t connectionHandle |
Connection handle of the update.
| uint16_t connInterval |
Requested connection interval.
| uint16_t connLatency |
Requested connection latency.
| uint16_t connTimeout |
Requested connection timeout.
| osal_event_hdr_t hdr |
GAP_MSG_EVENT and status
| uint8_t opcode |
| uint8_t status |
status from link layer, defined in ll.h