TI BLE5-Stack API Documentation  9.14.00
Data Fields
gapBondParams_t Struct Reference

Contains part of the GAP Bond Manager Parameters values. More...

Data Fields

uint8_t authenPairingOnly
 
uint8_t autoSyncAL
 
uint8_t bondFailAction
 
uint8_t bonding
 
uint8_t eccDebugKeys
 
uint8_t eccReGenPolicy
 
uint8_t eraseBondWhileInConn
 
uint8_t ioCap
 
uint8_t KeyDistList
 
uint8_t KeySize
 
uint8_t mitm
 
uint8_t pairMode
 
uint8_t removeLRUBond
 
uint8_t sameIrkAction
 
uint8_t secureConnection
 

Detailed Description

Contains part of the GAP Bond Manager Parameters values.

Field Documentation

§ authenPairingOnly

uint8_t authenPairingOnly

§ autoSyncAL

uint8_t autoSyncAL

§ bondFailAction

uint8_t bondFailAction

§ bonding

uint8_t bonding

§ eccDebugKeys

uint8_t eccDebugKeys

§ eccReGenPolicy

uint8_t eccReGenPolicy

§ eraseBondWhileInConn

uint8_t eraseBondWhileInConn

§ ioCap

uint8_t ioCap

§ KeyDistList

uint8_t KeyDistList

§ KeySize

uint8_t KeySize

§ mitm

uint8_t mitm

§ pairMode

uint8_t pairMode

§ removeLRUBond

uint8_t removeLRUBond

§ sameIrkAction

uint8_t sameIrkAction

§ secureConnection

uint8_t secureConnection

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale