![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.00
|
Stack image address information specific to build.
Go to the source code of this file.
Macros | |
| #define | ICALL_ADDR_MAPS |
| #define | ICALL_CUSTOM_INIT_PARAMS { USER0_CFG } |
| #define | ICALL_TASK_STACK_SIZES { 1500 } |
| #define | USER0_CFG &user0Cfg |
| user config More... | |
Functions | |
| void | startup_entry (const ICall_RemoteTaskArg *arg0, void *arg1) |
Variables | |
| icall_userCfg_t | user0Cfg |
| user config More... | |
| #define ICALL_ADDR_MAPS |
| void startup_entry | ( | const ICall_RemoteTaskArg * | arg0, |
| void * | arg1 | ||
| ) |
Initializer for an array of ICall_RemoteTaskEntry. Each element of the array corresponds to an entry function of an external image.
| icall_userCfg_t user0Cfg |
user config