TI BLE5-Stack API Documentation  9.14.00
File List
Here is a list of all files with brief descriptions:
 att.hATT layer interface
 bcomdef.hType definitions and macros for BLE stack
 bleapputil_api.hThis file contains the bleapputil_api for use with the Bluetooth Low Energy Protocol Stack
 bleapputil_timers.h
 comdef.hCommon Defines
 connection_monitor.h
 cs.h
 gap.hGAP layer interface
 gap_advertiser.hGAP Advertiser layer interface
 gap_initiator.hGAP Initiator layer interface
 gap_scanner.hGAP Scanner layer interface
 gapbondmgr.h
 gapgattserver.h
 gatt.hGATT layer interface
 gattservapp.hGATTServApp layer interface
 handover.h
 hci.hHCI layer interface
 hci_cs.h
 hci_tl.hTypes, constants, external functions etc. for the BLE HCI Transport Layer
 icall.hICall layer interface
 icall_addrs.hStack image address information specific to build
 l2cap.hL2CAP layer interface
 linkdb.h
 osal.hThis API allows the software components in the Z-Stack to be written independently of the specifics of the operating system, kernel, or tasking environment (including control loops or connect-to-interrupt systems)
 osal_memory.hHis module defines the OSAL memory control functions
 sm.hThis file contains the interface to the SM
 util.hUtil layer interface
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale