rfpacketerrorrate


Example Summary

The Packet Error Rate (PER) example showcases different RF transfer modes of the CC23xx. It combines tasks, events and several peripherals to a platform- independent application.

Test cases are provided for the following RF modes:

Peripherals Exercised

This example uses the following peripherals:

Example Usage

This example requires two boards, each running the PER Test application. However, the packet format is identical to the default one in SmartRF Studio, so that any compatible hardware can be used as well.

  1. Use the UART and hook it to a VT100-compatible terminal emulator at 115200 Baud. Use PuTTY or TeraTerm on Microsoft Windows. After a splash screen, you will see the main menu:

    Main Menu
    >Test: Rx
     Mode: MSK 250K
     Freq: 2405
     Pkts: 10
     Interval: No
     Length: 30
     Start...
    
  2. Navigate through the rows with BTN-2/DOWN, modify a value or start the selected test with BTN-1/UP.

  3. Use a second board with the PER test application as test companion for transmissions. Once started, the current progress is shown with these menus (TX mode on the left side, RX on the right):

    Sending...          |  Receiving...
    MSK 250K  2405      |  MSK 250K  2405
                        |  Pkts ok   : 10
    Pkts sent: 10       |  RSSI [dBm]: -26
                        |  PER  [%]  : 0.00
                        |  TP[bps]: 20867
                        |
                        |  ...finished.
    Push a button...    |  Push a button...
    

    The receiver prints the amount of successfully received packets (Pkts ok), the Signal strength of the current packet (RSSI), the observed packet error rate (PER) in percent, and the observed throughput in bits per second. Please note that the PER is n/a when sending more packets than configured in the receiver.

  4. You can always abort a running test case by pushing any button and go back to the main menu.

Application Design Details

The PER test application contains of one main task and an event handler to synchronize the task with buttons. After setting up all resources, the menu task is started and runs in an endless loop. It shows the menu and invokes test cases in either rx.c or tx.c.

PHY Packet Length Configuration

By default, the application compiles with variable packet length set up for each PHY. However, variable packet length is not supported for the 500KBPS MSK PHY in this application. 500KBPS MSK is always set up for fixed packet length. Variable packet length is set up for the PHY when the VARIABLE_LENGTH_SETUP symbol is defined. For fixed packet length set up, navigate in CCS to Project Properties -> Build -> Arm Compiler -> Predefined Symbols and change the VARIABLE_LENGTH_SETUP symbol to FIXED_LENGTH_SETUP.