Example Summary
Demonstrates how to use SPI driver in controller mode to communicate with another SimpleLink device. To run this example successfully, another SimpleLink device running the spiperipheral example is required.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
CONFIG_SPI_CONTROLLER- SPI peripheral assigned as a controllerCONFIG_SPI_CONTROLLER_READY- GPIO managed by controller to notify the peripheralCONFIG_SPI_CONTROLLERhas been openedCONFIG_SPI_PERIPHERAL_READY- GPIO to notify the controller the peripheral is ready for a transferCONFIG_GPIO_LED_0- Indicator LEDCONFIG_GPIO_LED_1- Indicator LED
BoosterPacks, Board Resources & Jumper Settings
This example requires two LaunchPads.
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Before running the example the following pins must be connected between controller and peripheral devices.
| SPI Controller LaunchPad | SPI Peripheral LaunchPad |
|---|---|
CONFIG_SPI_CONTROLLER_CLK |
CONFIG_SPI_PERIPHERAL_CLK |
CONFIG_SPI_CONTROLLER_PICO |
CONFIG_SPI_PERIPHERAL_PICO |
CONFIG_SPI_CONTROLLER_POCI |
CONFIG_SPI_PERIPHERAL_POCI |
CONFIG_SPI_CONTROLLER_CSN |
CONFIG_SPI_PERIPHERAL_CS |
CONFIG_SPI_CONTROLLER_READY |
CONFIG_SPI_CONTROLLER_READY |
CONFIG_SPI_PERIPHERAL_READY |
CONFIG_SPI_PERIPHERAL_READY |
The SPI can be used in 4-pin or 3-pin modes (chip select is optional). When running this example SPI peripherals on both SimpleLink devices must align on chip select use. Users must verify before running the example.
Although not in the table above, a ground jumper must also be connected between both boards.
Example Usage
Example output is generated through use of Display driver APIs. Refer to the Display driver documentation found in the SimpleLink MCU SDK User’s Guide.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port. The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
CONFIG_GPIO_LED_0turns ON to show the example is running.Once the peripheral is running, controller and peripheral devices will exchange messages in a loop. While the SPI transactions are taking place,
CONFIG_GPIO_LED_1will toggle on/off indicating transfers are occurring. After a transfer is complete, the messages are printed via UART. The loop is repeatedMAX_LOOPtimes.
Messages should appear as follows:
Starting the SPI controller example
This example requires external wires to be connected to the header pins. Please see the Board.html for details.
Controller SPI initialized
Controller received: Hello from peripheral, msg#: 0
Controller received: Hello from peripheral, msg#: 1
Controller received: Hello from peripheral, msg#: 2
Controller received: Hello from peripheral, msg#: 3
Controller received: Hello from peripheral, msg#: 4
Controller received: Hello from peripheral, msg#: 5
Controller received: Hello from peripheral, msg#: 6
Controller received: Hello from peripheral, msg#: 7
Controller received: Hello from peripheral, msg#: 8
Controller received: Hello from peripheral, msg#: 9
Done
Application Design Details
This application uses a single thread:
controllerThread - creates the controller SPI message, opens CONFIG_SPI_CONTROLLER and waits for the peripheral to be ready for a SPI transfer. When the peripheral is ready it starts the transfer. Once complete, the controller prepares the next transaction and waits for the peripheral once more. A total of MAX_LOOP SPI transactions are performed in this manner.
The controllerThread performs the following actions:
Before performing transfers, we must make sure the
spicontrollerandspiperipheralapplications are synchronized with each other. The controller will setCONFIG_SPI_CONTROLLER_READYto 1 to notify the peripheral it is ready to synchronize. The controller will then wait for the peripheral to setCONFIG_SPI_PERIPHERAL_READYto 1 in acknowledgment.Opens
CONFIG_SPI_CONTROLLERand setsCONFIG_SPI_CONTROLLER_READYto 0. SettingCONFIG_SPI_CONTROLLER_READYwill notify the peripheralCONFIG_SPI_CONTROLLERhas been opened.Waits for the peripheral to be ready for the SPI transfer. The peripheral will pull
CONFIG_SPI_PERIPHERAL_READYlow when ready for a transfer.Creates a SPI transaction structure and sets txBuffer to
Hello from controller, msg# n, where n is the iteration number.Toggles
CONFIG_GPIO_LED_1.Transfers the message. If the transfer is successful, the message received from the peripheral SPI is printed. Otherwise, an error message is printed.
Sleeps for 3 seconds.
Repeats from step 3 for
MAX_LOOPiterations.Closes the SPI driver object and terminates execution.
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.