Log Example

This example shows how to instrument your source code using Log, as well as using the respective tools to capture and view log output from the target.

Resources & Jumper Settings

If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.

If using CC32xx, then the device must be debugged in SWD mode and the SOP jumper must be placed in position 0 in order to send ITM messages on the SWO pin.

If using CC13XX/26XX the SWO jumper must be connected on the LaunchPad.

Definitions

The following terms are used throughout the Readme.

Term Definition
LogModule A parameter passed to Log APIs to indicate which software module the log statement originated from. Modules also control the routing of logs to sinks.
LogLevel The severity or importance of a given log statement.
Sink Also simply called a logger. This is a transport specific logger implementation.
The Logging framework is flexible such that multiple sinks may exist in a single firmware image.
CallSite A specific invocation of a Log API in a given file or program.
Record The binary representation of a log when it is stored or transported by a given sink. The log record format varys slightly with each sink depending on their implementation and needs. However, they all convey the same information.
Link Time Optimization (LTO) A feature of some toolchains that can significantly reduce the code overhead of the log statements through a process called dead code elimination. In order to maximize the benefits of this, all static libraries and application files should have LTO enabled.

Highlights

Beta Disclaimer

The logging ecosystem and this example are to be considered beta quality. They are not recommended for use in production code by TI. APIs and behaviour will change in future releases. Please report issues or feedback to E2E.

TI is seeking feedback in the following areas:

Overview

The example uses LTO to control inclusion of log statements in the built binary. There are two log modules used.

The routing of the log data is controlled by the relevant LogModule instance in SysConfig. This routing is controlled at the module level. That is, all log data from a given module goes to the same log sink.

The big picture:

file.c -->|[x]--> LogSinkBuf  --> memory, ROV
          |[ ]--> LogSinkITM  --> ITM, Wireshark
            ^
            |
LogModule --+

Visualization of logs depends on their transport. This is discussed in the following section.

Log Visualization

Each log module is routed to a different log sink. Due to the differing nature of the transport mechanisms used by the back end delegates, they are visualized using different methods. The table below shows the tooling used for visualizing the different types of logs.

Logger Visualization tool
LogSinkBuf Runtime Object View (ROV) 2
LogSinkITM Wireshark + TI Python Backend

The log statements can be viewed independently. It is not required to have both host side tools running in order for the example to run.

Example Usage

This demo illustrates a working example of logging. Note that some log sinks require special hardware initialization. In this example, both LogSinkITM and LogSinkBuf are used, but only LogSinkITM requires initialization:

LogSinkITM_init();

Please refer to the documentation of the particular log sink for more information on usage.

Import and Build the Example

  1. Import the project into your workspace.

  2. Build the project.

Load and Run the Program

This program uses ROV to display program output. You may interact with the program using memory flags controlled through the Expressions view.

  1. Follow the Quick Start Guide instructions in the readme in <SDK_INSTALL_DIR>/tools/log/tiutils
  2. Load the program.

  3. To view LogSinkBuf statements: Launch ROV.

    Tools -> Runtime Object View

    Open the ROV LogSinkBuf view

    Tools > Runtime Object View
    Connect
    LogSinkBuf
    LogSinkBuf > Records

    Enable continuous refresh to see the output as it is generated. The default refresh rate is 1 second.

  4. To view LogSinkITM statements: Launch Wireshark.

    Follow the steps in the “Extracting some Logs” section of the readme in <SDK_INSTALL_DIR>/tools/log/tiutils

  5. Run the program.

    In ROV, you will see the initial start up message, followed by a count update every 5 seconds.

    count=1
    count=2
    count=3

    In Wireshark, you will see the initial start up message (Hello world), and messages whenever the application’s semaphore is posted

    log_clkFxn: post semaphore
    ...

Note: LogSinkBuf requires ROV2 which is not available in IAR. Thus, there is no proper visualizer for these messages besides inspecting their records in memory. The ITM transport is supported across all IDEs/toolchains.

Conditional Log Inclusion

Log invocations are conditionally included in the final program based on the settings of the corresponding log module, if link-time optimization is enabled. If the log module is disabled, or the log-level for the particular invocation is insufficient, the linker will perform dead-code elimination, and optimize the call away.

It is therefore recommended to build with link time optimization if the toolchain supports it.

Source Code Instrumentation

To add instrumentation to your source code, requires three steps:

  1. Include Log.h
  2. Define a log module name
  3. Add an instrumentation call site

In log.c, you will see the following code which prints a greeting:

#include <ti/log/Log.h>

Log_printf(LogModule_App1, Log_DEBUG, "Hello World!");

The above code will implicitly declare a log module called LogModule_App1. This means that a logModule called LogModule_App1 must be defined, most easily by SysConfig. The log data associated with this log module will be routed to the logger instance specified by LogModule_App1.

Adding Modules

All log statements in the above example use either LogModule_App1 or LogModule_App2. Log modules are useful for grouping and sorting log statements that share configrations such as severity levels and sinks. In order to create a new module follow the steps below:

  1. Define a module name
  2. Create a Log module in SysConfig with the given name
  3. Configure the Log module to use a desired sink, and set log levels

SysConfig

Open the Logging category. You will find the following modules: