Example Summary

The C++ OPT3001 example application reads values from an OPT3001 ambient light sensor. It provides a basic example of utilizing TI-Drivers in a C++ application.

Peripherals & Pin Assignments

When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.

BoosterPacks, Board Resources & Jumper Settings

This example requires a BP-BASSENSORSMKII BoosterPack.

For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.

If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.

The Board.html can also be found in your SDK installation:

    <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>

Example Usage

The connection will have the following settings:

    Baud-rate:     115200
    Data bits:          8
    Stop bits:          1
    Parity:          None
    Flow Control:    None
    I2C Initialized!

    I2C device found at address 0x40!
    I2C device found at address 0x44!
    Finished looking for I2C devices.

    Information about the OPT3001 device..
    I2C Target Address      0x44
    Device ID:              0x3001
    Manufacturer ID:        0x5449
    Configuration Register: 0x8c90
    Low Limit:              0 lux
    High Limit:             83865 lux

    Set low limit to 30 lux
    Set high limit to 4000 lux

    Reading samples from OPT3001:
    Sample #1)   553 lux
    Sample #2)   556 lux
           .
           .
           .
    Sample #59)   552 lux
    Sample #60)   549 lux

    I2C closed!

To test the interrupt feature, cover the OPT3001 to trigger the low limit interrupt. Conversely, expose the sensor to additional light to trigger the high limit interrupt. When the sensor detects a value outside of the limit registers, you should see a message that resembles:

    ALARM: Low limit crossed!
    The sensor detected a value of 3 lux.
    The low limit is 20 lux

Application Design Details

This application uses two POSIX threads:

mainThread - performs the following actions:

  1. Opens and initializes an I2C, GPIO, Display and semaphore object.

  2. Displays information stored on the OPT3001 data registers and sets the limits of the interrupt mechanism.

  3. Uses the I2C driver to get data from the OPT3001 sensor.

  4. Extracts the light intensity value (in lux) and prints the value via the UART.

  5. The task sleeps for 1 second.

  6. After 60 light samples are recovered, the limit registers are reset and the device is set to shutdown mode. The I2C peripheral is closed and the example exits.

alarmThread - performs the following actions:

  1. Waits on a semaphore to be posted by an interrupt triggered by the OPT3001 interrupt pin.

  2. Displays an “ALARM: Low limit crossed!” or “ALARM: High limit crossed!” message whenever the OPT3001 sensor reads a value outside the programmed limits.

  3. Uses the I2C driver to get data from the OPT3001 sensor.

FreeRTOS: