Example Summary
This example shows how to use the SHA2 driver. The target accepts input over a serial port and displays back the hashed result. The input is limited to 256 bytes. If more than 256 bytes are entered, the application will not accept additional input and hash the intial 256 bytes received.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
BoosterPacks, Board Resources & Jumper Settings
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Example Usage
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection should have the following settings
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
The console application also needs to be setup to send the carriage-return (CR) character when ‘Enter’ is pressed. This is because it is used as the termination character in this demo. If the demo is not working properly, check the default configuration of the console application in question and make sure that it is sending the carriage-return character as expected.
Run the example.
Send the string to hash over the serial port. The string must be terminated by sending a carriage-return character.
The target will hash the string using SHA2 and echo back the result.
To confirm the example is behaving properly, the expected output for the input string “This is a demo string.” is FAE812FBA876DA7D4BC07C45485C27DBEA11D0627816C049FFF78CDD48FAA545.
Application Design Details
This examples shows how to use the SHA2 driver in single step hash mode.
The example expects the input string to be encoded in ASCII binary format. The user must make sure that the character binary represention used by the host side serial tool corresponds to that of the ASCII binary format.