Example Summary
This example is intended to show how an application can use the S2R RAM (Samples to RAM RAM) for extra scratch memory, and highlight some of the limitations of using S2R RAM.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
CONFIG_Display_UART- Used to display UART output.
BoosterPacks, Board Resources & Jumper Settings
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Example Usage
Example output is generated through use of Display driver APIs. Refer to the Display driver documentation found in the SimpleLink MCU SDK User’s Guide.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port. The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
- The example will ensure that the S2R RAM is clocked.
- The example will then perform the following sequence twice: write to S2R RAM, perform a dummy operation, and then verify that the S2R RAM contents remains unchanged. The two dummy operations are:
- Sleep
- Write to UART
The following is the expected example output.
Starting the s2rram example
Writing 0xAA to all bytes in S2R RAM buffer.
Verifying S2R RAM buffer after sleeping...
Verification was successful.
Writing 0x55 to all bytes in S2R RAM buffer.
This is a dummy operation that puts the device into Idle but not STANDBY.
It could be any operation that is known not to put the device in STANDBY.
For example a SPI transaction, crypto operation, etc.
Verifying S2R RAM buffer after performing dummy operation...
Verification was successful.
Application Design Details
The S2R RAM is intended for the S2R LRFD module, which for example is used for Channel Sounding. If however the S2R module is not used, the application can use the S2R RAM as additional scratch memory. There are some important limitations described in the list below:
- The S2R RAM must be clocked, and since this is part of the LRFD module, the LRFD module must be clocked as well.
- This will result in higher current consumption.
- Since the S2R RAM module is not clocked at boot, you cannot place initialized data in S2R RAM, since the auto-initialization sequence at startup will fail.
- The S2R RAM is not retained through STANDBY
- If the application relies on the S2R RAM being retained, it must not put the device in STANDBY for the period that the S2R RAM content must remain coherent.
- Whenever the device enters STANDBY, the application can no longer rely on any value in S2R RAM written to it before entering STANDBY. Once exiting STANDBY, new values can be written and read to and from S2R RAM again.
The TI provided linker files has memory regions defined for the S2R RAM, and the .s2rram section is placed in this memory region. To place a symbol in S2R RAM the application must place that symbol in the .s2rram section using compiler attributes. As mentioned above, no initialized data can be placed in S2R RAM, so only uninitialized data may be placed in the .s2rram section. Additionally data placed in .s2rram will not be auto zero-initialized.
The above mentioned limitations and requirements are handled in the example application. The key aspects are described in the list below.
- The application declares an uninitialized array
s2rramBufferand places it in the.s2rramsection. - To be able to read and write to the buffer, the S2R RAM must be clocked. This is achieved by setting a power dependency on the S2R RAM using this statement:
Power_setDependency(PowerLPF3_PERIPH_LFRD_S2RRAM); - When performing the
sleep(1)dummy operation, we must ensure that the device is not put into STANDBY, otherwise the verification might fail because the S2R RAM is not retained through STANDBY. To achieve this we set a power constraint to disallow STANDBY using this statement:Power_setConstraint(PowerLPF3_DISALLOW_STANDBY); - When performing the dummy operation to write to UART, we do not need set a power constraint because we know that that particular API call will never result in the device entering STANDBY. The power constraint is therefore released with this statement:
Power_releaseConstraint(PowerLPF3_DISALLOW_STANDBY); - At the end of the
mainThreadfunction, we release the dependency on S2R RAM, since it is no longer needed. This is done with the following statement:Power_releaseDependency(PowerLPF3_PERIPH_LFRD_S2RRAM);
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.