|
Radio Control Layer (RCL)
|
Go to the documentation of this file.
33 #ifndef ti_drivers_RCL_Scheduler_h__include
34 #define ti_drivers_RCL_Scheduler_h__include
45 #define RCL_SCHEDULER_SYSTIM_US(x) (((uint32_t) (x)) * 4U)
49 #define RCL_SCHEDULER_SYSTIM_MS(x) (((uint32_t) (x)) * 4U * 1000U)
53 #define ABS_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(100U)
54 #define IMM_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(90U)
55 #define RCL_SCHEDULER_MARGIN_ARM RCL_SCHEDULER_SYSTIM_US(40U)
56 #define RCL_SCHEDULER_MARGIN_CONFIGURE RCL_SCHEDULER_SYSTIM_US(76U)
57 #define RCL_SCHEDULER_MARGIN_LOAD RCL_SCHEDULER_SYSTIM_US(460U)
58 #define RCL_SCHEDULER_SLEEP_CUTOFF RCL_SCHEDULER_SYSTIM_MS(10U)
59 #define RCL_SCHEDULER_TRIG_NOW_DELAY RCL_SCHEDULER_SYSTIM_US(50U)
60 #if defined(DeviceFamily_CC23X0R5) || defined(DeviceFamily_CC23X0R2)
61 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(390U)
63 #define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(1000U)
78 typedef struct RCL_SchedulerStopInfo_s {
87 typedef struct RCL_SchedulerState_s {
void hal_trigger_command_fsm(void)
Definition: hal_octopus.c:115
RCL_CommandStatus RCL_Scheduler_setStartStopTimeEarliestStart(const RCL_Command *cmd, uint32_t earliestStartTime)
Set start and stop time for LRF based on command with earliest start time.
Definition: RCL_Scheduler.c:94
@ SchedulerStartAbsTimeNoDelay
Definition: RCL_Scheduler.c:59
uint32_t cmdStopTime
Definition: RCL_Scheduler.h:83
SchedulerStartType
Definition: RCL_Scheduler.c:55
@ RCL_SchedulerStopTimeSelect_None
Definition: RCL_Scheduler.h:67
RCL_StopType RCL_Scheduler_setSchedStopTime(RCL_SchedulerStopInfo *stopInfo, uint32_t schedStopTime)
Set scheduler stop time.
Definition: RCL_Scheduler.c:391
uint32_t apiStopEnabled
Definition: RCL_Scheduler.h:81
RCL_Command * currCmd
Definition: RCL_Scheduler.h:88
RCL_SchedulerState rclSchedulerState
Definition: RCL_Scheduler.c:51
RCL_CommandStatus RCL_Scheduler_setStartStopTime(const RCL_Command *cmd)
Set start and stop time for LRF based on command.
Definition: RCL_Scheduler.c:69
void hal_setup_start_time(uint32_t startTime)
Definition: hal_octopus.c:159
RCL_StopType
Stop types.
Definition: RCL_Command.h:129
void hal_cancel_hard_stop_time(void)
Definition: hal_octopus.c:210
static uint32_t RCL_Scheduler_getCurrentTime(void)
Get current time.
Definition: RCL_Scheduler.h:233
RCL_CommandStatus RCL_Scheduler_setCmdStopTimeNoStartTrigger(const RCL_Command *cmd)
Set stop time for LRF based on command when it does not need a start trigger.
Definition: RCL_Scheduler.c:132
@ RCL_CommandStatus_Finished
Definition: RCL_Command.h:90
RCL_SchedulerStopInfo gracefulStopInfo
Definition: RCL_Scheduler.h:94
@ RCL_CommandStatus_Queued
Definition: RCL_Command.h:85
bool RCL_Scheduler_isLater(uint32_t refTime, uint32_t chkTime)
Find if a time instant occurs after another, allowing wrap-around.
Definition: RCL_Scheduler.c:345
#define RCL_Debug_assert(expr)
Definition: RCL_Debug.h:39
RCL_CommandStatus
Command status.
Definition: RCL_Command.h:83
uint32_t cmdStopEnabled
Definition: RCL_Scheduler.h:79
@ RCL_StopType_Graceful
Definition: RCL_Command.h:132
RCL_Events postedRclEvents
Definition: RCL_Scheduler.h:91
RCL_CommandStatus RCL_Scheduler_setNewStartNow(void)
Set new start time for LRF to now, after a previous start.
Definition: RCL_Scheduler.c:142
RCL_CommandStatus RCL_Scheduler_setNewStartAbsTime(uint32_t startTime)
Set new start time for LRF to given absolute time, after a previous start.
Definition: RCL_Scheduler.c:150
uint32_t schedStopEnabled
Definition: RCL_Scheduler.h:80
@ RCL_SchedulerStopTimeSelect_Sched
Definition: RCL_Scheduler.h:69
int32_t RCL_Scheduler_delta(uint32_t refTime, uint32_t chkTime)
Find the time difference between two times, allowing wrap-around.
Definition: RCL_Scheduler.c:363
@ RCL_StopType_None
Definition: RCL_Command.h:130
Definition: RCL_Scheduler.h:87
uint32_t schedStopTime
Definition: RCL_Scheduler.h:84
uint32_t nextWantsStop
Definition: RCL_Scheduler.h:89
RCL_CommandStatus RCL_Scheduler_setNewStartRelTime(uint32_t relStartTime)
Set new start time for LRF to given time relative to previous LRF start.
Definition: RCL_Scheduler.c:158
Definition: RCL_Scheduler.h:78
RCL_SchedulerStopTimeState stopTimeState
Definition: RCL_Scheduler.h:90
@ RCL_CommandStatus_Error_StartTooLate
Definition: RCL_Command.h:108
uint32_t hal_get_current_time(void)
Definition: hal_octopus.c:133
void hal_setup_graceful_stop_time(uint32_t stopTime)
Definition: hal_octopus.c:184
@ RCL_Schedule_AbsTime
Definition: RCL_Command.h:144
RCL_SchedulerStopTimeState
Definition: RCL_Scheduler.h:72
@ RCL_CommandStatus_Active
Definition: RCL_Command.h:87
RCL_SchedulerStopTimeSelect stopTimeSelect
Definition: RCL_Scheduler.h:82
@ RCL_SchedulerStopTimeState_Found
Definition: RCL_Scheduler.h:74
@ RCL_CommandStatus_GracefulStop
Definition: RCL_Command.h:96
@ RCL_SchedulerStopTimeState_Programmed
Definition: RCL_Scheduler.h:75
#define RCL_EventSoftwareTriggered
Definition: RCL_Event.h:44
#define RCL_SCHEDULER_TRIG_NOW_DELAY
Definition: RCL_Scheduler.h:59
@ RCL_CommandStatus_HardStop
Definition: RCL_Command.h:97
@ RCL_SchedulerStopTimeState_Init
Definition: RCL_Scheduler.h:73
@ SchedulerNoStart
Definition: RCL_Scheduler.c:56
@ SchedulerStartNow
Definition: RCL_Scheduler.c:57
static void rclSchedulerFindEarliestStopTime(RCL_SchedulerStopInfo *stopInfo)
Definition: RCL_Scheduler.c:440
static RCL_CommandStatus rclSchedulerProcessCmdStartStopTime(const RCL_Command *cmd, uint32_t startTime, SchedulerStartType startType)
Definition: RCL_Scheduler.c:168
RCL_SchedulerStopInfo hardStopInfo
Definition: RCL_Scheduler.h:93
void * RCL_Command_Handle
Definition: RCL_Types.h:36
@ SchedulerStartAbsTimeAllowDelay
Definition: RCL_Scheduler.c:58
uint32_t actualStartTime
Definition: RCL_Scheduler.h:92
void hal_cancel_graceful_stop_time(void)
Definition: hal_octopus.c:216
bool RCL_Scheduler_postEvent(RCL_Command_Handle c, RCL_Events e)
Post event to command handler.
Definition: RCL_Scheduler.c:498
void hal_setup_hard_stop_time(uint32_t stopTime)
Definition: hal_octopus.c:169
RCL_SchedulerState rclSchedulerState
Definition: RCL_Scheduler.c:51
@ RCL_StopType_Hard
Definition: RCL_Command.h:133
RCL_SchedulerStopTimeSelect
Definition: RCL_Scheduler.h:66
@ RCL_SchedulerStopTimeSelect_Cmd
Definition: RCL_Scheduler.h:68
RCL_StopType RCL_Scheduler_setStopTimes(void)
Function to apply relevant stop times.
Definition: RCL_Scheduler.c:294