|
Radio Control Layer (RCL)
|
#include <stdint.h>#include <stddef.h>#include <stdbool.h>#include <ti/devices/DeviceFamily.h>#include <ti/drivers/rcl/RCL_Types.h>
Include dependency graph for LRFCC23X0.h:
This graph shows which files directly or indirectly include this file:Go to the source code of this file.
Macros | |
| #define | LRF_TxPowerTable_INVALID_VALUE ((LRF_TxPowerTable_Value){.rawValue = 0xFFFF}) |
| #define | LRF_EventNone ((LRF_Events){ .value = (0U << 0U)}) |
| #define | LRF_EventOpDone ((LRF_Events){ .value = (1U << 0U)}) |
| #define | LRF_EventPingRsp ((LRF_Events){ .value = (1U << 1U)}) |
| #define | LRF_EventRxCtrl ((LRF_Events){ .value = (1U << 2U)}) |
| #define | LRF_EventRxCtrlAck ((LRF_Events){ .value = (1U << 3U)}) |
| #define | LRF_EventRxNok ((LRF_Events){ .value = (1U << 4U)}) |
| #define | LRF_EventRxIgnored ((LRF_Events){ .value = (1U << 5U)}) |
| #define | LRF_EventRxEmpty ((LRF_Events){ .value = (1U << 6U)}) |
| #define | LRF_EventRxBufFull ((LRF_Events){ .value = (1U << 7U)}) |
| #define | LRF_EventRxOk ((LRF_Events){ .value = (1U << 8U)}) |
| #define | LRF_EventTxCtrl ((LRF_Events){ .value = (1U << 9U)}) |
| #define | LRF_EventTxCtrlAckAck ((LRF_Events){ .value = (1U << 10U)}) |
| #define | LRF_EventTxRetrans ((LRF_Events){ .value = (1U << 11U)}) |
| #define | LRF_EventTxAck ((LRF_Events){ .value = (1U << 12U)}) |
| #define | LRF_EventTxDone ((LRF_Events){ .value = (1U << 13U)}) |
| #define | LRF_EventTxCtrlAck ((LRF_Events){ .value = (1U << 14U)}) |
| #define | LRF_EventOpError ((LRF_Events){ .value = (1U << 15U)}) |
| #define | LRF_EventRxfifo ((LRF_Events){ .value = (1U << 16U)}) |
| #define | LRF_EventTxfifo ((LRF_Events){ .value = (1U << 17U)}) |
| #define | LRF_EventLossOfLock ((LRF_Events){ .value = (1U << 18U)}) |
| #define | LRF_EventLock ((LRF_Events){ .value = (1U << 19U)}) |
| #define | LRF_EventRfesoft0 ((LRF_Events){ .value = (1U << 20U)}) |
| #define | LRF_EventRfesoft1 ((LRF_Events){ .value = (1U << 21U)}) |
| #define | LRF_EventRfedone ((LRF_Events){ .value = (1U << 22U)}) |
| #define | LRF_EventMdmsoft0 ((LRF_Events){ .value = (1U << 23U)}) |
| #define | LRF_EventMdmsoft1 ((LRF_Events){ .value = (1U << 24U)}) |
| #define | LRF_EventMdmsoft2 ((LRF_Events){ .value = (1U << 25U)}) |
| #define | LRF_EventMdmout ((LRF_Events){ .value = (1U << 26U)}) |
| #define | LRF_EventMdmin ((LRF_Events){ .value = (1U << 27U)}) |
| #define | LRF_EventMdmdone ((LRF_Events){ .value = (1U << 28U)}) |
| #define | LRF_EventSystim0 ((LRF_Events){ .value = (1U << 29U)}) |
| #define | LRF_EventSystim1 ((LRF_Events){ .value = (1U << 30U)}) |
| #define | LRF_EventSystim2 ((LRF_Events){ .value = (1U << 31U)}) |
| #define | LRF_TxPowerEntry_INVALID_VALUE |
| #define | LRF_TRIM_NUM_VARIANTS 2 |
| #define | LRF_TRIM_NORMAL_BW 0 |
| #define | LRF_TRIM_HIGH_BW 1 /* Revision >= 4 only */ |
| #define | LRF_TRIM_MIN_VERSION_FULL_FEATURES 4 /* Only AppTrims revision 4 and above has all features */ |
| #define | LRF_TRIM_VERSION_RSSIOFFSET_ISSUE 4 /* AppTrims revision with issue in rssiOffset field */ |
| #define | LRF_TRIM_LIMIT_RSSIOFFSET_ISSUE (-4) /* If rssiOffset is less or equal to this, apply correction */ |
| #define | LRF_TRIM_CORRECTION_RSSIOFFSET_ISSUE 5 /* Correction to apply to devices with wrong RSSI offset */ |
| #define | LRF_BASE_ADDR 0x40080000U |
| #define | PBE_RAM_BASE_ADDR 0x40090000U |
| #define | BUF_RAM_BASE_ADDR 0x40092000U |
| #define | MCE_RAM_BASE_ADDR 0x40094000U |
| #define | RFE_RAM_BASE_ADDR 0x40096000U |
| #define | S2R_RAM_BASE_ADDR 0x40098000U |
| #define | TOPSM_RAM_SZ 0x00001000U /* 4 KB */ |
| #define | MAX_REG_CONFIG_LEN 1024U /* 1024 entries, using 4 KB */ |
| #define | LRF_TXPOWER_REFERENCE_TEMPERATURE 25 |
| #define | LRF_TXPOWER_TEMPERATURE_SCALING 0x100 |
Typedefs | |
| typedef uint8_t | LRF_TxPowerTable_TempCoeff |
Enumerations | |
| enum | LRF_TxPowerResult { TxPowerResult_Ok, TxPowerResult_Error } |
Functions | |
| static void | LRF_sendHardStop (void) |
| static void | LRF_sendGracefulStop (void) |
| static void | LRF_hardStop (void) |
| static uint32_t | LRF_getTxFifoWritable (void) |
| void | LRF_programTemperatureCompensatedTxPower (void) |
| Programs current TX power setting in radio with temperature compensation. More... | |
| LRF_TxPowerResult | LRF_programTxPower (LRF_TxPowerTable_Index powerLevel) |
| Finds settings corresponding to the highest tx power lower than the specified value in the tx power table and programs it in the radio. More... | |
Variables | |
| const LRF_TxShape | LRF_shapeBaseGfsk05 |
| const LRF_TxShape | LRF_shapeBaseGfsk067 |
| const LRF_TxShape | LRF_shapeBaseGfsk20 |
| union LRF_TxPowerTable_Value |
Type for tx power configuration.
Register value to be written to registers, prior to temperature compensation
| Data Fields | ||
|---|---|---|
| struct LRF_TxPowerTable_Value | __unnamed__ | |
| uint16_t | rawValue | |
| union LRF_Events_u |
| Data Fields | ||
|---|---|---|
| struct LRF_Events_u | __unnamed__ | |
| uint32_t | value | |
| union LRF_TxPowerTable_Index |
Index of the tx power table.
| Data Fields | ||
|---|---|---|
| struct LRF_TxPowerTable_Index | __unnamed__ | |
| int8_t | rawValue | |
| struct LRF_TxPowerTable_Entry |
Single entry of the tx power table. Maps power in dBm to specific register settings.
Collaboration diagram for LRF_TxPowerTable_Entry:| Data Fields | ||
|---|---|---|
| LRF_TxPowerTable_Index | power |
Power level |
| LRF_TxPowerTable_TempCoeff | tempCoeff |
Temperature coefficient |
| LRF_TxPowerTable_Value | value |
Settings to be compensated and written into register |
| struct LRF_TxPowerTable |
Tx power table, containing all characterized dBm to register settings mappings.
The table must be sorted from lowest to highest power level
Collaboration diagram for LRF_TxPowerTable:| Data Fields | ||
|---|---|---|
| uint32_t | numEntries | |
| LRF_TxPowerTable_Entry | powerTable[] | |
| struct LRF_TxShape |
| Data Fields | ||
|---|---|---|
| struct LRF_TxShape | __unnamed__ | |
| uint8_t | coeff[] | |
| union LRF_Trim1 |
Collaboration diagram for LRF_Trim1:| Data Fields | ||
|---|---|---|
| struct LRF_Trim1 | fields | |
| struct LRF_Trim1 | __unnamed__ | |
| LRF_DoubleWord | data | |
| union LRF_Trim2 |
Collaboration diagram for LRF_Trim2:| Data Fields | ||
|---|---|---|
| struct LRF_Trim2 | fields | |
| struct LRF_Trim2 | __unnamed__ | |
| LRF_DoubleWord | data | |
| union LRF_Trim_Variant |
Collaboration diagram for LRF_Trim_Variant:| Data Fields | ||
|---|---|---|
| struct LRF_Trim_Variant | fields | |
| struct LRF_Trim_Variant | __unnamed__ | |
| LRF_DoubleWord | data | |
| struct LRF_Trim_tempLdoRtrim |
| struct LRF_Trim_tempRssiAgc |
| struct LRF_TrimDef |
Collaboration diagram for LRF_TrimDef:| Data Fields | ||
|---|---|---|
| uint8_t | revision | |
| uint8_t | nToolsClientOffset | |
| uint8_t | reserved[2] | |
| LRF_Trim0 | trim0 | |
| LRF_Trim1 | trim1 | |
| LRF_Trim2 | trim2 | |
| LRF_Trim_Variant | trimVariant[LRF_TRIM_NUM_VARIANTS] | |
| LRF_Trim3 | trim3 | |
| LRF_Trim4 | trim4 | |
| struct LRF_SwConfig |
Software defined PHY parameters.
Collaboration diagram for LRF_SwConfig:| Data Fields | ||
|---|---|---|
| int32_t | rxIntFrequency |
Receiver intermediate frequency [Hz] |
| int32_t | rxFrequencyOffset |
Receiver frequency offset [Hz] |
| int32_t | txFrequencyOffset |
Transmitter frequency offset [Hz] |
| uint32_t | modFrequencyDeviation |
Transmitter frequency deviation [Hz] |
| const LRF_TxShape * | txShape |
Transmitter shape definition |
| uint8_t | bwIndex |
Index to use for bandwitdh dependent settings (0: normal 1: high) |
| uint8_t | bwIndexDither |
Index to use for bandwitdh dependent ADC dithering settings (0: low 1: normal/high) |
| struct LRF_SwParam |
Software defined PHY parameter list.
Collaboration diagram for LRF_SwParam:| Data Fields | ||
|---|---|---|
| const LRF_SwConfig * | swConfig |
Software defined parameters. |
| const LRF_TxPowerTable * | txPowerTable |
TX power table |
| const LRF_TrimDef * | trimDef |
Trim definitions. NULL: Do not apply trim. |
| struct LRF_Config |
| struct LRF_TxPowerTable_Value.__unnamed__ |
| struct LRF_Events_u.__unnamed__ |
| struct LRF_Trim0.fields.atstRefH |
| struct LRF_Trim1.__unnamed__ |
| struct LRF_Trim2.fields.dcoLdo0 |
| struct LRF_Trim2.fields.ifadcAldo |
| struct LRF_Trim2.fields.ifadcDldo |
| struct LRF_Trim2.__unnamed__ |
| struct LRF_Trim_Variant.fields |
| struct LRF_Trim_Variant.fields.ifadc0 |
| struct LRF_Trim_Variant.fields.ifadc1 |
| struct LRF_Trim_Variant.fields.ifadclf |
| struct LRF_Trim_Variant.__unnamed__ |
| struct LRF_Trim3.fields |
| Data Fields | ||
|---|---|---|
| fields | lrfdrfeExtTrim1 | |
| LRF_Trim_tempRssiAgc | lrfdrfeExtTrim0 | |
| struct LRF_Trim3.fields.lrfdrfeExtTrim1 |
| Data Fields | ||
|---|---|---|
| LRF_Trim_tempLdoRtrim | tempLdoRtrim | |
| uint8_t | hfxtPdError | |
| uint8_t | res | |
| struct LRF_Trim4.fields |
| Data Fields | ||
|---|---|---|
| fields | fend0Rssi | |
| fields | syntDiv0 | |
| uint16_t | res1 | |
| fields | ifamprfldo[LRF_TRIM_NUM_VARIANTS] | |
| struct LRF_Trim4.fields.fend0Rssi |
| struct LRF_Trim4.__unnamed__ |
| Data Fields | ||
|---|---|---|
| int8_t | rssiOffset | |
| uint8_t | trimCompleteN | |
| uint16_t | demIQMC0 | |
| uint16_t | res1 | |
| uint8_t | ifamprfldo[LRF_TRIM_NUM_VARIANTS] | |
| #define LRF_TxPowerTable_INVALID_VALUE ((LRF_TxPowerTable_Value){.rawValue = 0xFFFF}) |
Value indicating that no valid tx power could be found in the table.
| #define LRF_EventNone ((LRF_Events){ .value = (0U << 0U)}) |
No events
| #define LRF_EventOpDone ((LRF_Events){ .value = (1U << 0U)}) |
The PBE operation has finished
| #define LRF_EventPingRsp ((LRF_Events){ .value = (1U << 1U)}) |
When receiving a CMD_PING, PBE responds with a PINGRSP.
| #define LRF_EventRxCtrl ((LRF_Events){ .value = (1U << 2U)}) |
LL control packet received correctly
| #define LRF_EventRxCtrlAck ((LRF_Events){ .value = (1U << 3U)}) |
LL control packet received with CRC OK, not to be ignored, then acknowledgement sent
| #define LRF_EventRxNok ((LRF_Events){ .value = (1U << 4U)}) |
Packet received with CRC error
| #define LRF_EventRxIgnored ((LRF_Events){ .value = (1U << 5U)}) |
Packet received, but may be ignored by MCU
| #define LRF_EventRxEmpty ((LRF_Events){ .value = (1U << 6U)}) |
Empty packet received
| #define LRF_EventRxBufFull ((LRF_Events){ .value = (1U << 7U)}) |
Packet received which did not fit in the RX FIFO and was not to be discarded.
| #define LRF_EventRxOk ((LRF_Events){ .value = (1U << 8U)}) |
Packet received with CRC OK and not to be ignored by the MCU
| #define LRF_EventTxCtrl ((LRF_Events){ .value = (1U << 9U)}) |
Transmitted LL control packet
| #define LRF_EventTxCtrlAckAck ((LRF_Events){ .value = (1U << 10U)}) |
Acknowledgement received on a transmitted LL control packet, and acknowledgement transmitted for that packet
| #define LRF_EventTxRetrans ((LRF_Events){ .value = (1U << 11U)}) |
Packet retransmitted with same SN
| #define LRF_EventTxAck ((LRF_Events){ .value = (1U << 12U)}) |
Acknowledgement received on a transmitted packet.
| #define LRF_EventTxDone ((LRF_Events){ .value = (1U << 13U)}) |
Packet transmitted
| #define LRF_EventTxCtrlAck ((LRF_Events){ .value = (1U << 14U)}) |
Acknowledgement received on a transmitted LL control packet
| #define LRF_EventOpError ((LRF_Events){ .value = (1U << 15U)}) |
Something went awfully wrong, the reason is indicated in RAM-based register BLE_ENDCAUSE.
| #define LRF_EventRxfifo ((LRF_Events){ .value = (1U << 16U)}) |
Event from fifo, triggered when crossing threshold. Normal use for rxfifo is to generate IRQ when crossing threshold upwards (filling fifo). But downwards is also possible to configure, could be use case for using both fifos for TX or both for RX
| #define LRF_EventTxfifo ((LRF_Events){ .value = (1U << 17U)}) |
Event from fifo, triggered when crossing threshold. Normal use for txfifo is to generate IRQ when crossing threshold downwards (emptying fifo). But upwards is also possible to configure, could be use case for using both fifos for TX or both for RX
| #define LRF_EventLossOfLock ((LRF_Events){ .value = (1U << 18U)}) |
LOSS_OF_LOCK event
| #define LRF_EventLock ((LRF_Events){ .value = (1U << 19U)}) |
LOCK event
| #define LRF_EventRfesoft0 ((LRF_Events){ .value = (1U << 20U)}) |
RFESOFT0 event
| #define LRF_EventRfesoft1 ((LRF_Events){ .value = (1U << 21U)}) |
RFESOFT1 event
| #define LRF_EventRfedone ((LRF_Events){ .value = (1U << 22U)}) |
RFEDONE event
| #define LRF_EventMdmsoft0 ((LRF_Events){ .value = (1U << 23U)}) |
MDMSOFT event
| #define LRF_EventMdmsoft1 ((LRF_Events){ .value = (1U << 24U)}) |
MDMSOFT1 event
| #define LRF_EventMdmsoft2 ((LRF_Events){ .value = (1U << 25U)}) |
MDMSOFT event
| #define LRF_EventMdmout ((LRF_Events){ .value = (1U << 26U)}) |
MDMOUT event
| #define LRF_EventMdmin ((LRF_Events){ .value = (1U << 27U)}) |
MDMIN event
| #define LRF_EventMdmdone ((LRF_Events){ .value = (1U << 28U)}) |
MDMDONE event
| #define LRF_EventSystim0 ((LRF_Events){ .value = (1U << 29U)}) |
SYSTIM0 event
| #define LRF_EventSystim1 ((LRF_Events){ .value = (1U << 30U)}) |
SYSTIM1 event
| #define LRF_EventSystim2 ((LRF_Events){ .value = (1U << 31U)}) |
SYSTIM2 event
| #define LRF_TxPowerEntry_INVALID_VALUE |
Value indicating that no valid tx power could be found in the table.
| #define LRF_TRIM_NUM_VARIANTS 2 |
| #define LRF_TRIM_NORMAL_BW 0 |
| #define LRF_TRIM_HIGH_BW 1 /* Revision >= 4 only */ |
| #define LRF_TRIM_MIN_VERSION_FULL_FEATURES 4 /* Only AppTrims revision 4 and above has all features */ |
| #define LRF_TRIM_VERSION_RSSIOFFSET_ISSUE 4 /* AppTrims revision with issue in rssiOffset field */ |
| #define LRF_TRIM_LIMIT_RSSIOFFSET_ISSUE (-4) /* If rssiOffset is less or equal to this, apply correction */ |
| #define LRF_TRIM_CORRECTION_RSSIOFFSET_ISSUE 5 /* Correction to apply to devices with wrong RSSI offset */ |
| #define LRF_BASE_ADDR 0x40080000U |
| #define PBE_RAM_BASE_ADDR 0x40090000U |
| #define BUF_RAM_BASE_ADDR 0x40092000U |
| #define MCE_RAM_BASE_ADDR 0x40094000U |
| #define RFE_RAM_BASE_ADDR 0x40096000U |
| #define S2R_RAM_BASE_ADDR 0x40098000U |
| #define TOPSM_RAM_SZ 0x00001000U /* 4 KB */ |
| #define MAX_REG_CONFIG_LEN 1024U /* 1024 entries, using 4 KB */ |
| #define LRF_TXPOWER_REFERENCE_TEMPERATURE 25 |
Reference temperature for TX power, degrees C
| #define LRF_TXPOWER_TEMPERATURE_SCALING 0x100 |
Scaling factor for TX power temperature coefficients
| typedef uint8_t LRF_TxPowerTable_TempCoeff |
| enum LRF_TxPowerResult |
|
inlinestatic |
|
inlinestatic |
|
inlinestatic |
|
inlinestatic |
| void LRF_programTemperatureCompensatedTxPower | ( | void | ) |
Programs current TX power setting in radio with temperature compensation.
References hal_get_temperature(), LRF_TXPOWER_REFERENCE_TEMPERATURE, LRF_TXPOWER_TEMPERATURE_SCALING, lrfPhyState, LRF_TxPowerTable_Value::rawValue, RFE_PA0_IB_MIN_USED, LRF_TxPowerTable_Entry::tempCoeff, and LRF_TxPowerTable_Entry::value.
Referenced by LRF_programTxPower().
| LRF_TxPowerResult LRF_programTxPower | ( | LRF_TxPowerTable_Index | powerLevel | ) |
Finds settings corresponding to the highest tx power lower than the specified value in the tx power table and programs it in the radio.
| powerLevel | maximum allowed power level in dBm, or special value (LRF_TxPower_Use_Min, LRF_TxPower_Use_Max, LRF_TxPower_Use_Raw, or LRF_TxPower_None) |
References LRF_programTemperatureCompensatedTxPower(), LRF_TxPower_None, LRF_TxPowerTable_findValue(), LRF_TxPowerTable_INVALID_VALUE, lrfPhyState, LRF_TxPowerTable_Value::rawValue, LRF_TxPowerTable_Index::rawValue, swParamList, TxPowerResult_Error, TxPowerResult_Ok, LRF_SwParam::txPowerTable, and LRF_TxPowerTable_Entry::value.
Referenced by RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_dtmTx(), RCL_Handler_BLE5_genericTx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Ble5_txTest(), RCL_Handler_Generic_Tx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Generic_TxTest(), RCL_Handler_Nesb_Prx(), and RCL_Handler_Nesb_Ptx().
| const LRF_TxShape LRF_shapeBaseGfsk05 |
| const LRF_TxShape LRF_shapeBaseGfsk067 |
| const LRF_TxShape LRF_shapeBaseGfsk20 |