![]() |
![]() |
UART2LPF3 Hardware attributes. More...
#include <UART2LPF3.h>
Data Fields | |
| UART2_BASE_HWATTRS volatile uDMAControlTableEntry * | dmaTxTableEntryPri |
| volatile uDMAControlTableEntry * | dmaRxTableEntryPri |
| uint32_t | txChannelMask |
| uint32_t | rxChannelMask |
| int32_t | txPinMux |
| int32_t | rxPinMux |
| int32_t | ctsPinMux |
| int32_t | rtsPinMux |
| UART2LPF3_CodingScheme | codingScheme |
| uint8_t | irLPClkDivider |
| uint8_t | powerID |
| uint8_t | txChannelEvtMux |
| uint8_t | rxChannelEvtMux |
| bool | concatenateFIFO |
UART2LPF3 Hardware attributes.
The fields, baseAddr and intNum are used by driverlib APIs and therefore must be populated by driverlib macro definitions. These definitions are found under the device family in:
intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
The Low Power F3 devices use either three or two priority bits, depending on the device. That means ~0 has the same effect as (7 << 5) or (3 << 6), respectively.
Setting the priority to 0 is not supported by this driver. HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.
A sample structure is shown below:
To enable flow control, the .ctsPin and/or .rtsPin must be assigned. In addition, .flowControl must be set to UART2_FLOWCTRL_HARDWARE.
| UART2_BASE_HWATTRS volatile uDMAControlTableEntry* UART2LPF3_HWAttrs::dmaTxTableEntryPri |
uDMA controlTable primary TX entry
| volatile uDMAControlTableEntry* UART2LPF3_HWAttrs::dmaRxTableEntryPri |
uDMA controlTable primary RX entry
| uint32_t UART2LPF3_HWAttrs::txChannelMask |
Mask for uDMA TX channel number (1 << channel number)
| uint32_t UART2LPF3_HWAttrs::rxChannelMask |
Mask for uDMA RX channel number (1 << channel number)
| int32_t UART2LPF3_HWAttrs::txPinMux |
TX PIN mux value
| int32_t UART2LPF3_HWAttrs::rxPinMux |
RX PIN mux value
| int32_t UART2LPF3_HWAttrs::ctsPinMux |
CTS PIN mux value for flow control
| int32_t UART2LPF3_HWAttrs::rtsPinMux |
RTS PIN mux value for flow control
| UART2LPF3_CodingScheme UART2LPF3_HWAttrs::codingScheme |
UART TXD/RXD encoding/decoding scheme
| uint8_t UART2LPF3_HWAttrs::irLPClkDivider |
Clock divider for IR Low-Power mode
| uint8_t UART2LPF3_HWAttrs::powerID |
Power driver ID for this UART instance
| uint8_t UART2LPF3_HWAttrs::txChannelEvtMux |
Mux ID for this UART instance TX pin
| uint8_t UART2LPF3_HWAttrs::rxChannelEvtMux |
Mux ID for this UART instance RX pin
| bool UART2LPF3_HWAttrs::concatenateFIFO |
Concatenate RX and TX FIFO if write-only