![]() |
![]() |
Structure for MCAN Rx FIFO Status. More...
#include <MCAN.h>
Data Fields | |
| uint32_t | fillLvl |
| uint32_t | getIdx |
| uint32_t | putIdx |
| uint32_t | fifoFull |
| uint32_t | msgLost |
Structure for MCAN Rx FIFO Status.
| uint32_t MCAN_RxFIFOStatus::fillLvl |
Rx FIFO Fill Level - number of elements stored in Rx FIFO
| uint32_t MCAN_RxFIFOStatus::getIdx |
Rx FIFO Get Index
| uint32_t MCAN_RxFIFOStatus::putIdx |
Rx FIFO Put Index
| uint32_t MCAN_RxFIFOStatus::fifoFull |
Rx FIFO Full 0 = Rx FIFO not full 1 = Rx FIFO full
| uint32_t MCAN_RxFIFOStatus::msgLost |
Rx FIFO Message Lost