![]() |
![]() |
Struct containing the parameters required for signing a message. More...
#include <ECDSA.h>

Data Fields | |
| const ECCParams_CurveParams * | curve |
| const CryptoKey * | myPrivateKey |
| const uint8_t * | hash |
| uint8_t * | r |
| uint8_t * | s |
Struct containing the parameters required for signing a message.
| const ECCParams_CurveParams* ECDSA_OperationSign::curve |
A pointer to the elliptic curve parameters
| const CryptoKey* ECDSA_OperationSign::myPrivateKey |
A pointer to the private ECC key that will sign the hash of the message
| const uint8_t* ECDSA_OperationSign::hash |
A pointer to the hash of the message in octet string format. Must be the same length as the other curve parameters.
| uint8_t* ECDSA_OperationSign::r |
A pointer to the buffer the r component of the signature will be written to. Formatted in octet string format. Must be of the same length as other params of the curve used.
| uint8_t* ECDSA_OperationSign::s |
A pointer to the buffer the s component of the signature will be written to. Must be of the same length as other params of the curve used.