#include <DisplaySharp.h>
§ spiIndex
| uint32_t DisplaySharp_HWAttrsV1::spiIndex |
§ csPin
| uint32_t DisplaySharp_HWAttrsV1::csPin |
§ powerPin
| uint32_t DisplaySharp_HWAttrsV1::powerPin |
§ enablePin
| uint32_t DisplaySharp_HWAttrsV1::enablePin |
§ pixelHeight
| uint16_t DisplaySharp_HWAttrsV1::pixelHeight |
§ pixelWidth
| uint16_t DisplaySharp_HWAttrsV1::pixelWidth |
§ displayBuf
| void* DisplaySharp_HWAttrsV1::displayBuf |
§ font
| const Graphics_Font* DisplaySharp_HWAttrsV1::font |
The documentation for this struct was generated from the following file: