Struct containing the parameters required for finalizing an encryption/decryption and authentication/verification of a message in a segmented operation.
More...
#include <AESGCM.h>
Struct containing the parameters required for finalizing an encryption/decryption and authentication/verification of a message in a segmented operation.
§ input
| uint8_t* AESGCM_SegmentedFinalizeOperation::input |
- Encryption: The plaintext buffer to be encrypted and authenticated in the GCM operation.
- Decryption: The ciphertext to be decrypted and verified.
§ output
| uint8_t* AESGCM_SegmentedFinalizeOperation::output |
- Encryption: The output ciphertext buffer that the encrypted plaintext is copied to.
- Decryption: The plaintext derived from the decrypted and verified ciphertext is copied here.
§ mac
| uint8_t* AESGCM_SegmentedFinalizeOperation::mac |
- Encryption: The buffer where the message authentication code is copied.
- Decryption: The buffer containing the received message authentication code.
§ inputLength
| size_t AESGCM_SegmentedFinalizeOperation::inputLength |
Length of the input/output data in bytes. Can be 0 if finalizing without new payload data. Unlike this field in AESGCM_SegmentedDataOperation, the length doesn't need to be block-aligned.
§ macLength
| uint8_t AESGCM_SegmentedFinalizeOperation::macLength |
Length of mac in bytes. Valid MAC lengths are [4, 8, 12, 13, 14, 15, 16].
The documentation for this struct was generated from the following file: