![]() |
![]() |
AESCMACLPF3 Object. More...
#include <AESCMACLPF3.h>

Data Fields | |
| AESCommonLPF3_Object | common |
| volatile uint32_t | intermediateTag [AES_TAG_LENGTH_BYTES/4U] |
| uint32_t | finalInputBlock [AES_BLOCK_SIZE_WORDS] |
| AESCMAC_CallbackFxn | callbackFxn |
| AESCMAC_Operation * | operation |
| AESCMAC_OperationType | operationType |
| AESCMAC_OperationalMode | operationalMode |
| bool | threadSafe |
AESCMACLPF3 Object.
The application must not access any member variables of this structure!
| AESCommonLPF3_Object AESCMACLPF3_Object::common |
| volatile uint32_t AESCMACLPF3_Object::intermediateTag[AES_TAG_LENGTH_BYTES/4U] |
| uint32_t AESCMACLPF3_Object::finalInputBlock[AES_BLOCK_SIZE_WORDS] |
| AESCMAC_CallbackFxn AESCMACLPF3_Object::callbackFxn |
| AESCMAC_Operation* AESCMACLPF3_Object::operation |
| AESCMAC_OperationType AESCMACLPF3_Object::operationType |
| AESCMAC_OperationalMode AESCMACLPF3_Object::operationalMode |
| bool AESCMACLPF3_Object::threadSafe |